Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum boot from ssd in pi desktop
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 73 replies
  • Answers 11 answers
  • Subscribers 715 subscribers
  • Views 13023 views
  • Users 0 members are here
  • raspberry_pi_space
Related

boot from ssd in pi desktop

gdenicolas
gdenicolas over 9 years ago

I couldnt find the file pidesktop.deb. The webpage is really complicated.

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    0 cstanton over 9 years ago

    Hi gdenicolas ,

     

    You don't need the debian file to boot from the SSD. In the user manual is a step by step guide and explanation on how to set this up:

    Pi Desktop User Manual_EN_Rev3.2-FINAL.pdf

     

    I've asked internally about the debian file, and I've read through the manual where there's some typing errors that need to be fixed (eg. capitalization of linux commands).

     

    Feel free to ask me any questions on this as I've been working with this add-on board (and have one sat on my desk).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    My concern not loading the pidesktop.deb is that you lose out on :

     

    ppp-hdclone (What it does probably can be done just by dd'ing the image to the mSata)

     

    ppp-boot (This actually changes the /boot/cmdline.txt to change the root, which isn't mentioned. I had previously set the usb variable, but AFTER I put it all together so can't get the card out to test if it isn't needed)

     

    embest.service/embest-shutdown.service/rtc.py/sync-hwclock - Seem like they make sure the HWClock is up to date, not mentioned in the manual.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    I didn't. It was on the SD I made the changes. But still the issue that despite having the 0x3020000a set, it isn't booting from SSD.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    Tuc . wrote:

     

    Hi,

     

    I didn't. It was on the SD I made the changes. But still the issue that despite having the 0x3020000a set, it isn't booting from SSD.

     

    Tuc

    When I initially imaged the SSD it didn't boot either, and that was because of the software I used to write the image to the SSD didn't do it properly.

     

    What software/commands have you used to write the image to the SSD and under which operating system?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    Raspbian Pixel, fresh install to the SD.

     

    unzip -p|dd bs=1m of=/dev/sda

     

    I think thats it. Might be uppercase M, I get confused, some platforms take it, others don't. I didn't have space on the 8G card in it, so I had to stream the contents of the download and pipe into dd.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    I would suggest trying either the hard drive clone script that's included with the debian package to replicate your SDCard raspbian install, or try imaging the SSD by connecting it to another computer (this is outlined in the manual).

     

    Have you tried wiping the SSD and partitioning it via other ways (not imaging it) to see if it's compatible and working in with the Pi HAT add-on? There could be something funny going on there, too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    Unfortunately, I can't. I don't own anything else that can take the mSata card (https://smile.amazon.com/gp/product/B00TGIVRYU ). The Pi-Desktop is the only thing.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    Well, you don't need to connect the mSATA card into something else directly, you can plug it in via USB to another computer. This is covered in the user manual, as the SSD connects to the Pi in the Pi Desktop via USB, so to can it connect to another computer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to cstanton

    When I bought the Kinston SSH I expressed chose a SATA storage as I was having in home a number of recovered SATA-to-USB external powered boards from old HDD external boxes. These was heavy small boards to power externally 5 inches HDD with 5V 2A power supplies. This was to have a larger storage on the Raspberry PI old versions and the multi boot bit never had been mentioned.

     

    I also published an article on how to boot from SD card but using the external USB SATA connected HDD with the entire file system on it. The blog post (from 2015) is here: Meditech: RPI master storage system with some image of the first experimental tests while the disk setup procedure is here: Raspberry PI: USB hard disk boot

    As I saw none of the mechanical HDD was powered correctly by the PI including the 2.5 HDD declared as self-powered by the USB connector. Also today I use a couple of 3TB Western Digital USB HDD that work properly only if directly connected to the computer USB; if I use a HUB for these disks I should use a powered USB HUB else stability problems in data transfer still occurs.

     

    Seeing that the concept was working I bought a very low power consumption SSD Sata from my local retailer and a Startech SATA to USB connector supoprting both USB3 (full speed) and USB 2 on Amazon (https://www.amazon.es/gp/product/B00HJZJI84/ref=oh_aui_search_detailpage?ie=UTF8&psc=1 )

    Applying the settings mentioned above things worked fine. The PI was anyway booting from the SD card no longer stressed during the normal usage.

     

    Now with the introduction of the multi boot option settings in the PI3 things are working better and it was finally possible to remove the micro SD card.

     

    Just a note: as in terms of reliability an SSD is more durable than the SSD card thinking to make a device that should work for long time boxed (maybe to a client site) it is the worth to use this setup instead of the traditional one despite the advantage of a larger storage space for the file system with a cost of 50-60$

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    We might be misunderstanding each other. My card was a true mSATA, came with just the drive. No connectors/enclosures/etc. I connected to the hat, booted off SD, dd'd to the mSATA.

     

    So, I went on Amazon to get a connector. USB to SATA, then a card that converted SATA to mSATA. When I got it, I shut down the machine ready to take out the mSATA and put it into the adapter and run USB. I figured JUST for giggles I'd make sure one more time it didn't work. I already had the machine down, so I just pulled the SD card. Turned it on. Eventually got the 4 raspberrys, colorful screen, seemed to do that again, and finally booted Pixel. I shut down, restarted, and it seemed to be fine. Tried a few more times, worked. <SHRUG> Maybe I was too impatient the first time. But, the news is, I'm fine.

     

    Tuc

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tomgeorge
    0 tomgeorge over 9 years ago in reply to tuctboh

    For the record I too connected a mSATA SSD to the hat, found it was sda,

    downloaded Raspbian to the Raspberry Pi, dd it to /dev/sda  then

    followed the Raspberry Pi: USB: Hard Disk Boot instructions. Worked like

    a charm. df -h now shows /dev/root 230G 16G 202G 8% /

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adroadro
    0 adroadro over 6 years ago in reply to tuctboh

    Hi, i had the same problem…. now i have others haha, but in this respect i can tell you that the problem is that the mSata comes with NTFS partition, so the raspberry does not read that!!!

     

    Unfourtunelly!! But true... you must -i did-…. put the mSata in a carry with usb connection and format the mSata in a "FAT32" or "exFAT" format from your PC -i did it with win, any program Works-… and voilá! That's it!!! Your mSata Will be Reading by your Raspberry!!!

     

    Kind regards!!!

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • adroadro
    0 adroadro over 6 years ago in reply to tuctboh

    Hi, i had the same problem…. now i have others haha, but in this respect i can tell you that the problem is that the mSata comes with NTFS partition, so the raspberry does not read that!!!

     

    Unfourtunelly!! But true... you must -i did-…. put the mSata in a carry with usb connection and format the mSata in a "FAT32" or "exFAT" format from your PC -i did it with win, any program Works-… and voilá! That's it!!! Your mSata Will be Reading by your Raspberry!!!

     

    Kind regards!!!