Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum boot from ssd in pi desktop
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 73 replies
  • Answers 11 answers
  • Subscribers 715 subscribers
  • Views 12995 views
  • Users 0 members are here
  • raspberry_pi_space
Related

boot from ssd in pi desktop

gdenicolas
gdenicolas over 9 years ago

I couldnt find the file pidesktop.deb. The webpage is really complicated.

  • Sign in to reply
  • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    The SDCard isn't needed when booting from USB after the bit is set. The Pi prioritises booting from SDCard if it is inserted as well as the USB device.

     

    If you have only a USB bootable device inserted, and the SDCard removed, you don't have to change the location in /boot/cmdline.txt. It's probably best to set the bit before putting the Pi inside the enclosure.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    None of that was in any doco I received. image I actually got it all running by trial/error. I used a small SD card so don't care about its loss. But nice to have the deb for the extra RTC stuff.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    tuctboh

    You're right that it doesn't say which device it prioritises, though it does say on page 15 that the SD Card is no longer needed. Do you feel it should be explicitly stated to remove the SD Card ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to cstanton

    Christopher, my question is what is the method used to power-on again the Pi via a button after it has been powered off. I have an idea already applied in another case but sounds a bit "aged" ...

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tomgeorge
    0 tomgeorge over 9 years ago in reply to cstanton

    Several questions:

    1 gparted says my ssd card is not partitioned.  Should I partition it first or clone uCD card to SSD and then enlarge the partition?

    2. I did find and download pidesktop.deb. Is this the better way?

    3. Must the mCD card be removed to boot from the SSD?  Or can the 32 Gb mCD  be used for data?

    4. My current Debian desktop allows resetting the BIOS boot order so can have the boot sector on several hard drives and choose which to boot from. Is this possible? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to tomgeorge

    Hi Thomas,

     

    gparted says my ssd card is not partitioned.  Should I partition it first or clone uCD card to SSD and then enlarge the partition?

    None at all. Just format your ssd as Fat32 then when you create the image over it it is properly partitioned

    If you download and install the last Raspbian pixel image (I strongly suggest) at the first boot you see a screen saying that it is resizing the partition automatically. So no problem to enlarge the partition after.

    Anyway if the partition is not automatically resized it is one of the options of the command raspi-config

     

    I did find and download pidesktop.deb. Is this the better way?

    As the .deb extension of the file says, it is just a sort of program that I don't know but I can say for sure that it is not essential to the entire procedure. For now you can start ignoring it.

     

     

    Must the mCD card be removed to boot from the SSD?  Or can the 32 Gb mCD  be used for data?

     

    None at all image You should flash the SSD directly as it is a common micro SD card. No matter of the size (mine is 120 Giga). you should flash it with Etcher that is specific for this role, running on any platform (Linux, OSX and Windows). With this program you can flash any image on any external device. If Etcher refuses to flash your SSD as it is recognised as a HD instead of a external (removable) device, from the Etcher settings set the unsafe mode. Warning: in unsafe mode you can flash any img file also on your main pc hard disk so double check that you are selecting the correct device.

     

     

    My current Debian desktop allows resetting the BIOS boot order so can have the boot sector on several hard drives and choose which to boot from. Is this possible?

     

    As far as I know the process is specific for the Raspberry PI B3 that has a command supporting the boot device bit set changed from the microSD to a USB device (the SSD USB connected disk).

     

    For details and links take a look to my previous posts in this discussion.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to stone1343

    Thats fine. Thats what support sent me when I asked about it. I was making it available to people instead of having to beg/wait. But I certainly understand people being gun shy about downloading/using it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to tuctboh

    It's been posted up on here earlier: https://www.element14.com/community/docs/DOC-86805/l/pi-desktop-debian-file

     

    Update: Now with correct link!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    Yes, do think it would be useful. I think even more useful is telling you to install the "Type A to micro USB" *BEFORE* you put the lid on. I found I needed to pry the lid off (Whoever designed it meant for it NEVER to come off. image ) and press/lift the hat ever so slightly to get it to align JUST right. The 2nd time I put it together when I was testing things I ended up doing it outside the case so I could take out/put in the SD card... So it really is out of the case. Adds a nice blue glow to my work room

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to balearicdynamics

    Enrico Miglino wrote:

     

    Hi Thomas,

     

    gparted says my ssd card is not partitioned. Should I partition it first or clone uCD card to SSD and then enlarge the partition?

    None at all. Just format your ssd as Fat32 then when you create the image over it it is properly partitioned

     

    Formatting the SSD to Fat32 first isn't necessary though this can be a simpler way of allocating a drive letter to the device, and getting some software to acknowledge the device.

     

    If you're using Linux you can use the command 'dd' to write to the SSD with an image file, or from a microSD card. If you're using Windows then you can allocate a drive letter to the SSD and then do the same with software such as Win32DiskImager, or you don't need to assign a drive letter if you're using drive cloning software such as Norton Ghost.

     

    Also, https://www.raspberrypi.org/documentation/hardware/raspberrypi/bootmodes/usb.md alludes that the ability to set the required 'bit' for the Raspberry Pi to boot from USB is not limited to the Pi 3 and is capable on every model of Raspberry Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>