Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum photo frequency rate in picameraboardv2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 4 answers
  • Subscribers 708 subscribers
  • Views 1907 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
  • pics rate in picameraboardv2
Related

photo frequency rate in picameraboardv2

setcamerav2
setcamerav2 over 9 years ago

Hi,

what is the pictures (stills at 8mp resolution) rate for a picamera board v2 connected to RPI and taking only pictures (no other task).

Would it possible to shoot pictures at 8mp resolution at a rate of 2 pics per second for half an hour or so?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • fvan
    0 fvan over 9 years ago

    Hi,

     

    I don't know the supported rate, but you can easily try it out and verify the result.

     

    raspistill -o a%04d.jpg -t 1800000 -tl 500

     

    This command will take pictures for 30 minutes (-t) every 500ms (-tl).

     

    More info on https://www.raspberrypi.org/documentation/usage/camera/raspicam/timelapse.md

     

    Let us know how you get on!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 9 years ago in reply to fvan

    The rate will also depend if "Auto" is set on any of the settings.

     

    The answer will be interesting, but if you need almost continuous then video may be an option.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 9 years ago in reply to fvan

    The rate will also depend if "Auto" is set on any of the settings.

     

    The answer will be interesting, but if you need almost continuous then video may be an option.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to mcb1

    Mark, unfortunately I think no as - despite what is seems - it needs more process. If you capture video, frames are not a sequence of images but a video stream in some format (e.g. H264, MP4, etc. depending on the encoder you will use). The result is that after the very large storage you will use (half an hour or more) then you should extract just the frames you need and save them separately before deleting the video sequence. The other problem I see in this case is related to the very low frequency (2 fps) for the case of a video. Also on a professional machine for this kind of extra slow capture best practice suggest multiple shooting with stop motion techniques.

    In addition we should consider the resolution: a full HD video has a resolution of 2 MP while the image sensor resolution is 8 MP

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • setcamerav2
    0 setcamerav2 over 9 years ago in reply to balearicdynamics

    Thank you all very much!

     

    I do not have an RPI yet. I was asking just to know the capabilities of the processor.

    For example Gopro 4 can shoot time lapse photos at full resolution (12 Mp) at 1/2 second rate; each time calculating different exposure times and iso, I suppose. Yi cam can do that at a 2second rate.

    I am a complete newbie in computer.

    I would like to make a set of 6 cameraboards to take pano pictures, 360 deg x 180 deg.

    So, six RPIs and six cameraboards. I would need all the six cams to shoot at the same time. i.e. with a tolerable delay of 2 ms about, due to problems in scenes with moving objects

    I think I should use one RPi to send a command to shoot to all the others. But I have no idea if that is possible and, if yes, how.

     

    In general: how to connect some RPIs and use one to send a signal to the others to execute the same task at the same time.

     

    Thanks for any hints.

     

    Giuseppe