Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 7'' Touchscreen Display not powering on after energy failure
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 4 answers
  • Subscribers 704 subscribers
  • Views 9186 views
  • Users 0 members are here
  • ups-pico
  • touch screen
  • raspberry_pi
  • ras pi 3
Related

Raspberry Pi 7'' Touchscreen Display not powering on after energy failure

francisco.vaz
francisco.vaz over 9 years ago

I have recently bough this display Raspberry Pi 7'' Touchscreen Display and got it to work just fine. The touchscreen works, the image looks great and i can control it with the Python module rpi-backlight.

 

However I stumbled upon a problem that haven't been able to solve so far.

 

I'm setting up a kiosk that contains this display, a raspberry pi, a 3g modem and a ups (uninterruptible power supply). The ups module is used to power the raspberry and the 3g modem so that on a power failure, the kiosk can perform some operations, send some data through the 3g connection and perform an orderly shutdown. In case of a short (in time) power failure, the UPS module is smart enough not to shutdown the system.

 

The problem that I'm facing is that on a power failure as the monitor is not connected to the UPS, it will shutdown but when the power returns the monitor will not turn on again. The screen stays blank as in no image, no power, no backlight. To make the monitor work again I have to turn of the UPS system, power off the raspberry, power the display, and then power it on all again. If someone has a monitor like this it can replicate this problem by simply powering the monitor off and on again keeping the raspberry on.

 

After spending some time trying to solve this problem I learned that this monitor can receive I2C commands, however I been unable so far to find out the command codes and/or how to send it a "power on" command if it even exists.

The Python module rpi-backligh as the functionality to turn the monitor on and off which works great at start, but won't do anything after the monitor shutting down due to a power failure.

 

My setup is:

Raspberry Pi 3 Model B v1.2

Raspberry Pi 7'' Touchscreen Display

RPI SIM800 GSM/GPRS ADD-ON V2.0

UPS PIco HV3.0 - Uninterruptible Power Supply & I2C Control HAT

 

For OS I'm running Ubuntu MATE 16.04.

The OS is fully updated (sudo apt-get update, sudo apt-get dist-upgrade) as the raspberry firmware (rpi-update).

 

Does anyone have any idea of how to overcome this problem? Or a list of the I2C commands that this monitor can receive?

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to francisco.vaz

    Hi Francisco,

     

    No worries. I think I understand a bit more now. The red board is connected to the Pi so the UPS is powering the Pi during a failure scenario.

    You have two USB supplies connected; I can see a black cable going into the Pi, and a black cable going into the display board.

    So, you have no power at all to the display during the failure scenario.

     

    The red UPS board may not be able to power the Pi and the display, I don't know the specs of it. If it can, then you can run red and black wires from the 40-way connector 5V and GND pins respectively, from the top board (the 40-way connections are all wired through the boards sandwich) to the display board, and remove the USB connection from the display board. You probably need to confirm with the source of the red board, if it was tested with such conditions (i.e. with display, and with glitches and possibly varying voltage briefly). Anyway it is worth a try.

    If that doesn't work, it may be best to look for a different UPS solution that can handle the display and the Pi, if a software solution to perform a reset of the display cannot be found.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to fvan

    Sorry our comments crossed at the same time, yes exactly as you describe!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fvan
    0 fvan over 9 years ago in reply to shabaz

    Good to see we arrived at the same solution image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • francisco.vaz
    0 francisco.vaz over 9 years ago in reply to fvan

    That diagram is almost accurate, the only mistake is that the top 5V connects directly to the raspberry and not to the UPS. The UPS is then powered by the raspberry GPIOs.

    Powering the display directly from the GPIOs solves the issued and for now it's a good enough solution however as expected, on a black out, the battery drainage is pretty high and I don't know if it will hold the system on enough time to perform all the tasks it needs. I will perform some tests now and will get back here with the results.

     

    Thank you all for your inputs image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fagould4525
    0 fagould4525 over 8 years ago in reply to francisco.vaz

    @Franciso, good to see you solved your display power problem and sorry to see you didn't get the answer about powering off the RPi. I have the same question as to why the RPi does not power off. If you have found a solution, would you share it? I'm running Ubuntu Mate 18.04 and it doesn't power off the RPi even when configured for pi-top power off control.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<