Is the Logi-Pi board still going to be offered as a product? If so, is there an estimate on availability?
Thx
Is the Logi-Pi board still going to be offered as a product? If so, is there an estimate on availability?
Thx
Is this what you're after?
If so then:
Availability: 2
UK Farnell.com Availability (Product).
Availability: 67
Available until stock is exhausted
That is the product I'm looking for, but I was looking on the US site:
which states: "No Longer Manufactured". The European site says: Available until stock is exhausted
So, is this going to continue to be a product? There's no info on the Valent site to say the current status. I don't want to pursue development on this board if it's not going to be available later.
Is Valent perhaps working on a replacement? An FPGA board for the RPi with a Lattice chip would be sweet...
Thanks for the reply!
You're welcome.
Sorry I can't be of any more help - you're right, the US Newark site does indeed say that.
Is it a viable option to get it shipped from the UK / Europe?
dan luttrell wrote:
So, is this going to continue to be a product? There's no info on the Valent site to say the current status. I don't want to pursue development on this board if it's not going to be available later.
Is Valent perhaps working on a replacement? An FPGA board for the RPi with a Lattice chip would be sweet...
I don't want to speak for ValentF(x), but it sure looks to me like LOGI-Pi is at end-of-life.
There are lots FPGA boards out there. Joel Williams has done a remarkable job of maintaining his Cheap FPGA Development Boards site, which has boards from many vendors. For Lattice iCE40, there's a good list at the bottom of the IceStorm Project home page.
There aren't many boards that plug directly into a RasPi. There actually is a Lattice iCE40 8K board called icoBoard but it's only available in Germany and costs at least 69 euros. XESS has a RasPi adapter for their XULA boards but the FPGA board itself is expensive (it's a large FPGA) and you don't get many I/Os. For a while it looked like XESS was going to have the iCE40-based CAT board but that seems to have fizzled.
For Lattice iCE40 I think your cheapest way to get started is still the iCEstick if you can find a suitable vendor. Olimex has a nice little board with a 1K part and SRAM for around US$26 at Digi-Key. However, it doesn't have a programmer. Lattice iCE40blink boards bring out lots of I/O.
I do FPGAs professionally so I have lots of boards, mostly Xilinx and iCE40. While I have LOGI-Pi, I rarely use it with a RasPi. Instead, I program it over JTAG using an Adafruit FT232H breakout board as a cheap USB JTAG dongle. USB is my favorite way to talk to pretty much any hardware I'm playing with. Then it doesn't matter which machine I'm using as a host.
What sort of tasks do you have in mind for the FPGA, or to put it another way, if you were using a Lattice part which one would you go for.
I'm asking with a view to suggesting a Lattice board that might easily interface to a Pi.
MK
dan luttrell wrote:
So, is this going to continue to be a product?
I recently ran into a product where Farnell says: "no longer manufactured", but Mouser and digikey still have it! On closer inspection the "manufacturer order code" at farnell says it is "version B" and the others now carry "version C" of that same chip. This manufacturer is sometimes a bit dumb in choosing type numbers and this probably caused Farnell not to realize that there simply is "the same chip but a different version".... So the thing to learn from this is: As a manufacturer: do not include the version identifier into the order code.
And another thing to take away from this is to take the "no longer manufactured" from Farnell/newark with a grain of salt....
dan luttrell wrote:
So, is this going to continue to be a product?
I recently ran into a product where Farnell says: "no longer manufactured", but Mouser and digikey still have it! On closer inspection the "manufacturer order code" at farnell says it is "version B" and the others now carry "version C" of that same chip. This manufacturer is sometimes a bit dumb in choosing type numbers and this probably caused Farnell not to realize that there simply is "the same chip but a different version".... So the thing to learn from this is: As a manufacturer: do not include the version identifier into the order code.
And another thing to take away from this is to take the "no longer manufactured" from Farnell/newark with a grain of salt....