Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Only getting output from left speaker
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 577 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
  • speaker
Related

Only getting output from left speaker

amit.kucheria
amit.kucheria over 9 years ago

Hi,

 

I have the cirrus logic version of the card (Ver A1.01). Headphone output works fine but I recently decided to wire it up directly to a pair of speakers to have a standalone music player. However, only one channel (Left) seems to be working. I've swapped speakers to confirm that it isn't the speakers or the cables.

 

Anybody have ideas on what could be broken? The speaker circuit in the schematics seem simple enough with a CA04F2FT5AUD010G voltage suppressor in line with the output. I'm looking for ideas on where I should go about looking for problems on the board.

 

Regards,

Amit

  • Sign in to reply
  • Cancel
Parents
  • marcelheijkoop
    0 marcelheijkoop over 8 years ago

    I do use the speaker out too . If you use the alsa controls manually , it is easy to make a mistake and forget to open up both channels.

    Use the scripts from Hias, and it should work.

    Using speaker out means you probably also soldered some pins in the board, double check the soldering for any shorts or visible damage.

    As the output stage of the D-amp uses an H bridge , you can not combine any wires from the channels.

    Last resort could be to test with an image I have running here.

    ( or bring the te card here to test it in my setup )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • marcelheijkoop
    0 marcelheijkoop over 8 years ago

    I do use the speaker out too . If you use the alsa controls manually , it is easy to make a mistake and forget to open up both channels.

    Use the scripts from Hias, and it should work.

    Using speaker out means you probably also soldered some pins in the board, double check the soldering for any shorts or visible damage.

    As the output stage of the D-amp uses an H bridge , you can not combine any wires from the channels.

    Last resort could be to test with an image I have running here.

    ( or bring the te card here to test it in my setup )