Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Modbus Protocol on Raspberry Pi 3 using Serial GPIO Ports
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 3 answers
  • Subscribers 705 subscribers
  • Views 4491 views
  • Users 0 members are here
  • modbus rtu
  • raspberry_pi
  • modbus over serial
  • raspberry pi 3
Related

Modbus Protocol on Raspberry Pi 3 using Serial GPIO Ports

patil.sunny9999
patil.sunny9999 over 8 years ago

Hello There,

I want to make use of Modbus Protocol on my Raspberry pi 3 model B. I am Complete Beginner. After some Research i Found Some information about Modbus Protocol. i found these Libraries by which i can Use Modbus Protocol on Raspberry pi.

LIBMODBUS

PYMODBUS

MODBUS-TK

Please Suggest me that which one will be better to use.

 

As I have to communicate with MODSCAN 32 using my Raspberry Pi by RS232 circuitry, i have bought one

so I am quite sure that I need to make Raspberry Pi as SLAVE device. Because I am little confused with that please help me out.

Also Please Provide if any sample code is available to you, it will help me alot to understand better.

 

Thank you in advance

 

 

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago

    Hi there, I have a better suggestion image, try using Node-Red and the Modbus plugin, if you are a beginner then this I think will be an easier route to go, I have loads of Node-Red videos on my channel and alot of them use Modbus to talk to a thermal imaging camera and other devices

     

    Node Red is included with the Raspberry PI image and it is easy to add the Modbus plugin right from within Node-Red UI, look for the pallet manager. The plugin makes it so much easier to talk to modbus devices and node-red will allow easily to configure workflows and displays without the need for extensive coding. You can code stuff if you want but I would suggest getting to know Modbus first and then go from there.

     

    If you need help with Modbus I can help, I just have never needed to use the python interfaces.

     

    Regards

    peter

     

    Oh, my channel is https://www.youtube.com/thebreadboardca

     

    If necessary i will create a video for E14 and post it here to help, I have many devices I can choose from

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago

    Hi there, I have a better suggestion image, try using Node-Red and the Modbus plugin, if you are a beginner then this I think will be an easier route to go, I have loads of Node-Red videos on my channel and alot of them use Modbus to talk to a thermal imaging camera and other devices

     

    Node Red is included with the Raspberry PI image and it is easy to add the Modbus plugin right from within Node-Red UI, look for the pallet manager. The plugin makes it so much easier to talk to modbus devices and node-red will allow easily to configure workflows and displays without the need for extensive coding. You can code stuff if you want but I would suggest getting to know Modbus first and then go from there.

     

    If you need help with Modbus I can help, I just have never needed to use the python interfaces.

     

    Regards

    peter

     

    Oh, my channel is https://www.youtube.com/thebreadboardca

     

    If necessary i will create a video for E14 and post it here to help, I have many devices I can choose from

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • fed27
    0 fed27 over 5 years ago in reply to Robert Peter Oakes

    Hi Peter

     

    i have been using a raspberry pi and node red for modbus communications with PLCs for a while now, but I have only ever done it over TCP modbus.

    I now need to do the same but over modbus serial, we are trying not to use a hat as we might want them in future for other reasons.

    so that means I really need to use a USB modbus plug in device which I have various. I just can’t seem to set up the pi and node red to read modbus  through the USB adaptor.

     

    Please anyone who has done this successfuly before HELP.