Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How to update date and Time in Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 709 subscribers
  • Views 25040 views
  • Users 0 members are here
  • raspberry_pi
Related

How to update date and Time in Raspberry Pi

sameermp
sameermp over 8 years ago

I have purchased a Raspberry Pi 3 model B in August 2017. I am unable to set up Date and Time. Every time I turn on the hardware, It shows date - 12 April  2017.

I have tried setting it up with  Sudo raspi-config but could not do it.

Please guide me on the procedure.

Thanks.

  • Sign in to reply
  • Cancel
  • rew
    0 rew over 8 years ago

    The raspberry pi does not have the hardware to keep track of the date and time when it is turned off. It therefore tries to get the time from the network whenever it boots. I'm guessing you don't have an internet connection when the pi starts back in april.....

    You could have bought a PC for about 1000 euros. but you bought a raspberry pi for 40. There are some compromises.

    I haven't run into this problem for ages: Apparently the assumption: "you often have an internet connection" works for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gdstew
    0 gdstew over 8 years ago

    Here is an example of the date command which can be used to set the time/date if the Raspberry Pi is not connected to the internet:

     

    #sudo date --set='TZ="America/Chicago" 8 Oct 2017 14:32'

     

    Note that the use of the "nornal" backward ticks after --set= and at the end of the command are required to keep the shell (bash) from

    misinterpreting special characters in the command line.

     

    The time zone (TZ=) will have to be set according to where you are of course and the time is in 24 hour format.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sameermp
    0 sameermp over 8 years ago in reply to gdstew

    My Raspberry Pi is connected to internet via wifi. Even after setting the proper timezone and country, I does not update the time and date.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • adams_l
    0 adams_l over 8 years ago in reply to sameermp

    Maybe your router settings do not like Network Time Protocol (ntp).

     

    To disable ntp and manually update the time instead:

    'sudo update-services ntpd disable'

    and then

    'sudo apt-get install ntpdate'.

     

    Then you can update the date and time manually with

    'sudo ntpdate'

    or you can specify a timeserver like

    'sudo ntpdate pool.ntp.org'

     

    To set the time at boot, add 'ntpdate' to rc.local.

    If you want automatic updates, you could add 'ntpdate' as a cron job.

     

    --WLAJ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 8 years ago in reply to adams_l

    As far as I know, the raspberry already does the equivalent of

    sudo ntpdate pool.ntp.org

    at boot. That's the "sets the time from the network".

     

    I would suggest that instead of manually entering the time, you try this sudo ntpdate command manually first to see if it works for you. Only when it works is it useful to invest time in making such changes permanent (i.e. happen automatically on the next boot).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to sameermp

    Is the Raspbian ntp package installed?

    Check: dpkg -l ntp

     

    You should see something like this as output:

     

    ii  ntp            1:4.2.8p10+d amd64        Network Time Protocol daemon

     

    If not, do this:

    sudo apt -y install ntp

     

    That will get you network time automatically.  No manual intervention required.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ahmeqas
    0 ahmeqas over 6 years ago

    If nothing works for updating the time or date in your raspberry pi, as I have experienced, we can set the date and time manually. Visit Setting the Date & Time manually in a Raspbian Headless Setup on Raspberry Pi guide.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aswinvenu
    0 aswinvenu over 6 years ago

    Hi Sameer,

     

      Raspberry Pi doesn't have an RTC ( Real time clock) built in to the board due to multiple reasons. Instead they update the time through network using NTP (Network Time Protocol ). But in your case if Pi is not connected to internet then it is not possible for RPi to update the date and time after the reboot.

      Linux Kernel supports RTCs through SPI and I2C buses. So one option for you is to add an external RTC with a battery Attached. RTCs needs to be powered to keep the time and date upto date ( Generally using a dedicated button cell 2032).

    For example you can use DS1307 based solution.

     

    Please take a look this blog post on adding RTC to Rpi.

    https://learn.adafruit.com/adding-a-real-time-clock-to-raspberry-pi

    You can buy it from here:

    https://in.element14.com/adafruit-industries/264/rtc-breakout-board-kit-ds1307/dp/2215027?ost=DS1307+board

     

    Hope this helps.

    Regards,

    Aswin

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mikeburch
    0 mikeburch over 5 years ago in reply to e14 Contributor

    This worked perfectly for me using Twister.  Thank you!   Greetings from Arizona.