Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cameras not detected! vcgencmd get_camera outputs supported=2, detected=0 in cm3 with emmc flash
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 704 subscribers
  • Views 950 views
  • Users 0 members are here
  • troubleshooting
  • raspberry_pi
  • commfeedback
  • cm3
  • picam
Related

Cameras not detected! vcgencmd get_camera outputs supported=2, detected=0 in cm3 with emmc flash

r2work
r2work over 8 years ago

Hi,I am new to raspberry pi compute module.

I was working with the cm3 lite before this with a full desktop version installed and hence had no problems with the camera modules.

Since my cm3 lite got short i have to use the cm3 with flash memory which has the jessie lite version installed.

I did the procedure in the rpi in order to support dual cameras and hopefully succeeded with the blob files. I have connected the gpio pins for the camera setup as given in the tutorial

https://www.raspberrypi.org/documentation/hardware/computemodule/cmio-camera.md

 

I reboot the pi and i run the command vcgencmd version which outputs

 

Nov  3 2017 17:05:40

Copyright (c) 2012 Broadcom

version 1bcf9152e3b2ab5c67dcb9c7c1f6d9256d9a6f38 (clean) (release)

 

then, i ran vcgencmd get_camera which outputs

 

supported=2, detected=0

 

shows that the blob files are right.

To check the gpio pins i ran sudo raspi-gpio get and found that the raspi-gpio package was not installed as I was using the lite version. Then I installed it using sudo apt-install raspi-gpio

 

And now, sudo raspi-gpio get outputs

 

[code]BANK0 (GPIO 0 to 27):

  GPIO 00: level=0 fsel=0 alt=  func=INPUT

  GPIO 01: level=0 fsel=0 alt=  func=INPUT

  GPIO 02: level=0 fsel=1 alt=  func=OUTPUT

  GPIO 03: level=0 fsel=1 alt=  func=OUTPUT

  GPIO 04: level=0 fsel=0 alt=  func=INPUT

  GPIO 05: level=0 fsel=0 alt=  func=INPUT

  GPIO 06: level=0 fsel=0 alt=  func=INPUT

  GPIO 07: level=0 fsel=0 alt=  func=INPUT

  GPIO 08: level=0 fsel=0 alt=  func=INPUT

  GPIO 09: level=0 fsel=0 alt=  func=INPUT

  GPIO 10: level=0 fsel=0 alt=  func=INPUT

  GPIO 11: level=0 fsel=0 alt=  func=INPUT

  GPIO 12: level=0 fsel=0 alt=  func=INPUT

  GPIO 13: level=0 fsel=0 alt=  func=INPUT

  GPIO 14: level=0 fsel=4 alt=0 func=TXD0

  GPIO 15: level=0 fsel=4 alt=0 func=RXD0

  GPIO 16: level=0 fsel=0 alt=  func=INPUT

  GPIO 17: level=0 fsel=0 alt=  func=INPUT

  GPIO 18: level=0 fsel=0 alt=  func=INPUT

  GPIO 19: level=0 fsel=0 alt=  func=INPUT

  GPIO 20: level=0 fsel=0 alt=  func=INPUT

  GPIO 21: level=0 fsel=0 alt=  func=INPUT

  GPIO 22: level=0 fsel=0 alt=  func=INPUT

  GPIO 23: level=0 fsel=0 alt=  func=INPUT

  GPIO 24: level=0 fsel=0 alt=  func=INPUT

  GPIO 25: level=0 fsel=0 alt=  func=INPUT

  GPIO 26: level=0 fsel=0 alt=  func=INPUT

  GPIO 27: level=0 fsel=0 alt=  func=INPUT

BANK1 (GPIO 28 to 45):

  GPIO 28: level=0 fsel=4 alt=0 func=SDA0

  GPIO 29: level=0 fsel=4 alt=0 func=SCL0

  GPIO 30: level=0 fsel=1 alt=  func=OUTPUT

  GPIO 31: level=0 fsel=1 alt=  func=OUTPUT

  GPIO 32: level=0 fsel=0 alt=  func=INPUT

  GPIO 33: level=0 fsel=0 alt=  func=INPUT

  GPIO 34: level=0 fsel=0 alt=  func=INPUT

  GPIO 35: level=0 fsel=0 alt=  func=INPUT

  GPIO 36: level=0 fsel=0 alt=  func=INPUT

  GPIO 37: level=0 fsel=0 alt=  func=INPUT

  GPIO 38: level=0 fsel=0 alt=  func=INPUT

  GPIO 39: level=0 fsel=0 alt=  func=INPUT

  GPIO 40: level=0 fsel=0 alt=  func=INPUT

  GPIO 41: level=0 fsel=0 alt=  func=INPUT

  GPIO 42: level=0 fsel=0 alt=  func=INPUT

  GPIO 43: level=0 fsel=0 alt=  func=INPUT

  GPIO 44: level=0 fsel=0 alt=  func=INPUT

  GPIO 45: level=0 fsel=0 alt=  func=INPUT

BANK2 (GPIO 46 to 53):

  GPIO 46: level=1 fsel=0 alt=  func=INPUT

  GPIO 47: level=1 fsel=0 alt=  func=INPUT

  GPIO 48: level=0 fsel=4 alt=0 func=SD0_CLK

  GPIO 49: level=1 fsel=4 alt=0 func=SD0_CMD

  GPIO 50: level=1 fsel=4 alt=0 func=SD0_DAT0

  GPIO 51: level=1 fsel=4 alt=0 func=SD0_DAT1

  GPIO 52: level=1 fsel=4 alt=0 func=SD0_DAT2

  GPIO 53: level=1 fsel=4 alt=0 func=SD0_DAT3[/code]

 

and the my dt-blob-dualcam.dts file consists of the following,

 

dts-v1/;

 

/ {

  videocore {

 

    pins_cm {

 

      pin_config {

 

        pin@default {

          polarity = "active_high";

          termination = "pull_down";

          startup_state = "inactive";

          function = "input";

        }; // pin

 

        // BANK 0 - USER GPIO //

        pin@p0  { function = "input";   termination = "pull_up";    }; // GPU WILL USE THIS PIN FOR CAMERA 0 I2C0 SDA

        pin@p1  { function = "input";   termination = "pull_up";    }; // GPU WILL USE THIS PIN FOR CAMERA 0 I2C0 SCL

        pin@p2  { function = "output";  termination = "no_pulling"; }; // GPU WILL USE THIS PIN FOR CAMERA 0 LED

        pin@p3  { function = "output";  termination = "no_pulling"; }; // GPU WILL USE THIS PIN FOR CAMERA 0 SHUTDOWN

        pin@p4  { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p5  { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p6  { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p7  { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p8  { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p9  { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p10 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p11 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p12 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p13 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

///////////////////////////////////////////

// TO ENABLE UART0 UNCOMMENT THESE 2 LINES:

//       pin@p14 { function = "uart0";   termination = "no_pulling"; }; // UART0 TX

//       pin@p15 { function = "uart0";   termination = "pull_up";    }; // UART0 RX

// AND COMMENT OUT/REMOVE THESE 2 LINES:

        pin@p14 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p15 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

///////////////////////////////////////////

        pin@p16 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p17 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p18 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p19 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p20 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p21 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p22 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p23 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p24 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p25 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p26 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p27 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

 

        // BANK 1 - USER GPIO//

        pin@p28 { function = "input";   termination = "pull_up";    }; // GPU WILL USE THIS PIN FOR CAMERA 1 I2C0 SDA

        pin@p29 { function = "input";   termination = "pull_up";    }; // GPU WILL USE THIS PIN FOR CAMERA 1 I2C0 SCL

        pin@p30 { function = "output";  termination = "no_pulling"; }; // GPU WILL USE THIS PIN FOR CAMERA 1 LED

        pin@p31 { function = "output";  termination = "no_pulling"; }; // GPU WILL USE THIS PIN FOR CAMERA 1 SHUTDOWN

        pin@p32 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p33 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p34 { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p35 { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p36 { function = "input";   termination = "pull_up";    }; // DEFAULT STATE

        pin@p37 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p38 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p39 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p40 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p41 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p42 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p43 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE

        pin@p44 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE WAS INPUT NO PULL

        pin@p45 { function = "input";   termination = "pull_down";  }; // DEFAULT STATE WAS INPUT NO PULL

 

        // BANK 2 - DON'T TOUCH UNLESS YOU KNOW WHAT YOU'RE DOING //

        pin@p46 { function = "input";   termination = "no_pulling"; drive_strength_mA = <8>; polarity = "active_high"; }; // HPD_N

        pin@p47 { function = "output";  termination = "no_pulling"; drive_strength_mA = <8>; polarity = "active_low"; startup_state = "active"$

        pin@p48 { function = "sdcard";  termination = "pull_up";    drive_strength_mA = <8>; }; // SD CLK

        pin@p49 { function = "sdcard";  termination = "pull_up";    drive_strength_mA = <8>; }; // SD CMD

        pin@p50 { function = "sdcard";  termination = "pull_up";    drive_strength_mA = <8>; }; // SD D0

pin@p51 { function = "sdcard";  termination = "pull_up";    drive_strength_mA = <8>; }; // SD D1

        pin@p52 { function = "sdcard";  termination = "pull_up";    drive_strength_mA = <8>; }; // SD D2

        pin@p53 { function = "sdcard";  termination = "pull_up";    drive_strength_mA = <8>; }; // SD D3

 

      }; // pin_config

 

      pin_defines {

        pin_define@EMMC_ENABLE {

           type = "internal";

           number = <47>;

        };

 

        pin_define@NUM_CAMERAS {

          type = "internal";

          number = <2>;

        };

        pin_define@CAMERA_0_LED {

          type = "internal";

          number = <2>;

        };

pin_define@CAMERA_0_SHUTDOWN {

          type = "internal";

          number = <3>;

        };

        pin_define@CAMERA_0_UNICAM_PORT {

          type = "internal";

          number = <1>;

        };

        pin_define@CAMERA_0_I2C_PORT {

          type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_0_SDA_PIN {

          type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_0_SCL_PIN {

          type = "internal";

          number = <1>;

        };

pin_define@CAMERA_1_LED {

          type = "internal";

          number = <30>;

        };

        pin_define@CAMERA_1_SHUTDOWN {

          type = "internal";

          number = <31>;

        };

        pin_define@CAMERA_1_UNICAM_PORT {

          type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_1_I2C_PORT {

          type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_1_SDA_PIN {

          type = "internal";

          number = <28>;

        };

pin_define@CAMERA_1_SCL_PIN {

          type = "internal";

          number = <29>;

        };

      }; // pin_defines

 

    }; // pins_cm

 

 

    pins_cm3 {

 

      pin_config {

 

        pin@default {

          polarity = "active_high";

          termination = "pull_down";

          startup_state = "inactive";

          function = "input";

        }; // pin

pin@p0  { function = "input";  termination = "pull_up";    }; // CAMERA 0 I2C0 SDA

        pin@p1  { function = "input";  termination = "pull_up";    }; // CAMERA 0 I2C0 SCL

        pin@p2  { function = "output"; termination = "no_pulling"; }; // CAMERA 0 LED

        pin@p3  { function = "output"; termination = "no_pulling"; }; // CAMERA 0 SHUTDOWN

        pin@p14 { function = "uart0";  termination = "no_pulling"; drive_strength_mA = < 8 >; }; // TX uart0

        pin@p15 { function = "uart0";  termination = "pull_up"; drive_strength_mA = < 8 >; }; // RX uart0

        pin@p28 { function = "input";  termination = "pull_up";    }; // CAMERA 1 I2C0 SDA

        pin@p29 { function = "input";  termination = "pull_up";    }; // CAMERA 1 I2C0 SCL

        pin@p30 { function = "output"; termination = "no_pulling"; }; // CAMERA 1 LED

        pin@p31 { function = "output"; termination = "no_pulling"; }; // CAMERA 1 SHUTDOWN

        pin@p46 { function = "input";  termination = "pull_up";    }; // SMPS_SCL

        pin@p47 { function = "input";  termination = "pull_up";    }; // SMPS_SDA

        pin@p48 { function = "sdcard"; termination = "pull_up";    drive_strength_mA = < 8 >; }; // SD CLK

        pin@p49 { function = "sdcard"; termination = "pull_up";    drive_strength_mA = < 8 >; }; // SD CMD

        pin@p50 { function = "sdcard"; termination = "pull_up";    drive_strength_mA = < 8 >; }; // SD D0

        pin@p51 { function = "sdcard"; termination = "pull_up";    drive_strength_mA = < 8 >; }; // SD D1

        pin@p52 { function = "sdcard"; termination = "pull_up";    drive_strength_mA = < 8 >; }; // SD D2

        pin@p53 { function = "sdcard"; termination = "pull_up";    drive_strength_mA = < 8 >; }; // SD D3

        pin@p128 { function = "input";  termination = "no_pulling"; polarity = "active_low"; }; // Hotplug

        pin@p129 { function = "output"; termination = "no_pulling"; polarity = "active_low"; }; // EMMC_ENABLE_N

}; // pin_config

 

      pin_defines {

        pin_define@HDMI_CONTROL_ATTACHED {

           type = "external";

           number = <0>;

        };

        pin_define@EMMC_ENABLE {

           type = "external";

           number = <1>;

        };

        pin_define@POWER_LOW {

           type = "absent";

        };

        pin_define@LEDS_DISK_ACTIVITY {

           type = "absent";

        };

        pin_define@LAN_RUN {

           type = "absent";

        };

pin_define@SMPS_SDA {

           type = "internal";

           number = <46>;

        };

        pin_define@SMPS_SCL {

           type = "internal";

           number = <47>;

        };

        pin_define@ETH_CLK {

           type = "absent";

        };

        pin_define@WL_LPO_CLK {

           type = "absent";

        };

        pin_define@USB_LIMIT_1A2 {

           type = "absent";

        };

        pin_define@SIO_1V8_SEL {

           type = "absent";

        };

pin_define@PWML {

           type = "absent";

        };

        pin_define@PWMR {

           type = "absent";

        };

        pin_define@SAFE_MODE {

           type = "absent";

        };

        pin_define@SD_CARD_DETECT {

           type = "absent";

        };

        pin_define@ID_SDA {

           type = "absent";

        };

        pin_define@ID_SCL {

           type = "absent";

        };

 

        pin_define@NUM_CAMERAS {

type = "internal";

          number = <2>;

        };

        pin_define@CAMERA_0_LED {

          type = "internal";

          number = <2>;

        };

        pin_define@CAMERA_0_SHUTDOWN {

          type = "internal";

          number = <3>;

        };

        pin_define@CAMERA_0_UNICAM_PORT {

          type = "internal";

          number = <1>;

        };

        pin_define@CAMERA_0_I2C_PORT {

          type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_0_SDA_PIN {

  type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_0_SCL_PIN {

          type = "internal";

          number = <1>;

        };

        pin_define@CAMERA_1_LED {

          type = "internal";

          number = <30>;

        };

        pin_define@CAMERA_1_SHUTDOWN {

          type = "internal";

          number = <31>;

        };

        pin_define@CAMERA_1_UNICAM_PORT {

          type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_1_I2C_PORT {

type = "internal";

          number = <0>;

        };

        pin_define@CAMERA_1_SDA_PIN {

          type = "internal";

          number = <28>;

        };

        pin_define@CAMERA_1_SCL_PIN {

          type = "internal";

          number = <29>;

        };

      }; // pin_defines

 

    }; // pins_cm3

 

  };

 

};

 

In my /boot/config.txt file, i set the dt_param=12C=on to off mode.

I tried rebooting my pi but still couldn't figure out the problem as it still persists.

I found out some i2c issue with cm3 with emmc flash as in the given link,

https://www.element14.com/community/thread/61298/l/weird-i2c-issue-with-pi-cm3-solved?displayFullThread=true

but, could this be a problem?

Could somebody please help? image