Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rrechargeable AA batteries for pi portable?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 1440 views
  • Users 0 members are here
  • batteries
  • rechargeable batteries
  • portable
  • pi
  • aa
  • raspberyy pi
Related

Rrechargeable AA batteries for pi portable?

vinceverc
vinceverc over 8 years ago

Hello guys, i have a very basic understanding of electronics, but don't know much about batteries. So i figured, why not ask element 14's community?

I want to make a raspberry pi portable, and already have some stuff set up.

I am using a raspberry pi model B (yes i am using the rbp 1). And a cheap screen, this is like a 5" screen i got from a Chinese website, it uses around 515 mA when in use. Now i am using retropie and have made a controller that i connected to the gpio pins, i used pigrll (i don't remember the name exactly, it was code from adafruit). Now, as far as i remember the pi uses +- 500mA, this means that this device will use more than 1A. The problem i have is that I need to power this device with some sort of battery. I first thought of a cheap power bank, but the trouble is that most of them can only deliver 1 amp, and i once took one apart, (to use in another project) and accidentally stabbed the battery! This is why i would not like to use one of those again. So I thought, why not use some rechargeable AA batteries, i was thinking of buying four, 1200mAh generic batteries and using these. I was thinking about using two in parallel and two in series. And use a buck/boost converter to bump the voltage up to 5 volts.When i want to charge them, i just take them out and stick the batteries in one of those chargers. There are a couple of reasons i want to use this approach. I am rather scared of using other batteries with custom charging circuits and so on, apart from that, the adafruit ones are hard to buy here. Now, i did some research and found out that the voltage of these batteries drops but apparently the raspbery pi can actually use voltages as low as three volts, only the usb devices won't work, but that is no problem, as i won't use any.

My question is whether this is a good idea, and whether these batteries have auto cut-off to pretend over dischagre.

 

Kind regards,

Vincent

  • Sign in to reply
  • Cancel
Parents
  • genebren
    0 genebren over 8 years ago

    This a pretty interesting idea.  I would recommend trying something in a little larger format than AA.  I use a lot of li-ion in an 18650 size (larger than aa).  They come several different capacities (up to ~10000mAh).  You can also get multi-cell chargers for this format.  Given the 4.2V to 2.5V range, if they are in series, you might not need a boost at all. Or you could just run them in parallel (with schottky didodes) and then boost them to 5.0V.

     

    This should work well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vinceverc
    0 vinceverc over 8 years ago in reply to genebren

    Thank you for the quick response, so would this work with just the AA batteries and not the larger 18650 ones? And the schottky diodes, how should i use them? could i just use normal ones? (sorry i don't know alot about electronics.) And how about over discharge?

    Sorry for the many questions.

     

    Kind regards,

    Vincent

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 8 years ago in reply to vinceverc

    Sure, as Gerrit points out, AA battery would work fine.

     

    The schottky diodes would have been used, in series with each battery, to the common power to the boost circuit, to prevent current flows between cells. Schottky diodes are used do to their much lower forward voltage drops, so that more voltage reached the boost circuit.  To prevent the over discharge, the simplest method is to use voltage detector IC (2.5v) to enable the boost circuit, cutting off battery current flow when the batteries are too low.

     

    This is a proven technique that has been used in several commercial products.

     

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • genebren
    0 genebren over 8 years ago in reply to vinceverc

    Sure, as Gerrit points out, AA battery would work fine.

     

    The schottky diodes would have been used, in series with each battery, to the common power to the boost circuit, to prevent current flows between cells. Schottky diodes are used do to their much lower forward voltage drops, so that more voltage reached the boost circuit.  To prevent the over discharge, the simplest method is to use voltage detector IC (2.5v) to enable the boost circuit, cutting off battery current flow when the batteries are too low.

     

    This is a proven technique that has been used in several commercial products.

     

    Gene