Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Loud buzz on Raspberry Pi Audio Jack
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 4 answers
  • Subscribers 707 subscribers
  • Views 8484 views
  • Users 0 members are here
  • audio
  • hdmi
  • audio jack
  • buzz
  • raspberry_pi
  • raspberry pi
  • dvi
Related

Loud buzz on Raspberry Pi Audio Jack

ntewinkel
ntewinkel over 8 years ago

Hello,

 

I'm hoping someone might have the answer to this issue I'm having with my Kitty TV Raspberry Pi.

 

I have the Raspberry Pi (version 2, B+) connected to an old monitor via an HDMI cable connected to an HDMI-DVI adapter to the monitor, for video only.

The audio is supposed to go separately through the 3.5mm audio jack to the external speakers.

 

I tried two different (HDMI-DVI) adapters, and 2 different cables. I even tried using an external USB adapter, and the buzz even came through the 3.5mm jack on that adapter!

 

I also tried the Raspberry Pi 3, with the same result.

 

The kicker is, this was working at one point and the sound was perfect!

 

The sound issue happens regardless of what the Pi is doing - just showing the desktop it does that, and when using omxplayer to play the videos it also does that same buzz.

 

It's been a while since I last had it working, so I don't remember what changed.

I don't recall if I did an update, or if it was the Raspberry Pi 1 I was using at that time. The Pi 1 is now the sprinkler controller, so I don't really want to tear that apart to try that out.

 

I did try a few things in settings - forcing it to use audio out, and not hdmi, for example.

 

Here is a video showing the issue, and how it does not buzz when HDMI is not connected.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I'll try it on the bedroom TV next to see if it works when using audio through HDMI.

edit: The audio works on the TV through the direct HDMI connection, using the TV speakers. However, the audio jack is still giving the same buzzing sound. So it's not the HDMI-DVI that's the issue.

ps, those speakers work beautifully when connected to my iPhone. Using a headset I also hear the audio buzz. So it's not a bad connection or bad speakers.

 

edit:

This post from fall 2016 says it was the Raspberry Pi 2 I was using, so that's the same board I'm using now: Videos For Cats, on a Raspberry Pi

 

edit:

ps, the other thing I tried was to grab a brand new image off raspberrypi.org, but that didn't work. This is Raspbian Stretch. Previous one was Raspbian Jesse, which also had the buzz.

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Nico!

     

    That's a common problem, and not always easy to totally eliminate with wiring alone, but basically some current is flowing through wires with resistance (that are normally expected to be considered at 0V all along the wire), and that is causing the buzzing noise (which is likely at 60Hz).

    It's a process of elimination, I'd first try swapping out the audio cable for a new one (maybe a different vendor one), to see if it makes a difference. Most audio cables are really poor (I make my own ones).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to shabaz

    I have experienced similar issues. It came down to the audio cable.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to ninjatrent

    Well dang, Shabaz just said that too, but there aren't any audio cables I can swap - it's directly attached to these cheap little speakers. I might have to find some better speakers.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 8 years ago in reply to ntewinkel

    You're using PC speaker type devices? What happens when you turn the power cord around inside the wall socket?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to ntewinkel

    In my case, it was the connection between the audio jack on the pi and the audio plug. The pi's audio jack also contains the video connection. I attributed the buzz to the cheap audio cable's left or right inputs coming in contact with the video connection in the pi's av jack.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to ntewinkel

    In my case, it was the connection between the audio jack on the pi and the audio plug. The pi's audio jack also contains the video connection. I attributed the buzz to the cheap audio cable's left or right inputs coming in contact with the video connection in the pi's av jack.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ntewinkel
    0 ntewinkel over 8 years ago in reply to ninjatrent

    That's a good point - I didn't realize that the pi includes video in that same jack. Maybe a headphones extension cable will help.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to ntewinkel

    The video/audio jack is a weird idea.

    https://www.raspberrypi-spy.co.uk/2014/07/raspberry-pi-model-b-3-5mm-audiovideo-jack/

    https://www.raspberrypi-spy.co.uk/wp-content/uploads/2014/07/Model-B-Plus-Audio-Video-Jack-Diagram.png

    Most 3.5mm jacks will be trying to short out the video (sleeve) and Ground (Ring2), since the sleeve is longer.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer