Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Powered Hub w/ Raspberry Pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 5010 views
  • Users 0 members are here
  • usb hub
  • raspberry_pi
  • raspberry pi
Related

Powered Hub w/ Raspberry Pi

ntewinkel
ntewinkel over 8 years ago

Hello!

 

I'm trying to sort out some suspected power issues with my Raspberry Pi by using a powered USB hub.

 

I have a couple of questions...

 

1. If I supply external power to the hub, does it feed back to the Raspberry Pi it's plugged into?

1b. If so, is that a bad thing? Does it interfere with the main power supply to the Pi?

 

The reason I ask is because on Adafruit they recommend "There is a port for an external power supply but its connected directly to the 5V line so if you need to externally power, we recommend prying open the case and cutting the red 5V line from the USB connection." - I'm assuming that's to avoid the 5v going back to the host.

ps on that - if cutting is recommended, would a diode (spanning that cut) be a good idea to allow it to be used as a non-powered hub elsewhere?

 

2. Can a USB hub be powered through one of its ports? ie, It's a 4 port hub - Can I plug a powered usb cable into one of those ports to provide power to the rest of the things plugged into the hub?

 

And also sort of related:

3. Have you seen any powered USB hubs that use a micro-usb (or mini) port to accept power? That would make it easy to power it with a standard tablet charger or another dedicated Raspberry Pi charger.

 

Related notes:

I intend to use the hub to power a WiPi WiFi adapter and a generic sort of wireless keyboard (likely WiFi, maybe Bluetooth)

 

Thanks!

-Nico

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    0 ntewinkel over 8 years ago

    I ran a couple of tests today.

    I found a USB hub with a 5v wall adapter that uses the same 1.7mm plug as the cheap one I had on my desk.

     

    First with a cheap USB hub...

    image

     

    And then with the higher quality USB hub (which is also a card reader). Note that the green power lamp is indeed on...

    image

     

    So that answers question 1: For cheap USB hubs, yes the power could be backfeeding. For better quality USB hubs, it doesn't.

     

    ps, another test with the higher quality hub shows that power from the host does still go through to power the ports if the hub is not plugged in with the adapter. Good design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ntewinkel
    0 ntewinkel over 8 years ago

    I ran a couple of tests today.

    I found a USB hub with a 5v wall adapter that uses the same 1.7mm plug as the cheap one I had on my desk.

     

    First with a cheap USB hub...

    image

     

    And then with the higher quality USB hub (which is also a card reader). Note that the green power lamp is indeed on...

    image

     

    So that answers question 1: For cheap USB hubs, yes the power could be backfeeding. For better quality USB hubs, it doesn't.

     

    ps, another test with the higher quality hub shows that power from the host does still go through to power the ports if the hub is not plugged in with the adapter. Good design.