Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Hooking up a 20-pin TFT LCD Screen?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 4787 views
  • Users 0 members are here
  • tft display
  • raspberry_pi
  • lcd screen
Related

Hooking up a 20-pin TFT LCD Screen?

dissonantguile
dissonantguile over 8 years ago

I have an 5" TFT LCD screen that I pulled out of an old portable TV/Monitor which has a ZIF connector and a 20 pin flat flex cable attached to it. At first I figured I could simply attach this to the display ZIF socket on my Raspberry Pi Model B (v1 rev 2.1), however it seems that the LCD's connector has 5 (?) more pins than the Raspberry Pi does. Unfortunately, I do not have a scope to inspect exactly what each of these lines do.

 

Is it possible for me to figure out how to connect this directly to my Pi using the ZIF connector? The board for this device does have a 3.5mm jack for A/V input, should I simply wire the Pi's video output to the board's video input on the A/V input jack? It would be nice to not have to use the board because it contains a ton of extra components for picking up UHF/VHF frequencies and such.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • baldengineer
    0 baldengineer over 8 years ago

    You still can't use the Pi's ZIF connector (directly). However, you could use the GPIO pins. But it isn't a trivial amount of work.

     

    First, you need to determine the pin-out of the LCD panel. Not sure how you would go about reverse engineering it, so it'd be ideal if you could find some documentation on it.

    Second, you'd need to build a breakout board to connect to the LCD's flat ribbon, to the Pi's GPIO. (This step is relatively straightforward.)

    Third, configure the Pi's GPIO for LCD operation.

     

    The good news? There was a Ben Heck Episode where he did something very similar. He was trying to make a portable retropie/mame device. In this case, he was directly driving the LCD, similar to what you are trying to accomplish.

     

    Episode 322: Rasp Pi No HDMI - Portable MAME Part 1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • baldengineer
    0 baldengineer over 8 years ago

    You still can't use the Pi's ZIF connector (directly). However, you could use the GPIO pins. But it isn't a trivial amount of work.

     

    First, you need to determine the pin-out of the LCD panel. Not sure how you would go about reverse engineering it, so it'd be ideal if you could find some documentation on it.

    Second, you'd need to build a breakout board to connect to the LCD's flat ribbon, to the Pi's GPIO. (This step is relatively straightforward.)

    Third, configure the Pi's GPIO for LCD operation.

     

    The good news? There was a Ben Heck Episode where he did something very similar. He was trying to make a portable retropie/mame device. In this case, he was directly driving the LCD, similar to what you are trying to accomplish.

     

    Episode 322: Rasp Pi No HDMI - Portable MAME Part 1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer