Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Desktop - no power
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 706 subscribers
  • Views 742 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Pi Desktop - no power

Richardb49
Richardb49 over 8 years ago

I have had the Pi desktop for a couple months. Tonight, I tried to power it up but I have no LED.

     Disassembled the boards from the box.

     Plugged power into Pi itself and it powers up.

     Plugged power into the desktop board and no power to Pi.

     Checked voltages around U2 which appears to be a switching regulator. 5.27 volts to pin 4, but L1 has no voltage, which indicates to me the FET in the chip is not switching.

 

Does anyone have a schematic, or suggestions for repair?

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 8 years ago

    Hi Richard,

    I do not have an answer for you. Perhaps you could post a few pictures of the board and wiring. I thought I would acknowledge your question so that it would go back to the top of the cheque.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Richardb49
    0 Richardb49 over 8 years ago in reply to jw0752

    John,

     

    The “wiring” is very simple. The 2400mA power supply was plugged into the desktop board. USB devices plugged in were a keyboard, mouse, camera and an external hard drive. In addition, a display was connected to the HDMI port and a speaker to the A/V port (who also derived power via a USB connection). No SSD drive installed.

     

    I verified that power was getting to the power connector on the desktop board. The  volt bus was 0 volts (verified by checking voltage at the Raspberry Pi connector to the desktop board). The fuse on the incoming power is OK, and the incoming power is present on the switching regulator. But there is no voltage on the inductor.

     

    Plugging in the power to the Raspberry Pi board itself works. There is 5V at the connector. I did this without any peripherals plugged in and with the keyboard, mouse and display plugged in to the Raspberry Pi itself. 5 volts was getting to the desktop board as well.

     

    It appears that the switching regulator is not working. I may have overloaded it with all the peripherals plugged into the USB ports. I need a schematic/parts list to figure out what failed and to replace parts. I am quite familiar with switching regulators – I design them into our controller products for the HVAC industry.

     

    Best regards,

     

    Richard Benjamin

    Electrical/Software Design Engineer

    ................................................................................

     

     

     

    STULZ Air Technology Systems, Inc.

    1572 Tilco Drive

    Frederick, MD 21704 U.S.A.

     

    Office: +1 240-529-1266

    www.stulz-usa.com

     

     

     

    Connect with us              

    The contents of this e-mail message and any attachments are confidential and are intended solely for addressee. The information may also be legally privileged. This transmission is sent in trust, for the sole purpose of delivery to the intended recipient. If you have received this transmission in error, any use, reproduction or dissemination of this transmission is strictly prohibited. If you are not the intended recipient, please immediately notify the sender by reply e-mail or phone and delete this message and its attachments, if any.

    Please consider the environment before printing this email.

    Attachments:
    image
    image
    image
    image
    image
    image
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to Richardb49

    Hi Richard,

    The fact that no one has come forward with a schematic leads me to believe that the schematic isn't available. Do you have a recourse to return the board as defective? I can't believe that they would have designed a board with peripherals and then not designed the power supply to support those peripherals. If you can't return the board and if you are able to identify the switch chip you should try replacing it or at least look up the data sheet and see what reading should be expected on the individual pins.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 8 years ago in reply to Richardb49

    Hi Richard,

    The fact that no one has come forward with a schematic leads me to believe that the schematic isn't available. Do you have a recourse to return the board as defective? I can't believe that they would have designed a board with peripherals and then not designed the power supply to support those peripherals. If you can't return the board and if you are able to identify the switch chip you should try replacing it or at least look up the data sheet and see what reading should be expected on the individual pins.

    John