Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum I2C communication between PIC16F877a and Raspberry pi 3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 2634 views
  • Users 0 members are here
  • raspberry_pi
Related

I2C communication between PIC16F877a and Raspberry pi 3

alexvarghese
alexvarghese over 8 years ago

hi,

Can any one help me to start a communication with PIC 16f877a controller and raspberry pi  through I2C protocol .i am new to both Raspberry pi and Pic controller .i know only the basics in Pic and raspberry pi . PIC will sense the data from a ultrasonic sensor. the sensed data has to be transfer to the Rpi .

  • Sign in to reply
  • Cancel
Parents
  • 14rhb
    0 14rhb over 8 years ago

    Alex,

     

    Sometimes there can be a single bit set incorrectly in one register you've never noticed from the data sheet !

     

    You didn't say what tools you are using for the PIC development; I'm assuming you are using the Microchip MPLAB X IDE and XC8 compiler (both free to download from Microchip's site). If you are, then an additional step that helps get things up and running is to use Microchip's MPLAB Code Configurator (MCC) which gives a nice GUI for selecting options on each peripheral (I2C, SPI, UART etc) and then will generate the code for you. My only caveat is that it isn't always the best behaved add on for Netbeans (which MPLAB X is written for) but MCC does normally get those obscure registers setup correctly so that the peripheral is at least running.

     

    Another intermediate step to getting your project working is to perhaps use an Arduino. They have many easy to copy examples using I2C - use it to prod the other device or to listen for data (which can then be displayed via its inbuilt terminal).

     

    If you could post any circuit diagram (sketch or clear photo) and code that might help someone in the community spot what is up.image

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 8 years ago in reply to 14rhb

    @14rhb Microcontrocontrollers (PIC, AVR, arduino, STM32) like the pi, are often used as the MASTER in an i2c bus situation..... An arduino might for example, control a few relays based on a pressure sensor, or use a 9DOF sensor to control two motors to balance a robot. Anyway, the arduino is then a MASTER towards those sensors, and the code/libraries for that is well-used, well-debugged and well-documented. But the "arduino is an I2C slave" is not often used. I'm not even sure a library exists.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 14rhb
    0 14rhb over 8 years ago in reply to rew

    Is that phenonenon perhaps just how many home/maker projects are designed: where the Arduino is the 'intelligent' part on the I2C (eg Master) whilst servos, temperature sensors etc are the I2C slaves? You should be able to use the Arduino Wire.h library to configure the Arduino as a slave like in this article here by Nick Gammon.

     

    Rod

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 14rhb
    0 14rhb over 8 years ago in reply to rew

    Is that phenonenon perhaps just how many home/maker projects are designed: where the Arduino is the 'intelligent' part on the I2C (eg Master) whilst servos, temperature sensors etc are the I2C slaves? You should be able to use the Arduino Wire.h library to configure the Arduino as a slave like in this article here by Nick Gammon.

     

    Rod