Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi 3 boot issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 8 answers
  • Subscribers 710 subscribers
  • Views 1946 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Raspberry pi 3 boot issue

silentnight__
silentnight__ over 8 years ago

Hey guys!

 

Having an issue with my Pi 3. It was working 100% fine as usual at night, but the next morning when I turned it on, I got " no signal " on my TV...... bloody strange. The red light is on solid, and the green light is flashing sporadically. Nothing happened to it overnight, it wasn't dropped, knocked or anything..... just literally decided not to work the next day.

 

Anyone ran into this?

 

Thanks in advance.

Aaron

  • Sign in to reply
  • Cancel
  • rctho
    0 rctho over 8 years ago

    Turn on the tv before powering the pi. if there is no video device connected during startup it won't load the video drivers. make sure the input on your television is correct too.

     

    I hope that helps.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bwelsby
    0 bwelsby over 8 years ago

    Have you got a spare uSD you can install raspbian on and see if that works.

    Do you "shutdown" the Pi before removing power?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • silentnight__
    0 silentnight__ over 8 years ago

    Hey rctho.

     

    I do always do that man, I learned a while ago that that's an issue and it had me stumped for some time.

     

    @ Brian. Unfortunately I don't man, but I can get one.

     

    The odd thing is it just stopped working completely overnight, within the span of around 6 hours or so. No warning, no lead up or tell tale signs.... just dead.

     

    Hope these responses help.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mp2100
    0 mp2100 over 8 years ago

    How long have you been running the rPi?  SD cards do wear out.  They don’t have the long read/write life of other forms of memory.  But an SD card should last a year or two.

     

    It doesn’t help you today, but the rPi 3 (not earlier models) will boot and run from a USB drive.

     

    https://www.raspberrypi.org/documentation/hardware/raspberrypi/bootmodes/msd.md

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • silentnight__
    0 silentnight__ over 8 years ago

    The rPi is about 2 years old, so that could well be an issue. I'll write to a usb and attempt to boot from that to test if the card is indeed the issue.

     

    If it's not the card fellas, is there any other suggestions as to what could be the issue?

     

    Cheers!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ripntime
    0 ripntime over 8 years ago in reply to silentnight__

    Maybe corrupted file system to many bad shutdowns over time has corrupted boot files possibly. Best next solution is to start fresh, but if you have files on the micro-sd you want to keep get a micro-sd to SD adapter and load it in a laptop and take the files you want to keep. There is the chance that when you try to access it on the laptop it'll say it's corrupt you can try fixing it but that will put a lot of stress on the card ad might bring t closer to failure than just a format and reinstall would do.
    Sincerely Christopher

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • silentnight__
    0 silentnight__ over 8 years ago

    Thanks Chris!

     

    I'm going to grab a new mSD and start fresh then go from there.

     

    Thank you all so much for your help, it's muchly appreciated.

     

    Regards,

    Aaron.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 8 years ago

    Can you capture the blinky pattern for the Green LED? If it is blinking, then it is an indication that the SD card is being accessed.

    See the following link to see if the pattern you see matches one listed.

    https://elinux.org/R-Pi_Troubleshooting

     

    Also, if you have a FTDI-USB cable, you can get a Serial console to the Pi and look at the boot process and see if anything there leads to an issue.

    https://elinux.org/RPi_Serial_Connection

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ripntime
    0 ripntime over 8 years ago in reply to silentnight__

    Sometimes it's time vs money and the money for an sd card vs loosing hair is not worth it in the long run.  Plus it could have bad sectors which will produce intermittent problems on a Pi.
    A fresh start leaves nothing to chance. The old one can be used for release testing or for trying various Pi systems retropie etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 8 years ago in reply to ripntime

    With Flash memory and SSD, the location where data was written previously may not be the same place it is on the memory device due to wear leveling.  There is an attempt to remap the blocks in storage and mark an area that had a write error as bad, but this is only if there is free space left on the memory device.  The fun thing with flash Memory cards and SSDs is that unless the device supports SMART features and they are enable, you will not know the memory device is bad until it no longer works and you can not get to any of the data.  This is why it's good to not put anything important on a flash base storage device or ensure it is backed up often.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>