Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi 3 boot issue
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 8 answers
  • Subscribers 710 subscribers
  • Views 1934 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Raspberry pi 3 boot issue

silentnight__
silentnight__ over 8 years ago

Hey guys!

 

Having an issue with my Pi 3. It was working 100% fine as usual at night, but the next morning when I turned it on, I got " no signal " on my TV...... bloody strange. The red light is on solid, and the green light is flashing sporadically. Nothing happened to it overnight, it wasn't dropped, knocked or anything..... just literally decided not to work the next day.

 

Anyone ran into this?

 

Thanks in advance.

Aaron

  • Sign in to reply
  • Cancel
  • rew
    0 rew over 8 years ago in reply to jomoenginer

    jomoenginer  wrote:

     

    but this is only if there is free space left on the memory device. 

    Keep in mind that this is another "free" than what you'd see with "df", or in "6.4Gb used of 8Gb" in your file browser.

     

    When an SD card claims 8Gb, they actually mean 8 billion bytes. But in physical computer stuff that would normally be 8 * 2^30, which is a few percent more (about 7.2% if my wet-ware-calculator is correct). That 7% is used for wear leveling. So... worst-case you write the full 8Gb of data, and then start writing a single block of data again and again. Now all-but-one blocks are "in use" and your rewritten block will be written in the next-available block in the (7%*8GB=) 570Mb of "secret space". Now if we assume that the SD card works with 128kB blocks, you'll have written that single block 4600 times before the first datablock is getting written for the second time.....

     

    Every time you write to a DIFFERENT block, it will get a block from the pool of free blocks and then the old one will get added to the pool.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<