Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum NOOB: Rasberry Pi or Arduino - Larson Bar controlled by smartphone bluetooth
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 779 views
  • Users 0 members are here
  • bluetooth
  • led
  • raspberry_pi
  • arduino
Related

NOOB: Rasberry Pi or Arduino - Larson Bar controlled by smartphone bluetooth

cburnett1981
cburnett1981 over 11 years ago

I realize that the following project is not a beginner project.  And I am a beginner.  However, before I spend $ and time w/ either Rasberry Pi or Arduino, I'd like some input.

 

My final objective (who knows when I'll get to it) would be to create:

  • a ~20-24" long,  Larson Scanner, with
  • variable intensity low, med, high strength LED
  • Variable speed
  • variable color RGB
  • all controlled by Android or iOS over bluetooth.
  • battery or a/c powered

 

Example of commercial product w/ additional features that I can do w/o (audio and tactile)

 

Example of Ardiuno project of larson scanner, but missing a few features, key:  bluetooth.  I'm considering using Blynk, but bluetooth isn't currently an available option  (Blynk site reports next generation).  Also looking at a kickstarter for LightBlue Bean+

 

As I have no preference for Arduino over Rasberry Pi, some of what I have read in researching this project is that Rasberry Pi may be easier for Droid/iOS integration (those articles may have been out of date).

 

Thanks,

Casey

www.emdrforathletes.com

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    balearicdynamics over 11 years ago

    Hi Casey,

     

    I realize that the following project is not a beginner project.  And I am a beginner.  However, before I spend $ and time w/ either Rasberry Pi or Arduino, I'd like some input.


    Don't worry, there should always be a starting point to move from a beginner to and advanced image Then in my opinion this project don't seems me so much complex. I agree with clem57 that Arduino - as far as what we know reading your post - maybe perfectly working. But if you want to make something competing with a sort of commercial product, my suggestion is that you before see what the other has done, and possibly find at least a small detail that can make the difference. In this case, it is the worth to explain more in detail what do you have in mind, just before deciding to start with Arduino then discover that the Raspberry PI maybe a bit more expensive but opens the door to a more complete and innovative / reliable product.


    Enrico


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • balearicdynamics
    balearicdynamics over 11 years ago

    Hi Casey,

     

    I realize that the following project is not a beginner project.  And I am a beginner.  However, before I spend $ and time w/ either Rasberry Pi or Arduino, I'd like some input.


    Don't worry, there should always be a starting point to move from a beginner to and advanced image Then in my opinion this project don't seems me so much complex. I agree with clem57 that Arduino - as far as what we know reading your post - maybe perfectly working. But if you want to make something competing with a sort of commercial product, my suggestion is that you before see what the other has done, and possibly find at least a small detail that can make the difference. In this case, it is the worth to explain more in detail what do you have in mind, just before deciding to start with Arduino then discover that the Raspberry PI maybe a bit more expensive but opens the door to a more complete and innovative / reliable product.


    Enrico


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cburnett1981
    cburnett1981 over 11 years ago in reply to balearicdynamics

    @enrico  thanks for encouragement

    @Clems thanks for the direction

     

     

    The key difference between the commercial product  and my idea

     

    Hardware:  Much more portable (many therapist move between lots of offices and having a $$$ product in each is not feasible).  So the size of lightbar and bluetooth w/ phone are key.  wifi/networks wouldn't be an option as not just different offices, but sometimes different office spaces.  I plan on building a simple tripod, or option to hand from simple push pins for display purposes.

     

    hardware / software dream next generation:  build connection / application in stereo tones that match the lights.   build connectivity / application management for Tacticle sensors (think holding small vibrating paddles, like a phone on vibrate).

     

     

    App: Today, I was working with a patient, and realized that the latest research supports a small random change between each set of DAS .   So I was hoping to program the app to allow a range of speed or brightness to be unique each time the start button is selected (read below). 

     

    Apps : To allow for eventual recording the number of sets. 

     

    Beyond that , maybe sometime writing a premium app to be the clinical note for the treatment (this would add a whole new layer of complexity).  There is a research based standard protocol for how this is administered and monitored.

     

     

     

    Dream of just light bar draft 1

    App: Have a dial on screen for changing speed of lights with a max and min boundary. 

    App: Possibly dial for brightness of lights.  (v2. separate settings for tactile paddles and audio tones). 

    App: Setting to change color of lights from phone.  Can one LED be different colors?  I thought I read that they could.

     

    • Push / slide to start button on phone.  Lights begin.
    • Then Option 1
    • Have a planned set length that is adjustable by clinician  ~15s to ~45 s
    • Set ends automatically w/ countdown.
    • Or
    • Option 2
    • No timer
    • Set ends by pushing or sliding stop button.

    • Have option for constant speed of lights on each set.

     

    • Have option for random speed w/n a small variation (it is theorized that we as humans began to ignore novelty quickly).  In other words, each Start speed would be slightly different than the previous w/n a window of tolerance.  The lights would be a constant rate during the entire set.  But set A might be faster than B or C, etc.