Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum A raspberry pi - IKEA lack arcade idea
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 4 answers
  • Subscribers 707 subscribers
  • Views 1655 views
  • Users 0 members are here
  • raspberry_pi
Related

A raspberry pi - IKEA lack arcade idea

omereli
omereli over 8 years ago

Hi everybody! after looking for nice original ideas to build my own cheap and pretty arcade, i came across the IKEA lack coffee table arcades (such as element 14's) i have decided to do something similar but wall mounted and unique. check out my design in the attached pictures. i would very much like to hear feedback on my idea and how to improve.

frontSide

what you are looking at is:

 

a LACK IKEA side table with no legs, with a integrated 19' LCD screen mounted on a wall (i would welcome insights and ideas on how to mount it, flat or with some giveaway from the wall? it's a concrete wall - what mounting device is best.. anything..)

 

the controllers are mounted on two small LACK wall shelf's (the controller themselves are not finale.. i would probably use  some kit like

Easyget LED Arcade - i welcome input about this as well)

 

the pie it self is a challenge.. as it stands now it's just sort of sits inside a hole in the table.. and sticks out a bit.. would really like ideas about that.. the cables will go behind the table in channels i would carve out for them.

 

it's a good idea to note i have VERY limited woodworking skills, tools and money.. that is why i went with the IKEA HACK conept to begin with.. with that in mind, i am looking forward for your input.

 

Thank's!

 

BTW i am very sorry about my poor English grammar, i am afraid it is not my first language...

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 8 years ago

    Hello Omer,

     

    the idea sounds original and interesting

    Considering that the weighted part of the wall stuff is the screen, while the Ikea hacked border is lightweight, I think that probably the best solution (with concrete it works fine) is a wall mount monitor support. You can find cheap ones that are just for vertical mounting (not those with the orientable arm). They give a minimum of vertical slant to the monitor but it is not difficult to fix them in the desired position.

     

    I mean something like this: https://cloud.stefaanenhanne.be/index.php/login?user=enrico.miglino%40dekimo.com  without extension, just attached to the wall and very robust.

     

    Instead, there is something else you should consider with attention from the point of view of the ergonomy. Playing games (I think to traditional arcades like Doney Kong, Super Mario etc.) standing in front of the monitor is really a vintage scenario but the old bar games, if you remember, was mounting their monitor on the bottom of the player, with the screen image inverted and a mirror. The reason was not only due to the tube monitor but also for a question of ergonomy. Thanks to the mirror reflection path, it was possible to create a very compact game station keeping the screen at a distance of about 1 meter from the player. As far as I see in your design this distance will be dramatically shortened; I am worried that this can create a disease for the player.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 8 years ago

    Hello Omer,

     

    the idea sounds original and interesting

    Considering that the weighted part of the wall stuff is the screen, while the Ikea hacked border is lightweight, I think that probably the best solution (with concrete it works fine) is a wall mount monitor support. You can find cheap ones that are just for vertical mounting (not those with the orientable arm). They give a minimum of vertical slant to the monitor but it is not difficult to fix them in the desired position.

     

    I mean something like this: https://cloud.stefaanenhanne.be/index.php/login?user=enrico.miglino%40dekimo.com  without extension, just attached to the wall and very robust.

     

    Instead, there is something else you should consider with attention from the point of view of the ergonomy. Playing games (I think to traditional arcades like Doney Kong, Super Mario etc.) standing in front of the monitor is really a vintage scenario but the old bar games, if you remember, was mounting their monitor on the bottom of the player, with the screen image inverted and a mirror. The reason was not only due to the tube monitor but also for a question of ergonomy. Thanks to the mirror reflection path, it was possible to create a very compact game station keeping the screen at a distance of about 1 meter from the player. As far as I see in your design this distance will be dramatically shortened; I am worried that this can create a disease for the player.

     

    Enrico