Hi,
we are took new raspiberry pi 2 board. with prebuilt with HDMI screen it is booting fine. But we like to change the boot log on to serial port. we modified in cmdline.txt console to ttys0 and in /etc/inittab -- in that last line changed to ttys0-- then we got the below log. Initially green led "ACT" is blinking rate is fast and then after some time that led blink rate is reduced and only side small blink is coming -- then no other log is coming on serial port.
"Uncompressing Linux... done, booting the kernel" after that kernel is not booting
1 Either Linux kernel is booting eor
2. in the kernel do we need to configure the to serial port for the log.
regards,
Viswanath K.