Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace input delays
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 18 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 3509 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

PiFace input delays

jmac67
jmac67 over 7 years ago

I have a PiFace on a RaspberryPi, and it works great, but there is a several second delay between when the input switches to when the script responds. Can someone tell me where to find/change this delay time? Thanks, Jim

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi Jim,

     

    Unfortunately there's not enough information to help in a good way. If you could share your code it will help (ideally using syntax highlighting as shown here: How to Ask Questions using the Create Discussion tool   because Python uses spaces, and it will come out as a mess to the reader unless monospaced).

    Also, if you can explain what the code is to be used for, there may be a better solution based on context. For instance, if you're trying to activate (say) a camera shutter for capturing a balloon burst, then that requires a very different solution than activating a camera or alarm on intruder detection (this is just an example).

    Without seeing your code, it is not possible to tell if there is a deliberate or resolvable delay that can be changed in the code (and if the minimal delay will be sufficient for your needs), or if a different solution is needed.

    Right now it is not possible to tell if you need a script to execute and perform the unknown response within 10msec, or 1msec, or less.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi Jim,

     

    Unfortunately there's not enough information to help in a good way. If you could share your code it will help (ideally using syntax highlighting as shown here: How to Ask Questions using the Create Discussion tool   because Python uses spaces, and it will come out as a mess to the reader unless monospaced).

    Also, if you can explain what the code is to be used for, there may be a better solution based on context. For instance, if you're trying to activate (say) a camera shutter for capturing a balloon burst, then that requires a very different solution than activating a camera or alarm on intruder detection (this is just an example).

    Without seeing your code, it is not possible to tell if there is a deliberate or resolvable delay that can be changed in the code (and if the minimal delay will be sufficient for your needs), or if a different solution is needed.

    Right now it is not possible to tell if you need a script to execute and perform the unknown response within 10msec, or 1msec, or less.