Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Can you Replace the Guts of a EEE PC with a Pi3B+?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 5 answers
  • Subscribers 706 subscribers
  • Views 5465 views
  • Users 0 members are here
  • raspberry_pi
Related

Can you Replace the Guts of a EEE PC with a Pi3B+?

mattig89ch
mattig89ch over 7 years ago

Hello all,

 

First and foremost, I'm not an engineer.  I'm a network tech by training, and a Help desk tech by profession.  So this is something way out of my normal area of knowledge.  I did take a basic engineering course in colledge, but I failed that class so hard it was almost comical.  3 weeks in, I reach a point of simply not understanding what the teacher was saying.  It was like he was speaking another language.  So I dropped the class, and transferred into the networking field.  The mandatory programming classes were so hard, I barely squeeked by them.  But the actual networking stuff was easy for me.

 

I have a Rasberry Pi3B+ I'm not doing anything with.  Originally, I bought it to turn it into a reto-pi, and put some N64 ROMS on it.  Sadly, I can't see to give it enough power.  Every time I enable the Wi-Fi, it reboots.  I suspect the power draw is too great, so it shuts down.  Then when the power draw isn't as high as it needs to be, it powers up.  The wifi then comes on automatically, and it repeats the process.  I have tried multiple outlets, and and wall adapters (including the official Rasberry Pi power brick!).  So far, nothings worked.

 

I also have an old EEE PC that runs XP-Pro.  Yep, I'm that old.  What I want to do is to gut the thing and replace the innards with this Pi3 B+.  The screen works, the keyboard/track pad work great, and the battery still holds a charge last time I checked.  its just the motherboard/hard drive I want to replace.

 

Is something like this even possible?  If so, where would I look to even begin a project like this?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 7 years ago

    Hi,

     

    There are several threads on this topic (e.g. https://www.reddit.com/r/raspberry_pi/comments/6rxm63/computerception_a_raspberry_pi_zero_inside_a_2007/   ), but it seems no-one has managed it so far.

    I think it will be hard, because most of the things you want connecting to the EEE PC's interfaces, will have different interfaces on the Pi.

    Your best bet is just to get the Pi running as-is, since you'll need to do that anyway regardless of what you attach to its interfaces.

    It's not normal for it to reboot like this, so to troubleshoot, it is worth confirming: by official Pi power brick, do you mean the one that looks identical to this: https://www.newark.com/stontronics/t5875dv/psu-raspberry-pi-5v-2-5a-multi/dp/77Y6535  - what voltage and current values are marked on it? The correct one should say "Stontronics" on the back, and "5.1V 2.5A". If it doesn't say that, what manufacturer and values are marked on it?

    Although it looks like a normal USB supply, the official Pi one has a few unusual features, which are important for it to make the Pi 3 B+ function correctly.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 7 years ago

    Hi,

     

    There are several threads on this topic (e.g. https://www.reddit.com/r/raspberry_pi/comments/6rxm63/computerception_a_raspberry_pi_zero_inside_a_2007/   ), but it seems no-one has managed it so far.

    I think it will be hard, because most of the things you want connecting to the EEE PC's interfaces, will have different interfaces on the Pi.

    Your best bet is just to get the Pi running as-is, since you'll need to do that anyway regardless of what you attach to its interfaces.

    It's not normal for it to reboot like this, so to troubleshoot, it is worth confirming: by official Pi power brick, do you mean the one that looks identical to this: https://www.newark.com/stontronics/t5875dv/psu-raspberry-pi-5v-2-5a-multi/dp/77Y6535  - what voltage and current values are marked on it? The correct one should say "Stontronics" on the back, and "5.1V 2.5A". If it doesn't say that, what manufacturer and values are marked on it?

    Although it looks like a normal USB supply, the official Pi one has a few unusual features, which are important for it to make the Pi 3 B+ function correctly.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer