Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi for Industrial Uses
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 37 replies
  • Answers 26 answers
  • Subscribers 709 subscribers
  • Views 15707 views
  • Users 0 members are here
  • iiot
  • plc
  • pi compute
  • industry
  • sbc
  • compute module 3
  • raspberry_pi
  • raspberri pi
  • raspberry pi 3b+
  • process control
  • raspberry pi 3 a+
  • dcs
  • compute module
Related

Raspberry Pi for Industrial Uses

tonydbeck
tonydbeck over 7 years ago

I am interested to know what experience others have had using a Raspberry Pi in industry?  I would love to hear about:

 

  • Any issues with short and long term reliability?
  • Connectivity with Industrial control systems -
    • Have add on boards been used?
    • Have custom PCB's been made to interface 24V based I/O on PLC's / DCS systems etc?
    • How has it been hooked up to power?
  • Issues with EMI?
  • Long term SD card reliability?
  • Has a Pi been used to actually control some industrial equipment rather than for monitoring or HMI?
  • What version of Pi was used - eg. Compute module
  • Why use a Pi vs a PLC or industrialised PC?
  • What were the biggest challenges?
  • Was there any challenge from peers or management in using something that could be viewed as an educational tool rather than industrial control equipment?
  • What OS has been used?
  • Have there been any concerns around security? Especially if connecting to a Process Control Network.
  • What security precautions have been taken?

 

I can see lots of advantages to using a Pi in industry - for example the amount of power and versatility for such a low cost!

 

 

Even if you don't have experience using a Pi in industry - it would still be great to hear people points of view! 

 

I look forward to some interesting responses!

 

-------------------------------------------

Tony

  • Sign in to reply
  • Cancel
Parents
  • tonydbeck
    0 tonydbeck over 7 years ago

    I would also be interested to know what methods are used to make a device such as a Single Board Computer more suited for an industrial use?  Some methods I am aware of:

     

    • More PCB layers for EMC compliance and better heat dissipation - as used on the netPi
    • Components with larger temperature ranges
    • Conformal coatings
    • Use of Enteprise Multi-Level Cell (eMLC) or Single Level Cell (SLC) flash rather than Triple Level Cell (TLC) flash
    • Isolation circuits - eg. Opto Isolation
    • ESD protection cirucuits
    • EMI shielding - eg. metal enclosure
    • Ingress Protection - eg. High IP rated enclosure
    • Hardened OS - Use of Docker containers, no SSH access etc
    • ECC memory
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to tonydbeck

    You might also consider adding an RTOS to the list, as properly written software for RTOS can meet critical latency and jitter requirements.

     

    In addition to ECC memory, some of them will also have separate OS level fault tolerance, say by modularising the OS kernel and being able to hot reload any module on the fly for downtime-free updates (e.g. think telecommunications equipment often is capable of this).

     

    Sometimes, what makes something industrial may simply be the use of parts with a known long market lifetime - i.e. commitments from suppliers that the components will remain available so that you can offer assurance to integrators that your solution may still be serviced 15-20 years down the track.

     

    Cherrypicked unit testing may also be used to qualify units met required standards prior to shipping as industrial. Sometimes this entails better inspection as well (e.g. Xray).

     

    Sometimes there are design differences to allow for better (more rapid) field service testing/debugging through LCDs, test points and integration of better cooling solutions.

     

    But otherwise, it seems you've covered all of the main ones I'm aware of.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 7 years ago in reply to tonydbeck

    You might also consider adding an RTOS to the list, as properly written software for RTOS can meet critical latency and jitter requirements.

     

    In addition to ECC memory, some of them will also have separate OS level fault tolerance, say by modularising the OS kernel and being able to hot reload any module on the fly for downtime-free updates (e.g. think telecommunications equipment often is capable of this).

     

    Sometimes, what makes something industrial may simply be the use of parts with a known long market lifetime - i.e. commitments from suppliers that the components will remain available so that you can offer assurance to integrators that your solution may still be serviced 15-20 years down the track.

     

    Cherrypicked unit testing may also be used to qualify units met required standards prior to shipping as industrial. Sometimes this entails better inspection as well (e.g. Xray).

     

    Sometimes there are design differences to allow for better (more rapid) field service testing/debugging through LCDs, test points and integration of better cooling solutions.

     

    But otherwise, it seems you've covered all of the main ones I'm aware of.

     

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • tonydbeck
    0 tonydbeck over 7 years ago in reply to Gough Lui

    Some other really good points - thanks! RTOS's can certainly be very beneficial on an industrial platform.  This is an area I would really love to learn more about as my knowledge on the use of an RTOS is very weak.

     

    Some of the equipment (VFD's, DCS controllers / IO cards, PLC's etc)  where I work will have a published lifecycle from the vendor, which in some cases could be 15 to 20 years 

    Siemens will even take an excel list of your existing installed equipment and provide you with a report on where each item is on its lifecycle.

    With this information it is possible to create a life cycling plan for the equipment in the plant.

     

    It is funny though, that some industrialised equipment is so reliable that it ends up in service well beyond its supported life cycle!  We still use a number of Siemens S5 PLCs and Simovert P drives installed - but because they are so reliable, they are kept in place.  In some cases the engineering effort to update can be huge, and with limited resource, other projects can take priority.

     

    I had thought of one more things - Use of a hardware watchdog.

     

    Cheers

    ------------------

    Tony

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer