Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is there a smaller ethernet jack I can use on the Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 706 subscribers
  • Views 1471 views
  • Users 0 members are here
  • replacement
  • ethernet
  • jack
  • raspberry_pi
  • raspberry pi
  • soldering
Related

Is there a smaller ethernet jack I can use on the Raspberry Pi?

johnsnape
johnsnape over 7 years ago

I'd like to find a smaller jack for the ethernet port on the Raspberry Pi 3 so I could make the board fit in a smaller space. Is one available?

I want to de-solder the one on there and solder on a new, smaller port.

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    0 Gough Lui over 7 years ago

    I wouldn't advise doing so - it's not quite as simple as that because the jack is an integrated magjack meaning that the Ethernet Hybrid Transformer is integrated into the jack. If you removed the jack, you'd need to connect an external transformer which would be quite a similar size (or be absolutely sure you have a jack with integrated magnetics) - if you don't know what it looks like, it's something like this: https://au.element14.com/pulse-electronics/hxu6200nl/ethernet-transformer-choke-350uh/dp/2911454

     

    If you really need smaller, perhaps you should forego Ethernet entirely and consider using Wireless only if possible. That way, you might also consider a board such as the Raspberry Pi Zero W. Otherwise, you might consider a Model A variant with the USB port and use an external USB to Ethernet adapter. There is also a compute module for even smaller size but it is designed for embedded usage and has the minimal amount of peripherals on the SODIMM-form-factor card.

     

    Interesting trivia was that the first Raspberry Pi Model B boards had no functioning Ethernet because they mistakenly fitted standard RJ45 style jacks rather than integrated magjacks - https://www.raspberrypi.org/blog/manufacturing-hiccup/

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 7 years ago

    I wouldn't advise doing so - it's not quite as simple as that because the jack is an integrated magjack meaning that the Ethernet Hybrid Transformer is integrated into the jack. If you removed the jack, you'd need to connect an external transformer which would be quite a similar size (or be absolutely sure you have a jack with integrated magnetics) - if you don't know what it looks like, it's something like this: https://au.element14.com/pulse-electronics/hxu6200nl/ethernet-transformer-choke-350uh/dp/2911454

     

    If you really need smaller, perhaps you should forego Ethernet entirely and consider using Wireless only if possible. That way, you might also consider a board such as the Raspberry Pi Zero W. Otherwise, you might consider a Model A variant with the USB port and use an external USB to Ethernet adapter. There is also a compute module for even smaller size but it is designed for embedded usage and has the minimal amount of peripherals on the SODIMM-form-factor card.

     

    Interesting trivia was that the first Raspberry Pi Model B boards had no functioning Ethernet because they mistakenly fitted standard RJ45 style jacks rather than integrated magjacks - https://www.raspberrypi.org/blog/manufacturing-hiccup/

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnsnape
    0 johnsnape over 7 years ago in reply to Gough Lui

    I didn't realize it wasn't a dumb port, like USB. Thanks for that info! Now I understand why it's so large.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 7 years ago in reply to johnsnape

    You could Hardware wire as in off board the jack connection:

    https://www.sparkfun.com/products/13021