Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Audio out - amplifier for ear buds
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 706 subscribers
  • Views 1815 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Audio out - amplifier for ear buds

mgillett
mgillett over 7 years ago

I am nearly deaf, using the computer audio out 3.5 mm plug for earbuds I often can not hear the audio while attempting to watch a youtube video. Many persons do not carefully record their audio nor use closed caption.

 

I need to use earbuds rather than playing the sound through a speaker because I have to have the volume up so loud no-one can stand to be in the house. I turn the computer volume to the max, and the video playback to the max and can barely hear audio. It would be nice to have some range that I can turn up or down.

 

I have looked for circuits that will actually amplify the sound without blowing the little earbuds to pieces. I do not know the impedance of the earbuds but figure they are far lower than the 8 ohms for a regular speaker. I do wear blue tooth enabled hearing aids but the computer does not send the audio signal via blue tooth. They use blue tooth for the keyboard or mouse.

 

If I did have a device that could connect to my hearing aids through blue tooth, I would still need a way to control the sound level to make up for the wide variation in sound recording levels. I could write a list of ideal specifications like...

1. Simple

2. just plug into the 3.5 mm jack on the standard device such as phones, computers, etc.

3. A volume control knob

4. An automatic gain control that could level out all signal levels to a standard level so the volume control would simply be for controlling the level.

5. A bypass connection to go to an external speaker when watching a movie with someone (it would be nice to still have the ability to use my earbuds at the same time.

 

Issues:

1. The quality of the sound does not make much difference to me, I cannot distinguish the high fidelity nuances of music any longer. But the tone level can be very critical. When thinking of an equalizer the higher frequencies are completely gone, as are much of the lower frequencies. My hearing aids are tuned to optimize the level for my hearing. There is still the problem that the audiologist is not able to give enough volume to frequencies I am lacking because of the hearing devices feedback causing a squealing sound. I can't hear the squealing but people run out of the room when it happens. So they set the level as high as they can.

2. Headphones are uncomfortable to wear for long periods of time. The light ones seem to easily get dislodged, the expensive ones have a pressure that pushes against the head causes an ache in the head.

3. Blue tooth is wonderful, more than a few times I have gotten up forgetting I have the earbuds in and the cable yanks them out of my head.

4. I did not lose my hearing until I was an adult and a bit to close to a bomb going off. (A lot of soldiers have this problem)

5, I know there are commercial devices but I am not certain they will do what I am trying to do.

6. I originally thought an ic amp that ran on 5 volts with a volume level control that I could pug into the USB to get the power, the audio jack to get the signal, and an output jack to plug in the earbuds. Seems simple but would like some guidance. I am not sure where to find that guidance.

 

Appreciate any pointers,

Mike

  • Sign in to reply
  • Cancel
Parents
  • ralphjy
    0 ralphjy over 7 years ago

    I would worry about over amplification possibly causing further hearing damage.  Hearing aids are designed and adjusted to prevent this.  As others have mentioned there are ways to limit the maximum volume, but have you tried speech/voice to text converters?  If you are primarily interested in YouTube videos, I know converters exist for English.  I've never tried one but it might be worth a look while you work on a hardware solution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mgillett
    0 mgillett over 7 years ago in reply to ralphjy

    Yes, I have tried the converter programs, Youtube used to have one built into the program I think, It was 30% gibberish. IT actually only takes understanding about half the words to make sense of what a person is trying to communicate. Accents are very difficult to understand. I appreciate so many people using English (although I speak American, a language similar to English.)

     

    I have been concerned about too much sound pressure and use ear protection when using outdoor equipment, power tools and the like.

     

    I think the BlueTooth idea is the best one, as you said the hearing aids have high tech programs to limit the loud noise. I do have blue tooth on the cell phone that works very well for me to hear, it is the use of the computer. Primarily persons that record things without any regard to the sound levels.

     

    Those that do process their audio are greatly appreciated. It seems that certain kinds of "how to" videos are produced by people speaking too fastly in a second language, i.e. computer programming, java, ruby, SQL, the electronics are a great mix of persons from English (England) speaking countries. The programs may work better with there content.

     

    A big shout out to anyone who adds CC (Closed Captioning) to their videos. Thank you!

     

    For the home phone, I use something called a CAPTEL (Closed caption phone service). It uses a computer internet connection and a regular phone line. The persons that make that work are typing like crazy. I earned a masters degree from the University of Southern California through the phone and computer. The persons typing that stuff had to learn whole new vocabulary, and keep up with 8 to 12 person's in one sitting. The sessions would be 2 to 3 hours. That has not been automated yet, it is literally a person typing all that stuff. There is no possible way I could have passed those courses without that accommodation.

     

    I do appreciate your word on not "over diving" the audio pressure. Without a limiting device, it would be impossible to turn the levels down fast enough. The radio DJ's had something called an optimod that would ake their signal and boost it up to the maximum (I had a friend that was in the radio business that used these kinds of systems. I looked it up Orban still manufactures this type of equipment (OPTIMOD-FM 8700i) audio processing. This is not for audiophiles because there is suppression as well as pushing sound levels (so more noise etc.) These devices try to take the input signal and output a consistent full bandwidth signal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mgillett
    0 mgillett over 7 years ago in reply to ralphjy

    Yes, I have tried the converter programs, Youtube used to have one built into the program I think, It was 30% gibberish. IT actually only takes understanding about half the words to make sense of what a person is trying to communicate. Accents are very difficult to understand. I appreciate so many people using English (although I speak American, a language similar to English.)

     

    I have been concerned about too much sound pressure and use ear protection when using outdoor equipment, power tools and the like.

     

    I think the BlueTooth idea is the best one, as you said the hearing aids have high tech programs to limit the loud noise. I do have blue tooth on the cell phone that works very well for me to hear, it is the use of the computer. Primarily persons that record things without any regard to the sound levels.

     

    Those that do process their audio are greatly appreciated. It seems that certain kinds of "how to" videos are produced by people speaking too fastly in a second language, i.e. computer programming, java, ruby, SQL, the electronics are a great mix of persons from English (England) speaking countries. The programs may work better with there content.

     

    A big shout out to anyone who adds CC (Closed Captioning) to their videos. Thank you!

     

    For the home phone, I use something called a CAPTEL (Closed caption phone service). It uses a computer internet connection and a regular phone line. The persons that make that work are typing like crazy. I earned a masters degree from the University of Southern California through the phone and computer. The persons typing that stuff had to learn whole new vocabulary, and keep up with 8 to 12 person's in one sitting. The sessions would be 2 to 3 hours. That has not been automated yet, it is literally a person typing all that stuff. There is no possible way I could have passed those courses without that accommodation.

     

    I do appreciate your word on not "over diving" the audio pressure. Without a limiting device, it would be impossible to turn the levels down fast enough. The radio DJ's had something called an optimod that would ake their signal and boost it up to the maximum (I had a friend that was in the radio business that used these kinds of systems. I looked it up Orban still manufactures this type of equipment (OPTIMOD-FM 8700i) audio processing. This is not for audiophiles because there is suppression as well as pushing sound levels (so more noise etc.) These devices try to take the input signal and output a consistent full bandwidth signal.