Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum BCM2835 and SPI Transfers
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 5 answers
  • Subscribers 708 subscribers
  • Views 3888 views
  • Users 0 members are here
  • raspberry_pi
Related

BCM2835 and SPI Transfers

ceeej
ceeej over 7 years ago

I'm using a Pi3 to control a PLL (ADF4351) which requires an initial load of 6 32 bit config words to be sent via SPI, MSB first.

 

I've succesfully used BCM2835 to handle SPI before with a MCP23S17 so I know the library works and is installed correctly.

 

But, the 32 bit word thing, perhaps I'm missing something (likely) but I can't work out how to transfer more than 16 bits in one go, I can of course 'twiddle' the data to  make it work with bcm2835_spi_write but that feels unnecessarily awkward and not a little inelegant so, is it possible to do a 32 bit transfer using BCM2835 elegantly or do I need to start bit shifting and masking?

 

 

Any advice (except use another language) welcome and thanks in advance,

 

Clint

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 7 years ago

    You need to provide more information:

    SPI0 is different from SPI1 and 2 - which are you using ?

     

    Which language and which library are you using ?

     

    Have you read the Broadcom peripheral data sheet for the BCM2835?

     

    SPI0 supports  LOSSI which is not very common.

     

    SPI1 and 2 support 32 bit transfers in hardware.

     

    (Just saw Roger's post - sorry about duplication.)

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 7 years ago in reply to michaelkellett

    Repetita juvant, it seems

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 7 years ago in reply to michaelkellett

    Repetita juvant, it seems