Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum BCM2835 and SPI Transfers
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 5 answers
  • Subscribers 708 subscribers
  • Views 3891 views
  • Users 0 members are here
  • raspberry_pi
Related

BCM2835 and SPI Transfers

ceeej
ceeej over 7 years ago

I'm using a Pi3 to control a PLL (ADF4351) which requires an initial load of 6 32 bit config words to be sent via SPI, MSB first.

 

I've succesfully used BCM2835 to handle SPI before with a MCP23S17 so I know the library works and is installed correctly.

 

But, the 32 bit word thing, perhaps I'm missing something (likely) but I can't work out how to transfer more than 16 bits in one go, I can of course 'twiddle' the data to  make it work with bcm2835_spi_write but that feels unnecessarily awkward and not a little inelegant so, is it possible to do a 32 bit transfer using BCM2835 elegantly or do I need to start bit shifting and masking?

 

 

Any advice (except use another language) welcome and thanks in advance,

 

Clint

  • Sign in to reply
  • Cancel
Parents
  • adominator
    0 adominator over 6 years ago

    Well, I wish I could've gotten here earlier, but I stumbled upon this post while searching the web trying to find an answer for basically the same issue but this was while I was rewriting aspects of the BCM2835 to serve other purposes. What I found, but haven't implemented yet, is that you can modify the DLEN Register to the number of bytes you wish to send, and this can be done using Direct Memory Access(DMA) setup by the bcm2835 library through this function call: bcm2835_peri_write(bcm2835_spi0 + BCM2835_SPI0_DLEN/4, numOfBytes);

     

    BCM2835_SPI0_DLEN is divided by 4 since the addresses used are for 4 byte words so the address of the register needs to be divided by 4 in order to correct for DMA.

     

    If you want to look into this more, look at page 156 of the BCM2835 ARM Peripherals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • adominator
    0 adominator over 6 years ago

    Well, I wish I could've gotten here earlier, but I stumbled upon this post while searching the web trying to find an answer for basically the same issue but this was while I was rewriting aspects of the BCM2835 to serve other purposes. What I found, but haven't implemented yet, is that you can modify the DLEN Register to the number of bytes you wish to send, and this can be done using Direct Memory Access(DMA) setup by the bcm2835 library through this function call: bcm2835_peri_write(bcm2835_spi0 + BCM2835_SPI0_DLEN/4, numOfBytes);

     

    BCM2835_SPI0_DLEN is divided by 4 since the addresses used are for 4 byte words so the address of the register needs to be divided by 4 in order to correct for DMA.

     

    If you want to look into this more, look at page 156 of the BCM2835 ARM Peripherals.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer