Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Gertboard Compatibility with Raspberry Pi 4b
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 704 subscribers
  • Views 788 views
  • Users 0 members are here
  • raspberry_pi
Related

Gertboard Compatibility with Raspberry Pi 4b

raspman_5984
raspman_5984 over 6 years ago

Is the Gertboard compatible with the Raspberry Pi 4b? It looks like it could be a great add-on.

Thanks in advance.

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 6 years ago

    If memory serves me right there were two versions. If we were taking of the later one, it should. But the raspian Os has had several changes that may inhibit some functions possibly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gdstew
    0 gdstew over 6 years ago

    As far as I know you should be able to use a Gertboard with a RPi 4 using a 26 pin ribbon cable connected to the first 26 pins of the GPIO connector like it was

    done when they originally changed over to the 40 pin connector.  There are differences in GPIO register addresses between 256 MB, 512 MB, and 1 GB (?) RAM

    versions of the earlier RPis, and I believe the RPi 4 has different register addresses than all of the previous versions, that will prevent older software from working

    without changing the addresses in the software first. The register addresses should be the same for the RPi 4 regardless of how much RAM it has. There are also

    a few changes on which physical port pins on the different Broadcom SoCs are connected to the GPIO connector so software written for the earlier RPis will need

    to be adjusted to fix that. There are no differences in the physical interface between the two versions of the Gertboard that I am aware of.

     

    I have one each of both versions of the Gertboard and would be interested in finding out if anyone has modified software or a Gertboard library that has kept up

    with these changes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer