Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Battery Powered Raspberry PI Zero W
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 19 replies
  • Answers 11 answers
  • Subscribers 705 subscribers
  • Views 10442 views
  • Users 0 members are here
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Battery Powered Raspberry PI Zero W

iec
iec over 6 years ago

I am planning on building a mobile raspberry pi project, I have read many of the battery powered threads but do not have an EE background so I want to make sure that what I am planning on buying will work.

 

These items are all from adafruit

 

  • Lithium Ion Polymer Battery - 3.7v 2500mAh - pid 328 - chosen for slimline i.e. height
  • USB LiIon/LiPoly charger - v1.2 - pid 259
  • Raspberry PI Zero W - pid 3400

 

Is the lipoly charger the right board to power the pi and perhaps a small fan such as the Miniature 5V Cooling Fan for Raspberry Pi pid 3368

How long will the pi run with this battery?

Should I choose a different battery - smaller - larger?

What other questions should I consider for this project?

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 6 years ago

    Hi Eric,

     

    I'm unfamiliar with the Pi Zero W, but as I understand, it needs 5V for operation. If that's the case, then you'll need a board that can convert the battery voltage to 5V. If you search for 'Pi Zero W LiPo' you'll find some solutions.

    Aside from that, the items you've listed above would be required. A cooling fan is unnecessary (Pi Zero W won't get remotely hot for this to be needed) and will consume a lot of power and could cause complications.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • easyejl
    0 easyejl over 6 years ago

    Other questions you should answer for completeness

     

    • Is there any display?
    • Is there going to be audio out and will it be powered by the same battery?
    • How long do you expect it to run for between charges?
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • iec
    0 iec over 6 years ago in reply to easyejl
    • Is there any display?
      • no
    • Is there going to be audio out and will it be powered by the same battery?
      • no
    • How long do you expect it to run for between charges?
      • at least a couple of hours
    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • iec
    0 iec over 6 years ago in reply to shabaz

    thanks for the reply

     

    I'm unfamiliar with the Pi Zero W, but as I understand, it needs 5V for operation. If that's the case, then you'll need a board that can convert the battery voltage to 5V. If you search for 'Pi Zero W LiPo' you'll find some solutions.

    Aside from that, the items you've listed above would be required. A cooling fan is unnecessary (Pi Zero W won't get remotely hot for this to be needed) and will consume a lot of power and could cause complications.

    the USB LIION/LIPOLY CHARGER that I chose looks to me like it can handle 5v and that it can power the pi and charge at the same time am I not correct about this?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to iec

    Hi,

     

    No, that charger supports 5V input for charging the battery, but the load output is the same voltage as the battery, there is no boost type circuit there. According to the schematic, the load is connected to the battery connections:

    https://learn.adafruit.com/li-ion-and-lipoly-batteries/downloads

    A DC-DC converter circuit is needed to increase the voltage to 5V.

     

    Alternatively, a very low cost option could be to use a USB 'power bank' type device (like those used to charge mobile phones) since they accept 5V for charging, and they also output 5V. Many (not all) will stop outputting 5V during charge.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • iec
    0 iec over 6 years ago in reply to shabaz

    so something like this?

    https://www.adafruit.com/product/2465

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to iec

    Hi Eric,

     

    Yes, that will do it, but $20 is a bit of a rip-off for such a hobby type item, considering it is just USB power bank functionality minus the cell. There is this for less than half the price:

    https://www.dfrobot.com/product-1613.html?gclid=EAIaIQobChMIqt3z5cHP5gIVVeDtCh2R0g2nEAkYEiABEgIaKfD_BwE

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • iec
    0 iec over 6 years ago in reply to shabaz

    good deal!, nice, thank you

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • easyejl
    0 easyejl over 6 years ago in reply to iec

    So depending on the specifics of the application, I'd say that you're probably ok with using a battery booster. The other option depending on how small it needs to be is to pick up any cellphone battery pack and use that. I have a 20,000 mah battery pack attached to my pwnagotchi and it lasts well more than 3 days. I can't quite guess how long it really lasts, at 3 days it still had over 50% power. it has an e-ink display, but that draws almost no power as well.

    https://pwnagotchi.ai/


    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mp2100
    0 mp2100 over 6 years ago

    One option for this is from pimoroni

     

    https://shop.pimoroni.com/products/lipo-shim

     

    it provides 1.5 amps which is enough for a Pi zero W and a fan. The zero W is fairly efficient. 

     

    The lipo shim can be used with the included pin header socket, or soldered in permanently if you are sure that’s what you want.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
>