Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Building a Pi WiFi radio receiver controlled by vintage aircraft instruments. Some pointers, please ?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 30 replies
  • Answers 16 answers
  • Subscribers 706 subscribers
  • Views 6290 views
  • Users 0 members are here
  • raspberry_pi
Related

Building a Pi WiFi radio receiver controlled by vintage aircraft instruments. Some pointers, please ?

marco'polo
marco'polo over 6 years ago

Hello, new to this forum, I am seeking some help to get started in the right direction with this project.

 

My goal is to build a WiFi radio receiver with speakers operated by RP and controlled by vintage aircraft cockpit instruments, probably a Pi3+ (?). It needs to look nice and be original.

 

Here's an example of the radio part, with credits to Bob Rathbone

https://bobrathbone.com/raspberrypi/pi_internet_radio.html

There are exquisite instructions and manuals by him on how to build the radio part of this project so that is not my question.

image

 

Here's the twist and where I need to help getting started. I have 5 of these 80s analog, precise, unused instrument controllers. I would like to incorporate these to replace the stock rotary dials and control channel and volume. It would look cool, be original, but.... I don't know how to use the controller to feed inputs to the RP.

 

imageimageimage

Idea1: In the back there is a 37 pinout D-bus terminal. The most elegant would be to buy some female 37 pin board converter and find a way to feed the input to the RP, perhaps via the GPIO of the RP. I don't have a mapping of each pin's purpose, the closest I could find is in the pic below.

Does anyone have an idea how to discover the use of each pin and how to turn that into a listening variable input into a program on the RP ?

image

 

Idea2: If all else fails, there may be a brute force method of removing the backplate and gluing some rotary knob controller directly onto the disc. Might function but not elegant.

 

Expanding the project, I could even add some electric dial powered instruments/gauges to show volume level setting by feeding the right input back to the instrument.

 

imageimage

 

 

I would greatly appreciate if anyone could give me some general steps and ideas to follow especially for idea 1 above. THANKS!

  • Sign in to reply
  • Cancel
Parents
  • phoenixcomm
    0 phoenixcomm over 6 years ago

    marco First, Let me assure you this is not rocket science! You have the pin-out, or you can generate one your self, DVM to ground. and then probe. The good news is your print. above looks ok, So. Take a deep breath. I believe your pinouts show the tuning frequencies. What you have is only a Radio Head, ie each head has its own black box, radio. So for your indicated frequency "820Khz pins 12 and 6 will be connected via ground.  now with that said the BFO switch is SPST.  Then the function switch test/ADF/ant/off is just a rotary switch. All of this can be handled by Arduino. Now you have to send you selected frequency to your radio (pi whatever). since this is a Fixed system your and your Radio Heading will not work.  unless you just want to point to the radio station from where you are.

    I am working on a project Nexgen. I have a motto: 1) Do not harm to the equipment. 2) see rule 1, rules  3 -9 see rule 1. rule 10 ) for vacuum drivin stuff you will have to convert to small stepper! Another one is my fuel gauge there are no docs and everybody says property. Which leads me to rule 11)  Abuse it if you must!

    https://community.element14.com/resized-image/__size/620x300/__key/communityserver-discussions-components-files/91/contentimage_5F00_205930.htmlimage

    NexGen Flight Simulator

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to phoenixcomm

    BTW only the panel lamps run on 28vdc.  The rest use TTL levels and use pull resistors or the internal ones. and here is a link to my https://community.element14.com/resized-image/__size/620x300/__key/communityserver-discussions-components-files/91/5460.contentimage_5F00_205930.htmlRMI page

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to phoenixcomm

    BTW only the panel lamps run on 28vdc.  The rest use TTL levels and use pull resistors or the internal ones. and here is a link to my https://community.element14.com/resized-image/__size/620x300/__key/communityserver-discussions-components-files/91/5460.contentimage_5F00_205930.htmlRMI page

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to phoenixcomm

    BTW please look at my blogs about the Audio challenge The formulas are not really correct as they are for RADAR, not radio. The formulas in my next blog will have radio distance over the sea and that works for DME.  Now saying that ADF is very different it's mostly in AM radio band 19Khz to 1.75Mhz so the stations have bigger power and the antennas are much taller ie ABC was in Lodi, Nj but has 50kw output. At one point they transmitted from the top of the Empire State Building (1,250' + 200') and World Trade Towers. therefore height and power matter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • phoenixcomm
    0 phoenixcomm over 6 years ago in reply to phoenixcomm

    One last BTW if you use multiple heads you will have to devise a switching mechanism of sorts. One way is to use I/O expanders (I2C) or use separate Arduino per head (best as each radio head requirements are a little different.  One last thing Audio is a mess!! you can switch them with CMOS switches.  I aircraft you have a radio selector box with isolation amps one per channel and them mixed together (that is the selected ones with there own volume control). Since you can't do this you will be limited to one control head at one time. so you will have to fake it. Pi audio output can go and switch them with CMOS switches. that way each radio volume will work. FINS

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer