Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is there a way to customize the Raspbian OS
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 704 subscribers
  • Views 3995 views
  • Users 0 members are here
  • raspberry pi 4b
  • rasberry_pi_3_b_plus
  • raspberry_pi
Related

Is there a way to customize the Raspbian OS

movlbobl
movlbobl over 6 years ago

Is there a way I can customize the Raspbian Buster img File?

 

Here's what I want to customize:

1. For the first boot setup screen I want to only 9 specific countries along with 1 generic no country specific setting and the ability to add more countries if needed.

2. For those 9 countries I want 27 specific cities with the ability to add more if needed.

3. Set up specific Password Requirements for certain countries, i.e. Mexico needs 15 characters, France needs 11 characters and New Zealand only needs 6 characters.

4. Setting up IP addresses like IPv4, Gateway and netmask that can connect with other servers within a local network.

5. Customize packages on Raspian to add custom packages I do need and to take away packages I don't need i.e. Scratch.

6. Make my own software repository tree for future builds of the OS, for instance to build .iso and .img files.

7. Set Root and the Bootloader (if possible) passwords.

8. Set different accounts from the start.

 

My plan is to run this on a RaspberryPi 4, 1GB RAM and 4G RAM, I will also be comparing this by running the RaspberryPis with Fedora, and Chromium OS with the same qualifications.

 

I banned form the RaspberryPi forum for a month because I was being to confusing for them and kept insisting I didn't know what I was talking about.

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 6 years ago

    Hello,

    IMHO, you mentioned the question in a way that the notable friends above mentioned immediately the Linux rebuild option. I have done this on other kinds of Linux platforms for embedded devices (as a job) in past, but this is a very complex work that also requiring a lot of testing to be sure you reach a stable version.

     

    But... I think that if we see things from a different point of view, there is a more light perspective that may be helpful in saving you time ad big efforts. Consider that most (or all, I am not sure) of the changes you need can be just obtained customizing a pilot standard Raspberry Buster setup. At least it is what I have done in many different cases.

     

    Focus on the changes that you need and see how to do them using the normal Linux tools starting from a standard Raspbian version.

    Create an image of the modified installation

    Use it for set up all the other Raspberry Pi you need just like using the standard Buster image you downloaded from the official site.

     

    In addition, if something should be custoimzed after the first boot, follow the suggestion of clem57 and write down a first boot script that self-delete itself after setting the needed changes.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 6 years ago

    Hello,

    IMHO, you mentioned the question in a way that the notable friends above mentioned immediately the Linux rebuild option. I have done this on other kinds of Linux platforms for embedded devices (as a job) in past, but this is a very complex work that also requiring a lot of testing to be sure you reach a stable version.

     

    But... I think that if we see things from a different point of view, there is a more light perspective that may be helpful in saving you time ad big efforts. Consider that most (or all, I am not sure) of the changes you need can be just obtained customizing a pilot standard Raspberry Buster setup. At least it is what I have done in many different cases.

     

    Focus on the changes that you need and see how to do them using the normal Linux tools starting from a standard Raspbian version.

    Create an image of the modified installation

    Use it for set up all the other Raspberry Pi you need just like using the standard Buster image you downloaded from the official site.

     

    In addition, if something should be custoimzed after the first boot, follow the suggestion of clem57 and write down a first boot script that self-delete itself after setting the needed changes.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer