Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi Desktop: max current output?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 703 subscribers
  • Views 2042 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Pi Desktop: max current output?

rootard
rootard over 6 years ago

Hello

 

I have purchased a Element14 Pi Desktop that I'm using with my Pi 3B+ and the original Raspberry 2.5A PSU.


So far it was running fine with the RTC hat + SSD + 2 fans on the GPIO (1 for the heatsink and one for the case) + an Aeotec ZWave key connected on the USB port.

However the Pi froze after a few hours when I added an USB RFXCom device.

I suspect a power issue. I've tried to used a bigger 3A PSU with same results.

 

What is the maximum current provided by the Pi Desktop Hat?

Is there a fuse limiting the power provided to the Pi board?

Is there a way to solder the fans directly to the Hat input in order to avoid voltage drop? If yes on which pins?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 6 years ago

    A Pi 3 doesn't need two fans. It's even possible to use fully passive heatsinking with the Pi 3 under full load, but that's difficult with that enclosure.

    The fans will be consuming most power, not the RFXCom device or your other wireless device. If you can remove one fan, then there's a fair chance you may be ok in terms of power consumption, and it will still run at full speed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    A Pi 3 doesn't need two fans. It's even possible to use fully passive heatsinking with the Pi 3 under full load, but that's difficult with that enclosure.

    The fans will be consuming most power, not the RFXCom device or your other wireless device. If you can remove one fan, then there's a fair chance you may be ok in terms of power consumption, and it will still run at full speed.