Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum 20 pin ZIF connector to raspberry pi!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 3 answers
  • Subscribers 706 subscribers
  • Views 2115 views
  • Users 0 members are here
  • raspberry_pi
  • lcd screen
  • raspberry_pi3
Related

20 pin ZIF connector to raspberry pi!

samthefearful36
samthefearful36 over 6 years ago

So I took apart some old DV cameras and saw that they have tiny LCD panels inside the viewport and was wondering if I could hook these up to a raspberry pi. Does anyone know how to find the traces to get an image going?

I am willing to buy adapters as needed, thanks!

imageimage

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 6 years ago
    May I ask what information you would need

     

    Hi Samuel,

    From the two photos, it's not guessable which make/model of camcorder it came from. So, it's going to be very hard for anyone to speak up if they've managed to reverse-engineer the same model as the one you have, because they won't know which make/model you have, and so at least that information can help. It won't even come up in a google search (if someone searches for that particular model) since it's a photo. The make/model needs to be written down in your question or a comment, to increase your chances of finding someone who has worked with it before.

     

    Secondly, the amount of people out there who may have reverse engineered that same camcorder and who happen across the question+photo, are likely to be extremely low. You can increase the chances of getting information that might help, if you can provide photographs of the insides with chipset markings at least visible. The reason is, the flat-flex connection is not a standard, it can be used for many purposes, so it's not possible to tell much from the photo so far (except that some of the traces are wider and they may be power traces).

     

    I am willing to buy adapters as needed

    Just to set expectations, you're likely to need more than that - perhaps a custom PCB designed to attach to the connector. The reason is, it is an internal interface (not like a standard USB or RS232 interface) from a 20-year-old device. Realistically, it is going to be unlikely there are ready-made adapters for it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago
    May I ask what information you would need

     

    Hi Samuel,

    From the two photos, it's not guessable which make/model of camcorder it came from. So, it's going to be very hard for anyone to speak up if they've managed to reverse-engineer the same model as the one you have, because they won't know which make/model you have, and so at least that information can help. It won't even come up in a google search (if someone searches for that particular model) since it's a photo. The make/model needs to be written down in your question or a comment, to increase your chances of finding someone who has worked with it before.

     

    Secondly, the amount of people out there who may have reverse engineered that same camcorder and who happen across the question+photo, are likely to be extremely low. You can increase the chances of getting information that might help, if you can provide photographs of the insides with chipset markings at least visible. The reason is, the flat-flex connection is not a standard, it can be used for many purposes, so it's not possible to tell much from the photo so far (except that some of the traces are wider and they may be power traces).

     

    I am willing to buy adapters as needed

    Just to set expectations, you're likely to need more than that - perhaps a custom PCB designed to attach to the connector. The reason is, it is an internal interface (not like a standard USB or RS232 interface) from a 20-year-old device. Realistically, it is going to be unlikely there are ready-made adapters for it.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • samthefearful36
    0 samthefearful36 over 6 years ago in reply to shabaz

    I thought so also but what caught my attention was that it had 20 pins, much like the pi screen? However, if I can't just right up connect it I'm going to ditch the project for now.

     

    The camera model is a sony dcr-trv33.

     

    I am sure it is an LCD display because of color and no artifacts near magnets and the 20 pins, most CRT based displayed have 4 pins. 2 for power and 2 for composite.