Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help: Encountering CAN Bus Problem on SmartEdge IIoT Gateway
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 27 replies
  • Answers 17 answers
  • Subscribers 706 subscribers
  • Views 7480 views
  • Users 0 members are here
  • raspberry_pi
  • raspberrypi
  • smartedge iiot gateway
  • canbus
Related

Help: Encountering CAN Bus Problem on SmartEdge IIoT Gateway

khz_321
khz_321 over 6 years ago

Hi All,

 

I was wondering if anyone has had any experience using the CAN Controller on the SmartEdge IoT Gateway

The box has a Built-in MCP2515 CAN Controller on board, which is great & why I selected it for a project that requires CAN

 

For the most part, it works fine, but every so often I'm encountering "Garbage" data coming from the chipset (at a rate of about 1 message every 10 mins with a message cycle of 100ms)

This is shown below, when simply monitoring using candump and nothing else

 

image

the shown 67 EB in bytes 7 & 8 are the bits Garbage Data in question. It should be noted that when I do get the garbage, its always the same 2 Bytes and same values.

 

The sender device is broadcasting the same message repeatedly, so there should be no changes at all!

 

I was also able to confirm that it is not present on the physical bus by using a PCAN USB and datalogging with Pcan-View at the same time.

The data dump from Pcan-View shows no messages like the one highlighted!

 

Seems like this is happening on the Controller Hardware or Driver Implementation side on the IIoT Gateway

Anyone encountered this before? Either on this product or any other Raspberry Pi ?

 

I've tried adjusting the bit timing, sampling point, everything I could think of, but still encountering a random error every so often

 

Here is my CAN settings from /etc/network/interfaces

 

auto can0
iface can0 inet manual
   pre-up /sbin/ip link set can0 type can bitrate 250000 sample-point 0.875 triple-sampling on
   up /sbin/ifconfig can0 up
   down /sbin/ifconfig can0 down

 

And here is the output of ip -details -statistics link show can0

ip -details -statistics link show can0
4: can0: <NOARP,UP,LOWER_UP,ECHO> mtu 16 qdisc pfifo_fast state UNKNOWN mode DEFAULT group default qlen 10
    link/can  promiscuity 0 
    can <TRIPLE-SAMPLING> state ERROR-ACTIVE restart-ms 0 
  bitrate 250000 sample-point 0.875 
  tq 250 prop-seg 6 phase-seg1 7 phase-seg2 2 sjw 1
  mcp251x: tseg1 3..16 tseg2 2..8 sjw 1..4 brp 1..64 brp-inc 1
  clock 8000000
  re-started bus-errors arbit-lost error-warn error-pass bus-off
  0          0          0          0          0          0         numtxqueues 1 numrxqueues 1 gso_max_size 65536 gso_max_segs 65535 
    RX: bytes  packets  errors  dropped overrun mcast   
    17224264   2153033  0       1508    0       0       
    TX: bytes  packets  errors  dropped carrier collsns 
    16         2        0       0       0       0

 

Note: Kernel Version 4.14.79-v7+, & Software Image: avnet_iot_demo_20190719a_shrink

(Also tried with latest release avtse-iiotg-v-11-20200326.img, which apparently updated the MCP2515 driver, but problem still persists)

 

Any advice? 

  • Sign in to reply
  • Cancel
Parents
  • waynepeters10
    0 waynepeters10 over 5 years ago

    There are 2 known issues relating to TPM and CAN last byte data corruption.

     

    Solution 1:

    1) login to gateway.

    2) git clone https://github.com/avnet/avtse-iiotg-update.git

    3) cd avtse-iiotg-update

    4) sudo ./install-iot

     

    Solution 2: If you have a custom kernel

    1) replace this file and rebuild your kernel.  Fixes CAN bus last 2 bytes corrupt

    https://github.com/Avnet/smartedge-iiot-gateway/blob/master/drivers/spi/spi-bcm2835aux.c

    2) replace this file /usr/bin/tpm_device_provision with this. Fixes a TPM issue that always existed but the failure was compounded with the SPI driver patch.  Now provides reliable results.

    https://github.com/Avnet/avtse-iiotg-upgrade/blob/master/files/tpm_device_provision

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to waynepeters10

    waynepeters10  wrote:

    ...

    Solution 1:

    1) login to gateway.

    2) git clone https://github.com/avnet/avtse-iiotg-update.git

    3) cd avtse-iiotg-update

    4) sudo ./install-iot

    I'm testing this ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to waynepeters10

    waynepeters10  wrote:

    ...

    Solution 1:

    1) login to gateway.

    2) git clone https://github.com/avnet/avtse-iiotg-update.git

    3) cd avtse-iiotg-update

    4) sudo ./install-iot

    I'm testing this ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 4 years ago in reply to Jan Cumps

    roryyorke ,  the tests look good.

    Here are the first set of results:

    image

     

    I let the test run continuously for approx. 10 minutes, ID 200000, and it didn't report a mismatch.

     

    edit:after 600000 tests, still good:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • roryyorke
    0 roryyorke over 4 years ago in reply to Jan Cumps

    Thanks, Jan Cumps, that looks very promising.  We'll test, hopefully sometime this week, and let you know.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • roryyorke
    0 roryyorke over 4 years ago in reply to roryyorke

    We updated with avtse-iiotg-update, and the issue is solved.

     

    Thanks for the assistance!