Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cross build environment for Raspberry PI (or any Linux SBC) on Windows.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 2 answers
  • Subscribers 703 subscribers
  • Views 1074 views
  • Users 0 members are here
  • cross-compiling
  • raspberry_pi
  • raspberrypi
  • cross-platform
Related

Cross build environment for Raspberry PI (or any Linux SBC) on Windows.

umeshdeshmukh2024
umeshdeshmukh2024 over 6 years ago

I am used to microcontroller code development process. Recently to up my game I am trying to learn programming for raspberry pi.

Building code on Raspberry Pi is very slow.The problems or questions I am facing are given below.

 

1. Why is there are different tool chains for baremetal(arm-none-eabi) and linux target (arm-none-linux-gnueabihf)?

2. How to do cross build for linux device drivers?

3. If you want to cross build using some libraries for example openCV, how to do it?

  • Sign in to reply
  • Cancel
Parents
  • aswinvenu
    0 aswinvenu over 6 years ago

    Hi Umesh,

    Let me answer your question in the same order you asked.

     

    1. Why is there are different tool chains for baremetal(arm-none-eabi) and linux target (arm-none-linux-gnueabihf)?

              This depends on the architecture of the microprocessor/controller. If you have a relatively simple single core system (like ARM Cortex M series R series ) use arm-none-eabi. If you have a application processor like ARM Cortex A series you need to use arm-none-linux-gnueabihf. This is because most of the application processor run with a kernel and operating system. Breaking down the nomenclature GNU Embedded Application Binary Interface. GNU ABIs are standards. You can read about it online.

    Both these are used when you are not planning to run a linux operating system on the processor.

    To note here there are other versions of gnueabi gcc available called arm-none-linux-gnueabi (old versions of raspberry pis used to have this standard). The difference is HF (Hard Float) version has floating point support on the processor. On gnueabi version floating point support has to be added using software (using the same 32 bit length registers).

     

    2. How to do cross build for linux device drivers?

        I personally haven't cross build linux kernel on Windows PC. But when you corss build the Linux kernel driver you need to use arm-linux-gnueabihf- toolchain. Also you need to select the right target platform.

    The make command will look something like this : make ARCH=arm CROSS_COMPILE=<TOOLCHAIN_DIR>/bin/arm-linux-gnueabihf- oldconfig

     

    3. If you want to cross build using some libraries for example openCV, how to do it?

       Okay here openCV is an application code. So you use the same gcc-arm-linux-gnueabihf for cross compiling it. Try to use a virtual machine and run any Linux operating system on that. Then use that for all you crosscompiling experiments. Setting up windows env will sometimes give you headaches.

     

    I think I answered your questions.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • aswinvenu
    0 aswinvenu over 6 years ago

    Hi Umesh,

    Let me answer your question in the same order you asked.

     

    1. Why is there are different tool chains for baremetal(arm-none-eabi) and linux target (arm-none-linux-gnueabihf)?

              This depends on the architecture of the microprocessor/controller. If you have a relatively simple single core system (like ARM Cortex M series R series ) use arm-none-eabi. If you have a application processor like ARM Cortex A series you need to use arm-none-linux-gnueabihf. This is because most of the application processor run with a kernel and operating system. Breaking down the nomenclature GNU Embedded Application Binary Interface. GNU ABIs are standards. You can read about it online.

    Both these are used when you are not planning to run a linux operating system on the processor.

    To note here there are other versions of gnueabi gcc available called arm-none-linux-gnueabi (old versions of raspberry pis used to have this standard). The difference is HF (Hard Float) version has floating point support on the processor. On gnueabi version floating point support has to be added using software (using the same 32 bit length registers).

     

    2. How to do cross build for linux device drivers?

        I personally haven't cross build linux kernel on Windows PC. But when you corss build the Linux kernel driver you need to use arm-linux-gnueabihf- toolchain. Also you need to select the right target platform.

    The make command will look something like this : make ARCH=arm CROSS_COMPILE=<TOOLCHAIN_DIR>/bin/arm-linux-gnueabihf- oldconfig

     

    3. If you want to cross build using some libraries for example openCV, how to do it?

       Okay here openCV is an application code. So you use the same gcc-arm-linux-gnueabihf for cross compiling it. Try to use a virtual machine and run any Linux operating system on that. Then use that for all you crosscompiling experiments. Setting up windows env will sometimes give you headaches.

     

    I think I answered your questions.

     

    Regards,

    Aswin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer