Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Do I need to use an arduino for my pi based robot?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 702 subscribers
  • Views 1051 views
  • Users 0 members are here
  • lidar
  • 3D Printing
  • diy
  • robot learning
  • raspberry pi 3 b+
  • raspberry_pi
Related

Do I need to use an arduino for my pi based robot?

jman095
jman095 over 6 years ago

I want to start this off by saying that I'm kind of a beginner when it comes to more advanced robots. Before this project, the most advanced project I've made was a simple Arduino obstacle avoidance robot with an HC-SR04, so I apologize if I ask anything stupid. I'm in the process of making a 3d printed Raspberry Pi robot, and have been looking at similar projects. My robot is going to use an RPLidar sensor for navigation. I've noticed that similar projects use an Arduino in addition to the Raspberry Pi. I assume the reason for using the Arduino is to control the motors. I am using two geared DC motors (that look like standard size servos), an L298n motor driver, a Raspberry Pi 3b+, and an RPLidar A1 as the main components (I may add a Raspberry Pi Camera later). Is it necessary to include an Arduino? I also wanted to include a rechargeable li-po battery, and decided to use a 7.4v  850mAh battery to power the motors. I just want to make sure that it is safe to do so.

  • Sign in to reply
  • Cancel
  • genebren
    0 genebren over 6 years ago

    Sometimes in a complex project, it is easier to run a second processor (Arduino) to host multiple sensors and report results to a host processor (RPi).  Also, it is possible that the RPi may not have enough I/O pins to dedicate pins to each of the functions that you need, so an Arduino could provide more I/O ports.

     

    Good luck on your robot project.  There should be a lot of good robotics ideas here on the community, be sure to look around and see what others are up to.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer