Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum VM for ARM cpu
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 705 subscribers
  • Views 3995 views
  • Users 0 members are here
  • vm
  • arm
Related

VM for ARM cpu

dr13
dr13 over 5 years ago

Hi, did anybody found a VM running on the ARM cpu.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 5 years ago

    Hi David,

     

    This isn't going to get you useful information, because the next question is, what is your aim? What do you need the VM for?

    What type of virtualization?

     

    If you're asking for this, then you'll know in much more detail what you need it for, and then you'll be in a position to investigate.

    A VM is possible with Linux, google 'linux KVM'. However, it's not the same as on a PC and it won't run PC applications. You need a reasonable technical reason for it in order to use it with ARM. It might not even be the right solution, because you have not specified why you need it..

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dr13
    0 dr13 over 5 years ago in reply to shabaz

    Well my intention is to run windows 10 on the raspberry pi 4 B.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ajcc
    0 ajcc over 5 years ago in reply to dr13

    Searching I was disappointed to find that there are only unofficial builds of Windows 10 on ARM that run on the RPi 4, so I'd probably look into another ARM64 board (more of a laptop honestly) with official builds if you want the full Windows 10 on ARM. Which would be nice because Windows 10 on ARM have x86 emulation already built in, assuming that's the reason why you want a VM on the RPi?

     

    If you just want a Windows environment to run your own programs in on the RPi then there's Windows IoT Core, which was far as I can tell have no (official) support for the RPi 4 yet (or even the RPi 3 B+?).

    If you really want to run a VM on the RPi 4 I'd look into QEMU (you can install aqemu from apt on the RPi to get an easier to use graphical interface for QEMU). Sadly almost everything I find searching for Windows 10 on RPi 4 QEMU are guids on how to run Rasperry Pi OS on a Window PC. This solution will probably require a fast external SSD to be usable.

     

    Good luck with your endeavors!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ajcc
    0 ajcc over 5 years ago in reply to dr13

    Searching I was disappointed to find that there are only unofficial builds of Windows 10 on ARM that run on the RPi 4, so I'd probably look into another ARM64 board (more of a laptop honestly) with official builds if you want the full Windows 10 on ARM. Which would be nice because Windows 10 on ARM have x86 emulation already built in, assuming that's the reason why you want a VM on the RPi?

     

    If you just want a Windows environment to run your own programs in on the RPi then there's Windows IoT Core, which was far as I can tell have no (official) support for the RPi 4 yet (or even the RPi 3 B+?).

    If you really want to run a VM on the RPi 4 I'd look into QEMU (you can install aqemu from apt on the RPi to get an easier to use graphical interface for QEMU). Sadly almost everything I find searching for Windows 10 on RPi 4 QEMU are guids on how to run Rasperry Pi OS on a Window PC. This solution will probably require a fast external SSD to be usable.

     

    Good luck with your endeavors!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dr13
    0 dr13 over 5 years ago in reply to ajcc

    Thanks for the leads. VMware and VirtualBox has VM's for the X86 or the AMD64 instruction set on Windows or Linux OS's. Maybe now that there is Apple's MacBook's with M1 processors built on ARM, those companies will give us a dedicated VM for the ARM architecture.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hugohu
    0 hugohu over 5 years ago in reply to dr13

    ARM is not a single architecture-

     

    Instead, it's a company that makes a ton of them

     

    I think there's ARM 5, ARM72, ARM7. ARM9(these are usually, in my experience found in FPGAs and stuff?)

    Then a ton of ARM M- M0, M0+, M3, M33, M4, M7.