Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum New Person - Need Help Making Raspberry Pi Zero W Portable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 9 answers
  • Subscribers 704 subscribers
  • Views 4229 views
  • Users 0 members are here
  • raspberry pi zero w
  • newbie question
  • raspberry_pi
Related

New Person - Need Help Making Raspberry Pi Zero W Portable

mrmrag
mrmrag over 5 years ago

Hello everyone,

 

I'm very new to electronics and the Raspberry Pi space. I have a problem, and I just don't want to ruin anything.

I want to make my Raspberry Pi Zero W portable using a LiPo battery. I have gotten these links:

 

https://www.adafruit.com/product/2011

^^ The battery I would probably like to use. I would like for it to work for at least 2 hours, maybe more, if I can. I also need to conserve space because I am trying to make smart glasses.

https://www.adafruit.com/product/1304

 

 

 

https://www.adafruit.com/product/3196

^^This PCB to connect the LiPo Battery to the Pi Zero W

 

I am trying to make smart glasses where it takes input from a microphone (hopefully I can get a USB microphone and just connect it to the Raspberry Pi Zero W) and then takes the input, and sends it to my phone via Bluetooth, which then turns the audio to text. After that, it will take that text, send it back to the Raspberry Pi, and puts it up on the screen.

 

Question(s):

1) For the last link, I can't really find if it says that it will support Pi Zero W, it says it supports Pi Zero, does anyone know if it will also support Pi Zero W?

2) Will I need some other PCB to get to voltage to 5V or what I have it is alright?

3) I will also need to add a USB microphone and a small screen. Will this be able to handle it all / will I be able to connect everything onto the Raspberry Pi?

 

Thank you so much for looking at my question. I really appreciate it, and can't thank you enough.

  • Sign in to reply
  • Cancel
Parents
  • fmilburn
    0 fmilburn over 5 years ago

    Hi Fillip


    I have not used the shim but the Pimoroni site gives a bit more information and in the comments several people report using it with the Zero W which draws less power than the Pi 3 which is also mentioned. https://shop.pimoroni.com/products/lipo-shim#show-review

    The TPS61232 in the shim boosts to 5v so that is all you need.

    Small OLED screens require very little power

    There are also very low power mics but I’ve not used USB mics or checked their requirements

    The 2000 mAH battery may not meet your 2 hour requirement - your average current cannot exceed 1 amp and your battery has to meet it’s full rating, be fully charged, and hold voltage down to the cutoff of the boost converter.
    It looks like your choices will get you pretty close or exceed your requirements. Hopefully there is someone here who has actually used the hardware.  Else you might also post on the Pimoroni forums.

     

    Frank

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mrmrag
    0 mrmrag over 5 years ago in reply to fmilburn

    Thank you so much for your reply Frank! I really appreciate it and it will help me with my project, just a follow-up question, are there any quick links to the screens that are compatible with the Raspberry Pi0w, taking into account that I will have the LiPo SHIP in some of the slots(Sorry I don't know the name)?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mrmrag
    0 mrmrag over 5 years ago in reply to fmilburn

    Thank you so much for your reply Frank! I really appreciate it and it will help me with my project, just a follow-up question, are there any quick links to the screens that are compatible with the Raspberry Pi0w, taking into account that I will have the LiPo SHIP in some of the slots(Sorry I don't know the name)?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fmilburn
    0 fmilburn over 5 years ago in reply to mrmrag

    That is a good question.  It appears Pimoroni  does not give us a schematic for the SHIM which would be helpful but the header on the LiPo SHIM covers up SCL and SDA.  I am not sure it is using I2C because the TPS61232 doesn't need it.  In any event I2C can handle more than one device.  SPI is not covered up which is good.

     

    So when evaluating displays look for what pins are needed and realize the display cannot be directly placed onto the Pi.  I assume you are placing the display away from the Pi so jumpers/wire is needed.  If I2C is needed the pins will be covered up by the SHIM but you can solder wires between the display and the SHIM which is a bit of a hack.  SPI would be less of a problem it would appear as the pins are not covered up so solder directly to the Pi pads.  Look for displays that advertise they are useable with the Pi.  If you are concerned about your choice, make a new post here on Element14.  It sounds like an interesting project...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mrmrag
    0 mrmrag over 5 years ago in reply to fmilburn

    Hello, I'm so sorry for bothering you, again, I really hope this is one of the last times. So I have been looking at some displays, and there is really only one that looks to be good.

     

    https://www.adafruit.com/product/326#technical-details

    ^ This one says that it can be used with either SPI or I2C interface, so using SPI would be easier. It doesn't say that it can work with Raspberry Pi, but I also found it in this instruction where the same website tells you how to wire it: https://learn.adafruit.com/monochrome-oled-breakouts/python-wiring

     

    Unfortunately, that site only shows how to wire it using the I2C interface, so that might be a problem for me in the future if I buy this one, but I will definitely figure it out.

     

    I also found this one, I also found a guide to go along with it, this screen is just transparent unlike the first one:

    https://www.crystalfontz.com/product/cfal12856a00151b-128x56-transparent-oled-screen

    ^Display

    https://www.crystalfontz.com/product/cfa10105-oled-breakout-board

    ^Breakout board

    https://www.crystalfontz.com/blog/transparent-oled-on-raspberry-pi/

    ^

     

     

     

    1) Looking at the Breakout Board, would I be able to snap off the top part? Just because I won't use it and it will just take up space or is it a permanent part of the board?

     

    Overall I just wanted to confirm that those displays were okay to use. Thank you so much, and I'm sorry again.

     

    Fillip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fmilburn
    0 fmilburn over 5 years ago in reply to mrmrag

    The CrystalFonz display looks pretty cool, below is from their web page:

     

    This display supports, parallel, I2c, and SPI interfaces. We powered it up using an 3.3v Seeeduino/Arduino UNO Clone and a small break-out board. This little OLED uses the super common Solomon Systech SSD1309 integrated controller.

     

    I did a quick search and see where some claim the Systech SSD1309 controller can work with the Adafruit libraries but you will need to confirm that somehow or find a driver elsewhere.  You need that snap off PCB - it has all the goodies needed to connect it to a microcontroller or Pi.  You could perhaps snap it off and place it perpendicular to the display but it has to be connected.  Try contacting CrystalFonz and see what they say about that as well as drivers for the Pi.

     

    I have used the display that Adafruit is selling with microcontrollers but not the Pi and like it.  It looks like the SPI settings for the 0.96 128x64 are down at the very bottom of the page you have linked.

     

    Good luck image