Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum New Person - Need Help Making Raspberry Pi Zero W Portable
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 9 answers
  • Subscribers 704 subscribers
  • Views 4229 views
  • Users 0 members are here
  • raspberry pi zero w
  • newbie question
  • raspberry_pi
Related

New Person - Need Help Making Raspberry Pi Zero W Portable

mrmrag
mrmrag over 5 years ago

Hello everyone,

 

I'm very new to electronics and the Raspberry Pi space. I have a problem, and I just don't want to ruin anything.

I want to make my Raspberry Pi Zero W portable using a LiPo battery. I have gotten these links:

 

https://www.adafruit.com/product/2011

^^ The battery I would probably like to use. I would like for it to work for at least 2 hours, maybe more, if I can. I also need to conserve space because I am trying to make smart glasses.

https://www.adafruit.com/product/1304

 

 

 

https://www.adafruit.com/product/3196

^^This PCB to connect the LiPo Battery to the Pi Zero W

 

I am trying to make smart glasses where it takes input from a microphone (hopefully I can get a USB microphone and just connect it to the Raspberry Pi Zero W) and then takes the input, and sends it to my phone via Bluetooth, which then turns the audio to text. After that, it will take that text, send it back to the Raspberry Pi, and puts it up on the screen.

 

Question(s):

1) For the last link, I can't really find if it says that it will support Pi Zero W, it says it supports Pi Zero, does anyone know if it will also support Pi Zero W?

2) Will I need some other PCB to get to voltage to 5V or what I have it is alright?

3) I will also need to add a USB microphone and a small screen. Will this be able to handle it all / will I be able to connect everything onto the Raspberry Pi?

 

Thank you so much for looking at my question. I really appreciate it, and can't thank you enough.

  • Sign in to reply
  • Cancel
Parents
  • hugohu
    0 hugohu over 5 years ago

    Hi.

     

    The second link is only a charger.

     

    Lithium Polymer Batteries have a typical output voltage of 3.7V

     

    ***this information may be incorrect but the general idea is correct***

     

    You'll need a booster to bring that up to 5V.

    https://www.adafruit.com/product/2465

     

    Perhaps?

     

    That's my go-to suggestion, since it comes with battery charging, USB 5V out, etc.

     

    The Pi0 and Pi0W are essentially the same thing. The only thing is that one has wifi, one does not, and some parts aren't in same place(but camera, SD, GPIO, power/data, hdmi) are all the same.

     

    2 hours?

     

    I see here the pi 0 uses 120mA at idle and 170 watching 1080 HD video.

     

    With screen, I'd assume, perhaps, 130mA? An OLED would be suitable.

     

    (Monochrome, I mean)

     

    The battery indicated has 2000mA

     

    I'd suppose 300mA then an additional 50mA(this is pure guesswork) for bluetooth.

     

    it should, in theory work.

     

    You can also get 1A or so with that powerboost.

     

    let me know how the project goes.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mrmrag
    0 mrmrag over 5 years ago in reply to hugohu

    Thank you so much for your reply! I really appreciate it, just a follow-up question, are there any quick links to the screens that are compatible with the Raspberry Pi0w, taking into account that I will have the LiPo SHIP in some of the slots(Sorry I don't know the name)?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hugohu
    0 hugohu over 5 years ago in reply to mrmrag

    I’m on mobile but I will check the pin outs.

    due to this I recommend the power boost. Its USB.

    Pj screen? Adafruit screens are pretty nice, might be a bit expensive. There are cheaper 3.5” screens via GPIO on Amazon with less documentation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • hugohu
    0 hugohu over 5 years ago in reply to mrmrag

    I’m on mobile but I will check the pin outs.

    due to this I recommend the power boost. Its USB.

    Pj screen? Adafruit screens are pretty nice, might be a bit expensive. There are cheaper 3.5” screens via GPIO on Amazon with less documentation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer