Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Insight why display fails with buffer board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 16 answers
  • Subscribers 703 subscribers
  • Views 6384 views
  • Users 0 members are here
  • raspberry pi display
  • lcd display
  • spi data
  • raspberry_pi
Related

Insight why display fails with buffer board

colporteur
colporteur over 5 years ago

Can someone share their insight  into why no images are displayed on the LCD display when a buffer/level shifter board is inserted between the Pi and the display?

 

The project is to display images on a 1.3 inch display using a Raspberry Pi. Inspiration for the project came from Episode 465: Lego Raspberry Pi HQ Camera . I'm using the LCD screen Katie's  hifromkatie used in the project.

 

I can display images on the display https://github.com/pimoroni/st7789-python  connected directly to the Pi. Images are not displayed if I insert a buffer board between the Pi and the display. I have tried modules with TXS0108E and BSS138 chips and get the same results.

 

Attached is the pin out for connections. I confess I have limited experience with this communication protocol. I was hoping the buffer would provide some isolation for the Pi to enable me to move the display away from the Pi. I assumed a level shifter would not introduce issues but that does not appear to be the case.

 

Can you share any insight into what is causing the issue and possible solution.

 

 

 

image

 

Message was edited by: sean conway I added pictorials of the buffer/level shifting modules. The module on the left is is based on the TXS0108E chip and the right is a BSS138 fet based on an adafruit model https://www.adafruit.com/product/757

  • Sign in to reply
  • Cancel
Parents
  • Gough Lui
    0 Gough Lui over 5 years ago

    My best guess is that you're using level shifter boards or wiring which is too slow to accommodate the high-speed SPI that the display is demanding.

     

    The code you are using has this in the ST7789's __init__.py:

    SPI_CLOCK_HZ = 16000000

     

    This tells me that the communications between the Pi and the screen are going at 16MHz. This is not a speed you can just carelessly whip around jumper wires or any-old-level-shifter. My guess is the BSS138-based shifter you're using is one intended for I2C usage which is only 0.4MHz in the "fast" mode. The TXS0108E may well be able to do it - it does say it can do 60Mbps maximum at 3.3V in push-pull which is plenty but only 2Mbit/s in open-drain (check the configuration of the module you're using). But I fear that the wiring you're using just may not be good enough to get 16MHz consistently - I've not had much luck myself above 8MHz going with jumper wires. Long wires add capacitance that will serve to increase the load on the drivers and round-off your edges, but also have a tendency to radiate signal so may even cause radio interference to nearby electronics.

     

    Probably best to get a scope onto the lines with the display load connected to see what is arriving at the display ... I suspect the signal just isn't clean. Perhaps another way is to try and modify the library and use a slower SPI clock and see if the display would come up (perhaps with reduced performance if not timing critical).

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 5 years ago

    My best guess is that you're using level shifter boards or wiring which is too slow to accommodate the high-speed SPI that the display is demanding.

     

    The code you are using has this in the ST7789's __init__.py:

    SPI_CLOCK_HZ = 16000000

     

    This tells me that the communications between the Pi and the screen are going at 16MHz. This is not a speed you can just carelessly whip around jumper wires or any-old-level-shifter. My guess is the BSS138-based shifter you're using is one intended for I2C usage which is only 0.4MHz in the "fast" mode. The TXS0108E may well be able to do it - it does say it can do 60Mbps maximum at 3.3V in push-pull which is plenty but only 2Mbit/s in open-drain (check the configuration of the module you're using). But I fear that the wiring you're using just may not be good enough to get 16MHz consistently - I've not had much luck myself above 8MHz going with jumper wires. Long wires add capacitance that will serve to increase the load on the drivers and round-off your edges, but also have a tendency to radiate signal so may even cause radio interference to nearby electronics.

     

    Probably best to get a scope onto the lines with the display load connected to see what is arriving at the display ... I suspect the signal just isn't clean. Perhaps another way is to try and modify the library and use a slower SPI clock and see if the display would come up (perhaps with reduced performance if not timing critical).

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to Gough Lui

    I'm using this design for FPGA level shifting: Make a Logic Analyzer from your Dev Kit Part 3: Level Translator and Buffer

     

    A shifter - not a buffer, and you have to use the exact IC that's listed in the blog. But the IC can handle GHz. 16 data lines.

    The use case here is one direction. But not sure if the use case needs a buffer. It's not common in this scenario. These displays are made to directly attach to the logic and seem voltage compliant.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer