Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Insight why display fails with buffer board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 16 answers
  • Subscribers 703 subscribers
  • Views 6394 views
  • Users 0 members are here
  • raspberry pi display
  • lcd display
  • spi data
  • raspberry_pi
Related

Insight why display fails with buffer board

colporteur
colporteur over 5 years ago

Can someone share their insight  into why no images are displayed on the LCD display when a buffer/level shifter board is inserted between the Pi and the display?

 

The project is to display images on a 1.3 inch display using a Raspberry Pi. Inspiration for the project came from Episode 465: Lego Raspberry Pi HQ Camera . I'm using the LCD screen Katie's  hifromkatie used in the project.

 

I can display images on the display https://github.com/pimoroni/st7789-python  connected directly to the Pi. Images are not displayed if I insert a buffer board between the Pi and the display. I have tried modules with TXS0108E and BSS138 chips and get the same results.

 

Attached is the pin out for connections. I confess I have limited experience with this communication protocol. I was hoping the buffer would provide some isolation for the Pi to enable me to move the display away from the Pi. I assumed a level shifter would not introduce issues but that does not appear to be the case.

 

Can you share any insight into what is causing the issue and possible solution.

 

 

 

image

 

Message was edited by: sean conway I added pictorials of the buffer/level shifting modules. The module on the left is is based on the TXS0108E chip and the right is a BSS138 fet based on an adafruit model https://www.adafruit.com/product/757

  • Sign in to reply
  • Cancel
Parents
  • colporteur
    0 colporteur over 5 years ago

    First, I stabilized power for the display. The display was getting power from the module, not a channel but the power rail, now the display power is completely independent with ground reference the same.

     

    Next, I established a setup that had the display working but enabled me to move each connection to a level converter (one type first and then the second). Any of the signals CS, SCK, MOSI or DC that are moved to the level converters (the two I have on hand) the display doesn't work.

     

    This new knowledge, motivated me to look at how SPI signals are amplified to extend distances. It seems SPI and LED arrays have spawned a number of amplifiers. My research took me to the Open Source Hardware Association link https://www.oshwa.org/a-resolution-to-redefine-spi-signal-names , the fog of my confusion started to lift. I wasn't aware that industry used different nomenclature to describe the signals for the same protocol. Awe Shite, no wonder I was confused.

     

    Self directed learning has it pit falls. If you don't know, what you don't know, how do you know, when you don't know. Oh well, now I know, this has aligned or realigned me towards finding a solution. I have tried to avoid using the adjective "simple" in my dialog. I think it fits in the same category as the words, common sense. Knowledge can lead to understanding that gives the allusion its simple.

     

    If anyone has an SPI signal extender they have had success with I would be interested in exploring any references.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ralphjy
    0 ralphjy over 5 years ago in reply to colporteur

    The results of your experiment moving individual signals is interesting.  Maybe you should check that you aren’t missing something obvious.  The chip select pin is fairly low frequency.  You should check the levels and prop delay through your translator.  I think an issue on CS should be easy to spot.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur over 5 years ago in reply to ralphjy

    Thank you for reviewing my data. Another set of eyes can help uncover anomalies.

     

    I confess the cold medication induced stupor wasn't the ideal condition to be in for testing. On further review (i.e. testing) you observations are correct and the pins that won't work through the level converter are in fact different.

     

    Two pins (SCK & MOSI) if connected through the level converter cause the display to present no image. I thought maybe MISO would also would be included in the set but not according to my testing.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to colporteur

    I think MISO is not used. All data goes from master to display.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 5 years ago in reply to colporteur

    Is this module intended to shift voltage levels or drive a long cable?

    Presumably the Pi is 3.3 volts, what voltage is the LCD logic?

    How long is the cable? Some of these bidirectional level shifters cannot drive long cables.

    As Jan points out display driving signals are all unidirectional, so a bidirectional driver may not be needed.

    It sounds like the display works fine directly with Pi voltages - why is this buffer needed?

    Does the display cease to work because the cable gets too long?

    Make sure there is a good ground connection all the way from the Pi to the display, even with the buffer module in place.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • colporteur
    0 colporteur over 5 years ago in reply to Jan Cumps

    I would think the display would respond that it has received the data on the MISO line or is the line for sending data and not management like acknowledgements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ralphjy
    0 ralphjy over 5 years ago in reply to Jan Cumps

    I think in this instance the pin normally used for MISO is used for DC as shown in his first diagram (not sure why they did it that way).  Apparently, it can be remapped in the display class in the example programs from the library..

     

    # Create ST7789 LCD display class.

    disp = ST7789.ST7789(

        port=0,

        cs=ST7789.BG_SPI_CS_FRONT,  # BG_SPI_CS_BACK or BG_SPI_CS_FRONT

        dc=9,

        backlight=19,               # 18 for back BG slot, 19 for front BG slot.

        spi_speed_hz=80 * 1000 * 1000,

        offset_left=40 if display_type == "round" else 0

    )

     

    colporteur have you tried reducing the speed?  I think you do it by powers of 2.  Maybe you could try it at half speed to see if that helps.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • ralphjy
    0 ralphjy over 5 years ago in reply to Jan Cumps

    I think in this instance the pin normally used for MISO is used for DC as shown in his first diagram (not sure why they did it that way).  Apparently, it can be remapped in the display class in the example programs from the library..

     

    # Create ST7789 LCD display class.

    disp = ST7789.ST7789(

        port=0,

        cs=ST7789.BG_SPI_CS_FRONT,  # BG_SPI_CS_BACK or BG_SPI_CS_FRONT

        dc=9,

        backlight=19,               # 18 for back BG slot, 19 for front BG slot.

        spi_speed_hz=80 * 1000 * 1000,

        offset_left=40 if display_type == "round" else 0

    )

     

    colporteur have you tried reducing the speed?  I think you do it by powers of 2.  Maybe you could try it at half speed to see if that helps.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer