Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Insight why display fails with buffer board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 24 replies
  • Answers 16 answers
  • Subscribers 703 subscribers
  • Views 6384 views
  • Users 0 members are here
  • raspberry pi display
  • lcd display
  • spi data
  • raspberry_pi
Related

Insight why display fails with buffer board

colporteur
colporteur over 5 years ago

Can someone share their insight  into why no images are displayed on the LCD display when a buffer/level shifter board is inserted between the Pi and the display?

 

The project is to display images on a 1.3 inch display using a Raspberry Pi. Inspiration for the project came from Episode 465: Lego Raspberry Pi HQ Camera . I'm using the LCD screen Katie's  hifromkatie used in the project.

 

I can display images on the display https://github.com/pimoroni/st7789-python  connected directly to the Pi. Images are not displayed if I insert a buffer board between the Pi and the display. I have tried modules with TXS0108E and BSS138 chips and get the same results.

 

Attached is the pin out for connections. I confess I have limited experience with this communication protocol. I was hoping the buffer would provide some isolation for the Pi to enable me to move the display away from the Pi. I assumed a level shifter would not introduce issues but that does not appear to be the case.

 

Can you share any insight into what is causing the issue and possible solution.

 

 

 

image

 

Message was edited by: sean conway I added pictorials of the buffer/level shifting modules. The module on the left is is based on the TXS0108E chip and the right is a BSS138 fet based on an adafruit model https://www.adafruit.com/product/757

  • Sign in to reply
  • Cancel
Parents
  • jc2048
    0 jc2048 over 5 years ago

    It might help us if you gave a bit more detail of the thing you're having the problem with. A red oval isn't very illuminating.

     

    Having said that, the reason might be that you aren't using a 'buffer board', you're using a level-translation board.

     

    The 'A' side of the TXS0108E device can only go to 3.6V max, so don't power that side with 5V or you'll blow it up. You'd have to add a regulator to drop the 5V to power the 3.3V side. So Pi to 'B' side, display to 'A' side, and a 3.3V regulator to power the display and the 'A' side from the Pi's 5V.

     

    Does that make sense? If not, say and I'll try and draw something.

     

    If you wanted to [had to?] power the display from 5V, maybe two level-translate boards back-to-back, one at each end of the cable [depends how cheap they are, really]. The cable section would then operate 3.3V [you'd still need a 3.3V supply, though, for the cable section].

     

    But since you just want to buffer, why not use a buffer logic chip? Or even just try it without any buffering and see how far you can get: the Pi I/O pins probably drive quite well. With CMOS outputs to CMOS inputs, where the high and low side are fairly well balanced, series termination at the sending end works quite nicely [for ribbon cable, try something like 100R] and you could probably manage several feet without any problems at all, and further with abit of care [to improve your chances, best to keep crosstalk down and regularise the cable impedance by interleaving grounds with the signal wires]. The weakest part might be the return data from the display, depending how they've done it, but you could add a buffer at the display end or maybe you might be able to just ignore that if you don't use any return data.

     

    Edit, 31st March.

     

    I'm wrong here. I took it from your drawing that the signalling on the Pi was 5V, but it's not: it's 3.3V. So what I've written is gibberish [though the bit about getting signals down a ribbon cable still stands]. Perhaps take more note of what the others are writing below.

     

    If I were in your place, I'd ditch any idea of working with 5V, run everything on 3.3V, and, if it were even necessary to buffer, consider a bus buffer like a 74LVC125 ( SN74LVC125SN74LVC125  ) or something like that.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • jc2048
    0 jc2048 over 5 years ago

    It might help us if you gave a bit more detail of the thing you're having the problem with. A red oval isn't very illuminating.

     

    Having said that, the reason might be that you aren't using a 'buffer board', you're using a level-translation board.

     

    The 'A' side of the TXS0108E device can only go to 3.6V max, so don't power that side with 5V or you'll blow it up. You'd have to add a regulator to drop the 5V to power the 3.3V side. So Pi to 'B' side, display to 'A' side, and a 3.3V regulator to power the display and the 'A' side from the Pi's 5V.

     

    Does that make sense? If not, say and I'll try and draw something.

     

    If you wanted to [had to?] power the display from 5V, maybe two level-translate boards back-to-back, one at each end of the cable [depends how cheap they are, really]. The cable section would then operate 3.3V [you'd still need a 3.3V supply, though, for the cable section].

     

    But since you just want to buffer, why not use a buffer logic chip? Or even just try it without any buffering and see how far you can get: the Pi I/O pins probably drive quite well. With CMOS outputs to CMOS inputs, where the high and low side are fairly well balanced, series termination at the sending end works quite nicely [for ribbon cable, try something like 100R] and you could probably manage several feet without any problems at all, and further with abit of care [to improve your chances, best to keep crosstalk down and regularise the cable impedance by interleaving grounds with the signal wires]. The weakest part might be the return data from the display, depending how they've done it, but you could add a buffer at the display end or maybe you might be able to just ignore that if you don't use any return data.

     

    Edit, 31st March.

     

    I'm wrong here. I took it from your drawing that the signalling on the Pi was 5V, but it's not: it's 3.3V. So what I've written is gibberish [though the bit about getting signals down a ribbon cable still stands]. Perhaps take more note of what the others are writing below.

     

    If I were in your place, I'd ditch any idea of working with 5V, run everything on 3.3V, and, if it were even necessary to buffer, consider a bus buffer like a 74LVC125 ( SN74LVC125SN74LVC125  ) or something like that.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 5 years ago in reply to jc2048

    I updated the drawing to provide a visual of the type of bidirectional modules the red circle represents. Each output operates on its own channel. I have used these type of units in the past with good success.

     

    I interchange the terms buffer and level shifter. A bidirectional level shifter is the name pulled from the parts sites. To me it buffers the Pi from the outside world.

     

    The power supply I have tried a number of power configurations. Power both sides from the Pi, power both sides from external sources, power one side 3.3v Pi and the other side external. I have also confirmed that each channel is working or the level shifts. Using gpiozero I confirm the output can turn an LED on and off.

     

    The choice of bidirectional module was dependent on what was on the shelf. I was hoping to not have to introduce another parts module to deal with the issue. Again never used this com protocol before so maybe that is something I need to be aware of.