Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Anyone know how to access RasPi GPIO without sudo?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 709 subscribers
  • Views 9372 views
  • Users 0 members are here
  • raspberry_pi
Related

Anyone know how to access RasPi GPIO without sudo?

johnbeetem
johnbeetem over 13 years ago

I've finally gotten around to playing with RasPi GPIOs, using Gert van Loo and Dom's C code at the RasPi Wiki.  It works fine, except that you have to run the executable as root or use sudo to access /dev/mem.

 

Does anyone here know how to access /dev/mem as a normal user?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Not sure what you have against running as root--either via su, sudo $SHELL, or setuid--but you could try:

     

    $ sudo chown pi /dev/mem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Not sure what you have against running as root--either via su, sudo $SHELL, or setuid--but you could try:

     

    $ sudo chown pi /dev/mem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to e14 Contributor

    Keith Chiem wrote:

     

    Not sure what you have against running as root--either via su, sudo $SHELL, or setuid--but you could try:

     

    $ sudo chown pi /dev/mem

    I like to run as a normal user most of the time so that I don't accidentally destroy system files.  I'll try your suggestion with /dev/mem, and if it doesn't work I'll take a closer look at permissions for /dev/mem.

     

    One think that's a bit different in my case is that I'm editing and running programs within the XXICC programming environment (xxicc.org).  I'm not generating a stand-alone GPIO program which I can then run using sudo.  I currently have to run XXICC using sudo, so I'm not protected form destroying system files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Keith Chiem wrote:

     

    $ sudo chown pi /dev/mem

    That will not work.  As well as any access controls imposed by the filesystem, you also need to have capability CAP_SYS_RAWIO to open the /dev/mem device.  So you do need to be setuid root (or setcap).

     

    Note that you do not need any special permissions for any of the later steps, however.  So you can start as root, open /dev/mem, drop privileges with set(res)uid, mmap just the registers you need, close the device to make it impossible to map any more, and then continue with the rest of your code safely.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago in reply to e14 Contributor

    Roger Wolff wrote:

     

    Now back to your problem...
    If you make a little program that allows you to manipulate just the GPIO outputs, that won't allow you to cause all the other mischief you'd be able to make with "/dev/mem" access, then you can install that program with superuser permissions (setuid) and then you can use that program as a normal user.

     

    I have written such a program. IIRC, it is contained in this package:

    http://www.bitwizard.nl/software/gpio_spi_i2c_20120419.tgz

     

    The program can be made setuid by doing:

      sudo chown root <program name>

      sudo chmod 4755 <program name>

     

    jopaji wrote:

     

    Keith Chiem wrote:

     

    $ sudo chown pi /dev/mem

    That will not work.  As well as any access controls imposed by the filesystem, you also need to have capability CAP_SYS_RAWIO to open the /dev/mem device.  So you do need to be setuid root (or setcap).

     

    Note that you do not need any special permissions for any of the later steps, however.  So you can start as root, open /dev/mem, drop privileges with set(res)uid, mmap just the registers you need, close the device to make it impossible to map any more, and then continue with the rest of your code safely.

    Well, I finally got around to testing these suggestions.  I got CAP_SYS_RAWIO to work (mostly), but decided that it was too dangerous.  So I went with a combination of Roger's suggestion to use chown and chmod so that my programs starts as root, and jopaji's suggestion to call setuid(getuid()) to drop superuser access after using mmap() so as to become a normal user.

     

    This scheme is also described by nroff-man at the Raspberry Pi Forum: http://www.raspberrypi.org/forums/viewtopic.php?f=29&t=22515

     

    I also learned that you should close /dev/mem once you have done the mmap() so that you don't have a dangerous file descriptor lying around.  Here's my final code, which sets global pointer RasPiGPIO to the virtual address of the GPIO registers or NULL on failure:

     

    // Attempt to map RasPi GPIO registers to a virtual address.

    // Set RasPiGPIO to that address, or NULL if unable to map (print warning).

    static void AccessRasPiGPIO(void)

    {

        int fd = open("/dev/mem", O_RDWR);

        if (fd < 0)

        {

            fprintf(stderr, "Cannot access Raspberry Pi GPIOs: you probably need sudo.\n");

            return;

        };

        // 0x20200000 is the Debian base for mapping RasPi GPIOs using /dev/mem.

        RasPiGPIO = mmap(NULL, 0x1000, PROT_READ | PROT_WRITE, MAP_SHARED, fd, 0x20200000);

        if (RasPiGPIO == MAP_FAILED)

        {

            fprintf(stderr, "Cannot access Raspberry Pi GPIOs: mmap() failed.\n");

            RasPiGPIO = NULL;

        } else printf("XXICC can access Raspberry Pi GPIOs.\n");

        close(fd);    // No longer need /dev/map once we have the virtual address.

    }

     

    After I call this function, I set the user ID back to the original user with the code: setuid(getuid());

    Thank you to everyone for their suggestions!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    If you are the only one with access it is no real problem. I don't particularly wish to give sudo access to the kids.