Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Anyone know how to access RasPi GPIO without sudo?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 709 subscribers
  • Views 9383 views
  • Users 0 members are here
  • raspberry_pi
Related

Anyone know how to access RasPi GPIO without sudo?

johnbeetem
johnbeetem over 13 years ago

I've finally gotten around to playing with RasPi GPIOs, using Gert van Loo and Dom's C code at the RasPi Wiki.  It works fine, except that you have to run the executable as root or use sudo to access /dev/mem.

 

Does anyone here know how to access /dev/mem as a normal user?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Not sure what you have against running as root--either via su, sudo $SHELL, or setuid--but you could try:

     

    $ sudo chown pi /dev/mem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Arjan
    0 Arjan over 13 years ago

    Either you have to run your application as root, or use a device driver than trying to use /dev/mem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 13 years ago in reply to Arjan

    Unix has a "security model". As a normal users you can do stuff, but you should not be able to access other people's files on the same computer. And as a user you should not be able to cause the computer to stop working.

     

    This means that as a rule, you should not be able to directly access hardware, like the physical memory of the computer. So that's why /dev/mem is protected so that normal users cannot access it.

     

    Now "/dev/mem" allows you much, much more "mischief" than just changing a GPIO. So that's why /dev/mem must be protected against normal users.

     

    If "allowable" things need to happen, the normal way to achieve this is to make a setuid program. The program GETS the priviledges needed once it is executed, the program then checks permissions (if neccessary) and then allows you to do the little thing you wanted.

     

    As an example, the system cannot and should not allow you to insert a random packet onto the network. However the operating system does not provide a way to send "ICMP ECHO REQUEST" packets. There is a program that does that: "ping"! So the ping program gets privileges, uses that to send a carefully prepared ICMP ECHO REQUEST packet, and display the results. Although it uses the system mechanism for "sending arbitrary packets", it should restrict you to only send the innocent ICMP ECHO REQUEST packets. The ping program doesn't have any further permission checking (that I know of).

     

    Now back to your problem...
    If you make a little program that allows you to manipulate just the GPIO outputs, that won't allow you to cause all the other mischief you'd be able to make with "/dev/mem" access, then you can install that program with superuser permissions (setuid) and then you can use that program as a normal user.

     

    I have written such a program. IIRC, it is contained in this package:

    http://www.bitwizard.nl/software/gpio_spi_i2c_20120419.tgz

     

    The program can be made setuid by doing:

      sudo chown root <program name>

      sudo chmod 4755 <program name>

     

    The program I wrote has NOT been checked for security in this scenario.

     

    The responsibility of "keeping the system safe" is moved from the kernel to the program with the elevated permissions. So if the "ping" program contained a bug that, say, would allow hackers to specify arbitrary network packets, then the protection of the system that normal users cannot send arbitrary network packets breaks down.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to e14 Contributor

    Keith Chiem wrote:

     

    Not sure what you have against running as root--either via su, sudo $SHELL, or setuid--but you could try:

     

    $ sudo chown pi /dev/mem

    I like to run as a normal user most of the time so that I don't accidentally destroy system files.  I'll try your suggestion with /dev/mem, and if it doesn't work I'll take a closer look at permissions for /dev/mem.

     

    One think that's a bit different in my case is that I'm editing and running programs within the XXICC programming environment (xxicc.org).  I'm not generating a stand-alone GPIO program which I can then run using sudo.  I currently have to run XXICC using sudo, so I'm not protected form destroying system files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Does anyone here know how to access /dev/mem as a normal user?

    Don't do that.  There's a device driver for the gpios that can be made to expose them under /sys/class/gpio. Access is comparitively slow, but at least it's safer than messing with /dev/mem

     

    You can find documentation for 'gpiolib' towards the end of Documentation/gpio.txt in any recent linux kernel source tree. There you'll find out how to export particular gpios to userspace. 

    Note that you likely still need to chown some files under /sys/class/gpio to allow user access after exporting them as root. Roger is quite right on the security model - consider that gpio's will often be connected to something that sensitive and you should understand why you normally need root to access them.

     

    Here's a trivial example in bash

     

    echo 55 > /sys/class/gpio/export

    echo out > /sys/class/gpio/gpio55/direction

    echo 1 > /sys/class/gpio/gpio55/value

     

    however note that 55 isn't a valid value unless you've added a gpio expander like the mcp23008 I'm using, and recompiled the kernel appropriately.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Does anyone here know how to access /dev/mem as a normal user?

    Don't do that.  There's a device driver for the gpios that can be made to expose them under /sys/class/gpio. Access is comparitively slow, but at least it's safer than messing with /dev/mem

    Thank you for the suggestions, but I don't want slow.  This is more out of principle (what others call "pig-headedness") than any real need for my LEDs to blink one million times faster than my eye can resolve.  I figure, hey, it's my computer and what's the point of having memory-mapped I/O if I can't access it as memory?  If you're going to go through several layers of condoms to protect your GPIOs, you might as well be using a mainframe and where's the fun in that?

     

    OTOH, I do accidentally delete files from time to time and I'd hate to accidentally delete a system file or directory while being root, so I don't like to stay root for more milliseconds than necessary.  OTOH, I find I've almost never screwed up a system by accessing the wrong memory address, probably because I'm more careful doing the latter.  Back when I was programming PDP-11s, I caused any number of bus errors but never accidentally wrote bad words into the hard drive control registers.

     

    So here's something else I tried: I changed the permissions on /dev/mem to the dreaded 666 to allow anyone to access it.  That didn't work.  I also tried changing permissions on /dev/mem to 660 and added myself to the "kmem" group.  That didn't work either.  I'm a little nervous about changing the ownership of /dev/mem to myself since I'd worry that root might want to be the owner somewhere else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Keith Chiem wrote:

     

    $ sudo chown pi /dev/mem

    That will not work.  As well as any access controls imposed by the filesystem, you also need to have capability CAP_SYS_RAWIO to open the /dev/mem device.  So you do need to be setuid root (or setcap).

     

    Note that you do not need any special permissions for any of the later steps, however.  So you can start as root, open /dev/mem, drop privileges with set(res)uid, mmap just the registers you need, close the device to make it impossible to map any more, and then continue with the rest of your code safely.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mobilewill
    0 mobilewill over 13 years ago

    Here is how I did it.

     

    http://www.mobilewill.us/2012/07/raspberry-pi-and-gpio-permissions.html

     

     

    I gave access to a user to run only a script as root by editing the sudoers file. This keeps the security but allows you to access the GPIO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Greeting John

     

    I use wiringPi and have written a small daemon framework that I will finish once I sort out hardware/logic requirements.

    This sort of set up allows user space programs to talk to the daemon although I am not doing this at present.

    My application needs a push button and a tamper switch plus relay outputs (4 at first).

    Camera plus streaming audio. Motion & avconv. Signally to end points. Control of relays from EP.

    Logic to deal with a gate opener and general security at a distant gate (150m for my proof of concept).

    Push button at camera. Plays sound, cyborg voice, turns on relay (light at cam), signals end point RPi.

    End point at home TV. View, send audio to, and push button or web interface to open gate.

    The perfect application for the RPi and allows further system integration with other systems.

     

    Eventually I want to hook MC9S08 and STM32V modules to the RPi all of which I have and am reasonably competent with.

    As for Linux. I am an early implimenter starting in the days when it took days to get the bits to get a 386 going.

    By no means a ubber geek I am entirely self taught and work on a need to know basis.

     

    Always looking for people wishing to join in and can provide a private vehicle for a small development group on my hobby web site zlham.geek.nz.

    Sorry I do not accept freemail addresses unless I know who wants an account in which case it is best to email me before applying.

     

    If the OP is interested in code I can put it up on my ftp site with the caviate that it is not fit for public release as such and will be taken down again in a week or so.

     

    Regards

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to johnbeetem

    Thank you for the suggestions, but I don't want slow.  This is more out of principle (what others call "pig-headedness") than any real need for my LEDs to blink one million times faster than my eye can resolve.  I figure, hey, it's my computer and what's the point of having memory-mapped I/O if I can't access it as memory?  If you're going to go through several layers of condoms to protect your GPIOs, you might as well be using a mainframe and where's the fun in that?

    At this point I'll respectfully suggest you're looking at it the wrong way. You have two conflicting requirements, you should pick one and be done with it. Either run as root and accept that you can delete files either by using 'rm -rf /' or by scribbling the wrong stuff into /dev/mem, or run as a normal user and accept those limitations.

     

    You should also realise that the same gpio driver that you don't want to use 'owns' the memory locations you want to manually write to and as such you can't prevent the kernel from changing those locations behind your back. (you could try compiling out the gpio driver, but as the sdcard driver depends on it you'll have other problems).

    This is part of the compromise you sign up to by running linux as your OS. You are of course free to do other things by not running linux, going for a bare metal approach and treating the Pi like an arduino.

     

    I also agree with the sentiment that it's your computer and you should be able to do what you like. For that reason, especially on something like the Pi, I suggest simply running as root and forgetting about the 'problem' altogether image    I have effectively just one user on my Pi - root (there are a few more, but no others can login and they're only there to keep stuff that expects them happy)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>