Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum libusb and OpenOCD?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 2517 views
  • Users 0 members are here
  • raspberry_pi
Related

libusb and OpenOCD?

johnbeetem
johnbeetem over 12 years ago

I have a some questions about libusb and OpenOCD.  There might be a better group to ask about these, but a number of people who comment in this group know about these sorts of things.  Besides, I will want to run this stuff on RasPi so it applies.

 

Basically, I'm interested in learning to do low-level USB programming for talking to external USB devices.  I don't want to write a device driver -- I want to do everything from Userland.  From what I've read, libusb appears to be the right software for this, but it's confusing.  Before I get started, I'd like to learn from others' experience.  Here are some specific questions:

 

1.  There are several versions of libusb out there, and it appears to have an interesting FLOSS history.  There's libusb-0.1 which is old, but stable.  There's libusb-1.0 which has a different API, but it's actively being developed.  Then there's libusbx which is a fork of libusb-1.0, but it may have rejoined since libusb.org today lists libusbx-1.0.16 (2013-07-11) as the latest version.  Has anyone here developed with any of version of libusb and has some tips to share?  Also, does anyone here know about libusb history?

 

2.  Is there any better libusb documentation that what's available at libusb.org?  Google found me this this tutorial from Jan 2010, which seems to be a good start.  I'd appreciate any pointers.  There's no point doing "program by experiment" if someone has already done it and written it up.

 

I'm also interested in OpenOCD.  Has anyone here used it at the API level?  I took a quick look at the user guide and the developer documentation, and from a first impression it seems overly complex.  I need to decide if it's worth delving into OpenOCD or whether I'm better off building on my own JTAG code already written.

 

Thank you for any comments you may have.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 12 years ago

    OK, I'm making progress.  I got the "simple.c" and "find_all.c" examples working, so libftdi is able to see my FT2232H Mini-Module.  I'm still on Ubuntu 11.10 [*] so it apt-got libftdi 0.19 and still has libusb-0.1, but that should be OK for now.

     

    I didn't have to uninstall ftdi_sio explicitly: libftdi did that for me automatically.  I did have to sudo, which is an annoyance.

     

    Onward to MPSSE, JTAG, and eternal youth!

     

    [*] Why Ubuntu 11.10?  Two reasons: (1) I hate upgrading software and (2) I used a Univac 1110 in my undergrad days, so nostalgia I guess.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I did have to sudo, which is an annoyance.

    https://github.com/libusbx/libusbx/wiki/FAQ#wiki-Can_I_run_libusbx_applications_on_Linux_without_root_privilege

     

    however, with an old enough setup it may be using /proc/bus/usb instead of /dev/bus/usb and so different steps need to be taken.  I don't follow ubuntu, so have no idea what needs done for 11.10, but I'd be surprised if it's still using the /proc interface.  I have a vague memory that you could compile libusb in a way that disabled the new interface and that I had to do that at one point when libusb wasn't keeping up with kernel changes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I did have to sudo, which is an annoyance.

    https://github.com/libusbx/libusbx/wiki/FAQ#wiki-Can_I_run_libusbx_applications_on_Linux_without_root_privilege

     

    however, with an old enough setup it may be using /proc/bus/usb instead of /dev/bus/usb and so different steps need to be taken.  I don't follow ubuntu, so have no idea what needs done for 11.10, but I'd be surprised if it's still using the /proc interface.  I have a vague memory that you could compile libusb in a way that disabled the new interface and that I had to do that at one point when libusb wasn't keeping up with kernel changes.