Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum pci bus on raspberry pi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 16 replies
  • Answers 1 answer
  • Subscribers 709 subscribers
  • Views 2972 views
  • Users 0 members are here
  • pci
  • bus
  • raspberry_pi
  • pcie
Related

pci bus on raspberry pi

e14 Contributor
e14 Contributor over 12 years ago

Hello,

 

Is that possible to add a PCI or PCIe Bus on Raspberry pi?

 

If yes, how can i do it and what i need to buy?

 

King Regards,

Ricardo Silva

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 12 years ago

    It isn't possible at a reasonable cost (in money and effort). You don't say what you want to do with it so I can't be any more helpful. You would do much better to find a board that supports PCI(e) by design.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelkellett

    Thanks for the answer.

    The main goal is to use an ISDN card to make a telephone exchange. The ISDN card via USB are not so good :/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    Which ISDn card would you use - I'm wondering if it is possible to make an ISDN interface directly to the Pi without the use of a ready made card. It would need ISDN interface chips and possibly an FPGA.

     

    A possibly suitable chip with microcontroller or spi interface is:

     

    Cologne Chip - XHFC-4SU ISDN Controller IC

     

    It'll be  alot of work !

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Lurchi
    0 Lurchi over 12 years ago in reply to michaelkellett

    I think I would go for the XHFC as well. It is available as 1 to 4 ports (2 B + 1D channel each), control is quite easy, the data streams can be most likely handled using the raspberry I2S port, and there is already some code in the linux kernel to handle those (IIRC the XHFCs where also built on ISA bus cards, which will much easier map to this approach than full blown PCI(e)).

     

    Stefan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Lurchi
    0 Lurchi over 12 years ago in reply to michaelkellett

    I think I would go for the XHFC as well. It is available as 1 to 4 ports (2 B + 1D channel each), control is quite easy, the data streams can be most likely handled using the raspberry I2S port, and there is already some code in the linux kernel to handle those (IIRC the XHFCs where also built on ISA bus cards, which will much easier map to this approach than full blown PCI(e)).

     

    Stefan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Lurchi

    That kind of boards is used by the ISP Provider when install the ISDN in the costumer.

     

    So I can have access for free. Don't need to pay. Then, I link the XHFC to a BRI card (PCI) and I have a telephony exchange image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to e14 Contributor

    If you just want to plug cards in and use ready made software then forget about the PI - it's not going to happen. Find a second hand PC - you should be able to get one for the same kind of money as the RPi with all the necessary bits and pieces.

     

    MK