Raspberry Pi Forum I need help connecting to internet
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 684 subscribers
  • Views 872 views
  • Users 0 members are here
  • raspberry_pi
Related

I need help connecting to internet

Former Member
Former Member over 12 years ago

First off, I'll introduce myself. My name is Dan, and I am a pc tech/repair guy during my free time. I am young, so I don't have a lot of knowledge yet, but I am learning. I currently have next to no knowledge of how to navigate any Linux distro.

 

My issue is in internet connections. I have connected my pi (type b with pimame/raspbian os) to my router via a normal cat5 ethernet cable, and expected the network lights to blink. The result was disappointing, the lights did not blink, neither did I have access to the web through midori. The router is configured to use DHCP (I cannot access that part of my router, however my dad can, and he is a CTO for a school district). I have looked all over the internet for why this would happen, and have found no documentation for what to do in this situation. I am not sure what to do, I really only want to install ndiswrapper, that way I can install win2k drivers for my USB Wi-Fi dongle (D-link DWA-130 version E1), that way I can have wireless connection. I have also tried connecting to my pc. I connected the two with a standard ethernet cable, and installed PuTTY in order to connect the two. I get an error that the connection timed out. I have also gone the route of modifying the cmdline.txt and adding my pc's ipv4 address (which is not static I believe). I have also gone into the terminal on my pi in order to set an ip address, but that doesn't seem to assist me at all in my connection with my pc, or router.

 

If there is any way to fix my ethernet port or board (if broken), or install ndiswrapper via and offline installer or download, I would be grateful. This "malfunction" is starting to get on my nerves. If you need any more information, I would be glad to provide it.

 

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 12 years ago

    Hello Dan,

    have you try using a cross-over cable?

    When you directly connect two client with an ethernet cable you must use a cross cable.

    You have to use a cross cable also if you connect a client directly to a router port if it has not an integrated switch.

    A straight cable is fine to connect router, server or client to a switch.

     

    Ethernet port use two pairs of the rj45 connector: pins 1-2 and 3-6.

    A standard cable (straight cable) connect pins 1, 2, 3 and 6 of one connector to the same pins of the other connector.

    A cross cable connect pair 1-2 of one end to pair 3-6 on the other end, and pair 3-6 to pair 1-2.


    Enjoy your raspy....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to Former Member

    Andrea Pergola wrote:

     

    Hello Dan,

    have you try using a cross-over cable?

    When you directly connect two client with an ethernet cable you must use a cross cable.

    You have to use a cross cable also if you connect a client directly to a router port if it has not an integrated switch.

    A straight cable is fine to connect router, server or client to a switch.

     

    Ethernet port use two pairs of the rj45 connector: pins 1-2 and 3-6.

    A standard cable (straight cable) connect pins 1, 2, 3 and 6 of one connector to the same pins of the other connector.

    A cross cable connect pair 1-2 of one end to pair 3-6 on the other end, and pair 3-6 to pair 1-2.

     

    Enjoy your raspy....

    You shouldn't need a cross-over cable with RasPi.  The LAN9512 chip supports Auto-MDIX and I think it's enabled by default.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • johnbeetem
    0 johnbeetem over 12 years ago in reply to Former Member

    Andrea Pergola wrote:

     

    Hello Dan,

    have you try using a cross-over cable?

    When you directly connect two client with an ethernet cable you must use a cross cable.

    You have to use a cross cable also if you connect a client directly to a router port if it has not an integrated switch.

    A straight cable is fine to connect router, server or client to a switch.

     

    Ethernet port use two pairs of the rj45 connector: pins 1-2 and 3-6.

    A standard cable (straight cable) connect pins 1, 2, 3 and 6 of one connector to the same pins of the other connector.

    A cross cable connect pair 1-2 of one end to pair 3-6 on the other end, and pair 3-6 to pair 1-2.

     

    Enjoy your raspy....

    You shouldn't need a cross-over cable with RasPi.  The LAN9512 chip supports Auto-MDIX and I think it's enabled by default.