Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi - Splash Screen
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 704 subscribers
  • Views 2524 views
  • Users 0 members are here
  • splash
  • splashscreen
  • raspberry_pi
  • raspberrypi
  • screen
Related

Raspberry Pi - Splash Screen

JJHW
JJHW over 12 years ago

How would I add a splash screen image that is shown on boot rather then the command line text. All the methods I have seen still show the command line then the image.

Any ideas appreciated!

  • Sign in to reply
  • Cancel
Parents
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago

    hi found this

    you will need to install omxplayer first

    sudo apt-get install omxplayer

     

    First off, you will want to copy the 15 to 20 second movie file to your Raspberry Pi device.  Anything shorter and the video will end before it’s finished booting and you will continue to see the kernel messages.  You can use any video file that omxplayer can play back, but I like .mov and .mp4 files.

    • You will need to edit your /boot/cmdline.txt file:
      • sudo nano /boot/cmdline.txt
    • Add quiet to the end of the line. It will look something like this:
      • dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200 console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 elevator=deadline rootwait quiet
      • Make sure that is all on one line.
    • Press ctrl-x, type y to confirm save, then press enter to return to the command line.
    • Copy your video somewhere to the Raspberry Pi.  I keep mine in /home/pi/ and call the video video.mov
    • You will now need to create a startup script that will run omxplayer at bootup.  I have modified the script from the above link.
      • sudo nano /etc/init.d/asplashscreen

    #! /bin/sh
    ### BEGIN INIT INFO
    # Provides:          asplashscreen
    # Required-Start:
    # Required-Stop:
    # Should-Start:     
    # Default-Start:     S
    # Default-Stop:
    # Short-Description: Show custom splashscreen
    # Description:       Show custom splashscreen
    ### END INIT INFO
    do_start () {    omxplayer /home/pi/video.mov & 
        exit 0
    }
    case "$1" in
      start|"")
        do_start
        ;;
      restart|reload|force-reload)
        echo "Error: argument '$1' not supported" >&2
        exit 3
        ;;
      stop)
        # No-op
        ;;
      status)
        exit 0
        ;;
      *)
        echo "Usage: asplashscreen [start|stop]" >&2
        exit 3
        ;;
    esac
    :

    • Press ctrl-x, y to confirm saving, and press enter to return to the command line
    • Now you need to set the file to be executable
      • sudo chmod a+x /etc/init.d/asplashscreen
    • And activate it
      • sudo insserv /etc/init.d/asplashscreen

    You should now be ready to go!

    Reboot your Pi and enjoy the startup movie.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago

    hi found this

    you will need to install omxplayer first

    sudo apt-get install omxplayer

     

    First off, you will want to copy the 15 to 20 second movie file to your Raspberry Pi device.  Anything shorter and the video will end before it’s finished booting and you will continue to see the kernel messages.  You can use any video file that omxplayer can play back, but I like .mov and .mp4 files.

    • You will need to edit your /boot/cmdline.txt file:
      • sudo nano /boot/cmdline.txt
    • Add quiet to the end of the line. It will look something like this:
      • dwc_otg.lpm_enable=0 console=ttyAMA0,115200 kgdboc=ttyAMA0,115200 console=tty1 root=/dev/mmcblk0p2 rootfstype=ext4 elevator=deadline rootwait quiet
      • Make sure that is all on one line.
    • Press ctrl-x, type y to confirm save, then press enter to return to the command line.
    • Copy your video somewhere to the Raspberry Pi.  I keep mine in /home/pi/ and call the video video.mov
    • You will now need to create a startup script that will run omxplayer at bootup.  I have modified the script from the above link.
      • sudo nano /etc/init.d/asplashscreen

    #! /bin/sh
    ### BEGIN INIT INFO
    # Provides:          asplashscreen
    # Required-Start:
    # Required-Stop:
    # Should-Start:     
    # Default-Start:     S
    # Default-Stop:
    # Short-Description: Show custom splashscreen
    # Description:       Show custom splashscreen
    ### END INIT INFO
    do_start () {    omxplayer /home/pi/video.mov & 
        exit 0
    }
    case "$1" in
      start|"")
        do_start
        ;;
      restart|reload|force-reload)
        echo "Error: argument '$1' not supported" >&2
        exit 3
        ;;
      stop)
        # No-op
        ;;
      status)
        exit 0
        ;;
      *)
        echo "Usage: asplashscreen [start|stop]" >&2
        exit 3
        ;;
    esac
    :

    • Press ctrl-x, y to confirm saving, and press enter to return to the command line
    • Now you need to set the file to be executable
      • sudo chmod a+x /etc/init.d/asplashscreen
    • And activate it
      • sudo insserv /etc/init.d/asplashscreen

    You should now be ready to go!

    Reboot your Pi and enjoy the startup movie.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • atharvabenheckfan
    0 atharvabenheckfan over 12 years ago in reply to atharvabenheckfan

    this solution will show 4-5 lines of command text before the movie which cannot be bypassed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • JJHW
    0 JJHW over 12 years ago in reply to atharvabenheckfan

    Thank you seems to works so far, I still wish i could skip the first 4-5 lines but that is still better then showing the whole kernel launching

    thanks again