Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum boot failure, timeout waiting for hardware interrupt
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 17078 views
  • Users 0 members are here
  • raspberry_pi_get_started
  • raspberry_pi
Related

boot failure, timeout waiting for hardware interrupt

e14 Contributor
e14 Contributor over 12 years ago

I've acquired a brand new RaspberryPi/8GB-USD and set it up with the recommended OS, Raspbean.  Booting occasionally works, so I am familiar with the desktop, but mostly it fails and I just have to retry by switching the power off and on.

 

The error seems to be connected with the lower of the two USB ports and I get it regardless of which device (keyboard or mouse) I plug in to that port. In response to hidraw2: USB HID v1.10 Device USB Keyboard1 on usb-_usb1.3/Input1bcm2700 I get nnc0: Timeout waiting for hardware interrupt - cmd25 followed by Timeout waiting for hardware interrupt - cmd12.

 

I've noticed that when I plug into the bottom USB port it doesn't go in quite as far as when I plug into the top port.  Is there any chance that I've been given a faulty kit?

 

Hugh

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 12 years ago

    I suspect that the error is about "mmc0". This is the SD card.

     

    Can you find a different SD card to test on short notice? I'd suggest that you do that!

     

    The raspberry pi is quite tolerant of its input voltage. However, Micro USB cables are often sold that have a resistance that result in a way too low voltage. Sometimes this can cause problems. Check the voltage at the raspberry pi (TP1 and TP2). The SD card is supposed to run at 3.3V, leaving quite somar margin before things go wrong if the 5V is not enough. But in fact, the 3.3V dropping too low is the first sign of "not enough power".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 12 years ago

    I suspect that the error is about "mmc0". This is the SD card.

     

    Can you find a different SD card to test on short notice? I'd suggest that you do that!

     

    The raspberry pi is quite tolerant of its input voltage. However, Micro USB cables are often sold that have a resistance that result in a way too low voltage. Sometimes this can cause problems. Check the voltage at the raspberry pi (TP1 and TP2). The SD card is supposed to run at 3.3V, leaving quite somar margin before things go wrong if the 5V is not enough. But in fact, the 3.3V dropping too low is the first sign of "not enough power".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer