Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum a simple "printf" function
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 20 replies
  • Answers 2 answers
  • Subscribers 677 subscribers
  • Views 3065 views
  • Users 0 members are here
  • raspberry_pi
Related

a simple "printf" function

Former Member
Former Member over 11 years ago

Hi all,

            Why all of my "printf" lines have these kind of errors:

stray "\302" in program

stray "\250" in program

stray "\" in program

 

I deleted the lines and typed again but still the same. I do not think there are some typo error as all the lines with the "printf" have errors.

 

Thanks,

 

Clem

  • Sign in to reply
  • Cancel
Parents
  • bprewit
    0 bprewit over 11 years ago

    Hi, Clem:

     

    These types of errors are typically caused by stray unprintable characters in the source; the compiler objects to them as they don't fit the defined syntax.

     

    It might be helpful if you posted the actual source code and corresponding error messages.

     

    HTH,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to bprewit

    //Include standard io

    #include <stdio.h>

    #include <stdlib.h>

     

     

    //Include ArduPi library

    #include "arduPi.h"

     

     

    //Include the Marth library

    #include <math.h>

     

     

     

     

     

     

    //Needed for Serial Communication

    SerialPi Serial;

     

     

    //Needed for accessing GPIO (pinMode, digitalWrite, digitalRead,

    //I2C funcions)

    WirePi Wire;

     

     

    //Needed for SPI

    SPIPi SPI;

     

     

    //Values need for Steinhart-Hart equation

    //and calculating resistance.

    #define TENKRESISTOR 10000 //our 10K resistor

    #define BETA 4000 // This is the Beta Coefficient of your thermistor

    #define THERMISTOR 10000  //The resistance of your thermistor at room temp

    #define ROOMTEMP 298.15 // standard room temperature in Kelvin (25 Cesius).

     

     

    //Number of readings to take

    //these will be averaged out to

    //get a more accurate reading

    //You can increase/decrease this as needed

    #define READINGS 7

     

     

    int main() {

      setup();

      while(1) {

      loop();

      }

      return(0)    ;

    }

     

     

    void setup(void){

      printf(¨Starting up thermometer\n¨);

      Wire.begin();

    }

     

     

     

     

     

     

    void loop(void) {

      float avResistance;

      float resistance;

      int combinedReadings[READINGS];

      byte val0;

      byte val1;

     

     

      //Our temperature variable

      float kelvin;

      float fahrenheit;

      float celcius;

     

     

      int channelReading;

      float analogReadingArduino;

     

     

      /***********************

      ADC mappings

     

     

      Pin Adress

     

     

      0 0xDC

      1 0x9C

      2 0xCC

      3 0x8C

      4 0xAC

      5 0xEC

      6 0xBC

      7 0xFC

        ****************/

     

     

    //0xDC is our analop 0 pin

    Wire.beginTransmission(8);

    Wire.write(byte(0xDC));

    Wire.endTransmission();

     

     

    /* Grad the two bytes returned from the analog 0 pin, combine them

      and write the value to the combinedReadings array

    */

     

     

    for(int r=0; r<READINGS; r++) {

      Wire.requestFrom(8,2);

      val0 = Wire.read();

      val1 = Wire.read();

      channelReading = int(val0)*16 + int(val1>>4);

      analogReadingArduino = channelReading * 1023 / 4095;

      combinedReadings[r] = analogReadingArduino;

      delay(100);

    }

     

     

    //Grab the average of our 7 readings

    //in order to get a more accurate value avResistance = 0;

    for (int r=0; r<READINGS; r++) {

      avResistance += combinedReadings[r];

    }

    avResistance /= READINGS;

     

     

    /* We can now calculate the resistance of the readings that have come

    * back from analog 0

    */

    avResistance = (1023 / avResistance) - 1;

    avResistance = TENKRESISTOR /avResistance;

    resistance = avResistance / THERMISTOR;

     

     

    //Calculate the temperature in Kelvin

    kelvin = log(resistance);

    kelvin /= BETA;

    kelvin += 1.0 / ROOMTEMP;

    kelvin = 1.0 / kelvin;

    //printf(¨Temperature in K ¨);

    //printf(¨%f \n¨,kelvin);

     

     

    //Convert from Kelvin to Celsius

    celcius = kelvin -= 273.15;

    // printf(¨Temperature in C ¨);

    //printf(¨%f \n¨, celsius);

     

     

    //Convert from Celsius to Fahrenheit

    fahrenheit = (celcius * 1.8) + 32;

    //printf(¨Temperature in F ¨);

    //printf(¨%f \n¨, fahrenheit);

     

     

    //Three second delay before taking our next reading

    delay(3000);

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iagorubio
    0 iagorubio over 11 years ago in reply to Former Member

    Clem, you can cross compile in your desktop and then load the code on the pi.

     

    As you are using Eclipse, you just need the C plugin.

     

    C plugin (CDT) - Eclipse CDT

     

    The cross compiler - https://github.com/raspberrypi/tools/archive/master.zip.If you have git or load git on the Eclipse - EGit - you can clone the cross compiler from here https://github.com/raspberrypi/tools

     

    And then setup it to use the pi cross compiler on Eclipse  - GuruCoding.com - Raspberry Pi Eclipse Tutorial - Setting Up Cross-Compilation In Eclipse

     

    After that you can compile your code for arm in the workstation, and load it on the Pi.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to iagorubio

    Hi Iago,

                Thanks again, I will fix that one later, now I just bought another set of Pi and now my objective is to set them head less so that I can use my desktop to access them, followed this RPi VNC Server - eLinux.org but the TightVNC is not working whatever I did, the same website recommended using X11VNC which according to that website is better and more secure and can changed the default port from 5901 but never mentioned how.  Found this Setting-Up Raspberry Pi for Headless Mode with X11VNC | Code Chief's Space and followed now successfully installed X11VNC and now it is working on a default port 5901, searched the internet how to change the default but unsuccessful even though I followed them like putting x11vnc -bg -nevershared -forever -tightfilexfer -usepw rfbport 566 -display image

     

    Thanks,

     

    Clemzky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iagorubio
    0 iagorubio over 11 years ago in reply to Former Member

    You should open a new thread for this question Clemzky, so people on the list will get a meaningful subject on what is being talked on the thread so people with x11vnc experience can jump in the discussion.

     

    Right now thy are getting a message saying "A simple printf" when we are talking about headless raspberry. Some people that may be interested or experienced on the topic can miss it.

     

    I have checked the command line switches for x11vnc and looks like "rfbport" is the right command line option http://www.karlrunge.com/x11vnc/x11vnc_opts.html

     

    The only thing I don't see right in your x11vnc invocation, is you are not using it as a command line switch with a dash in front of it "-rfbport" .

     

    Try with: " sudo x11vnc -bg -nevershared -forever -tightfilexfer -usepw -rfbport 566 -display  :0".

     

    If it doesn't works try the verbose option "-v" to see if the output tells you something about what's going wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to iagorubio

    Hi Iago,

                Will do but for now time to rest I burnt my 15 hours in front of the computer, using command line will work but when i put it inside the xsession.rc to load the settings during boot up so that i do not have to do it manually, still it goes to the default port 5901.

     

    Thanks a lot,

     

     

    Clemzky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bprewit
    0 bprewit over 11 years ago in reply to Former Member

    Hi, Clem:

     

    I may not be the right person to answer this question as I'm primarily a Unix guy; I typically use vi to edit program source files.  On Windows, I'd normally use Notepad++ (free).  The Arduino editor/compiler also works in this situation .. it did hit on the problem fairly quickly.

     

    Regards,

     

    Bruce

     

    EDIT: MIsunderstood the "arduPi" part of things .. although the arduino editor DID actually hone on the problem fairly quickly ..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iagorubio
    0 iagorubio over 11 years ago in reply to Former Member

    Are you using sudo in the command line or using root permissions ?

     

    xsession.rc will be executed with the permissions of the user running the server and 566 is a privileged port. Only root can open privileged ports.

     

    If you use a port higher than 1024 does it works ? Only ports below 1024 are privileged, 5901 as example is not a privileged port.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bprewit
    0 bprewit over 11 years ago in reply to Former Member

    Okay, dirt-simple way to do VNC with a raspberry pi:

     

    1. Become root user: sudo su -
    2. Use raspi-config to enable desktop login.
    3. Install tightvncserver: apt-get install tightvncserver.
    4. Edit the file /etc/lightdm/lightdm.conf as follows:
      1. Comment out lines beginning with 'autologin'.
      2. Uncomment the lines in the section [VNCServer]  The server port can be set via the line beginning 'port='; I set it to 5901 to correspond to the VNC standard. Please see below.
      3. Change the "width" and "height" lines to suit.
      4. I changed the line 'depth=8' to 'depth=16', for no particularly good reason.
    5. Restart lightdm: /etc/init.d/lightdm restart

    This will give you a greeter (login screen) available using a vnc viewer at "ipaddr-or-hostname:x" where "ipaddr-or-hostname" is either the ip address or recognized hostname of your RPi and x is either (port number) or  (5900+x-display-number).

     

    IMHO, using the greeter takes care of a whole lot of security issues and more or less allows running VNC on default ports; I've used this technique to provide remote access to Linux systems for many years without any trouble.  Sure, the passwords are sent clear-text but someone would have to REALLY WANT to hack your pi .. YMMV

     

    EDIT: added 'sudo su -' as first command ..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to bprewit

    Hi Bruce,

                    Thanks for your time answering my question, I followed your instructions, rebooted then the greeter appears, I forgot my password and almost panic;-) managed to log in using tightvnc with port 5901 using my desktop, so it looks like the instruction above does not work in my pi.

     

    Thanks,

     

    Clemzky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bprewit
    0 bprewit over 11 years ago in reply to Former Member

    Hi, Clem:

     

    I'm not sure from your message if you were successful or not .. if not, then let's figure out why!

     

    Regards,

     

    Bruce

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to bprewit

    Hi Bruce,

               Still not successful, the only thing happens with your instruction was I have a greeter but still I am logging in using port 5901 not on the port I set.

     

    Thanks,

     

    Clemzky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to bprewit

    Hi Bruce,

               Still not successful, the only thing happens with your instruction was I have a greeter but still I am logging in using port 5901 not on the port I set.

     

    Thanks,

     

    Clemzky